Hello,
I have recently designed a power supply circuit using the flyback converter topology to step down my input voltage and produce a 5v output supply to power an embedded systems project I am working on.
One key design consideration was meeting a requirement for 2kV galvanic isolation between the input and output stages of this converter. When choosing a transformer I selected [THIS - 750319924] model which is available through DigiKey.
At the time I selected it I was operating under the assumption that I could calculate the peak voltage isolation by simply multiplying the value given by the component page on DigiKey’s site (1500 Vrms) by sqrt(2) which gives 2115 Vpeak.
However, after a colleague pointed out that the official datasheet for said transformer lists the isolation test voltage as 1500 V (AC).
Now I have confused myself and I am unsure if this is the same thing. A cursory google search tells me that V (AC) =/= Vrms. Can anyone provide more information or clarify this for me? I am wondering if the product page on DigiKey incorrectly listed the component’s isolation at 1500 Vrms when it should actually be 1500 V (AC). Are these really the same thing?
I am stressing about whether I need to change out my transformer for something with a higher isolation rating, but doing so will increase cost and require a larger physical footprint on the final pcb.
Any assistance would be greatly appreciated. Thanks!