I want to make my own power station for a vehicle but I am having some problems finding this box and the company want to sell only their preinstalled packages.
Any help is appreciated.
I can’t tell from the photo what box you are looking for. Can you provide the details on what is needed?
The larger enclosure which appears to be 18x30x2.
I can see if we have a similar enclosure. What dimensions do you need?
Ideally 16” x 26” x 2”.
The website the box is from is out of Australia, and I’m waiting to hear back if they will give me more info.
There are no options with similar dimensions. Please look through the enclosures we have here and see if any of those dimensions will work.
Ok, thanks. I think those will be too deep. I’ll grab more measurements.
Also, If it turns out that there is not an off the shelf option you can e-mail the below address.
They will need the full dimensions that you are wanting/needing the enclosure to be.
Modenclosures@digikey.com
If you are able to do so You should provide a drawing that would also include any other feature you would want.
– Switch holes
– Screw hole locations with sizes(thread size)
– Cord entry locations
– etc.
They can then work with you to do any further defining / refinement that is needed and also quote you on the overall item.