Introduction
Angle sensors are devices used to measure the change in angle or inclination of objects or systems and convert them into usable output signals. They have wide applications in various fields such as automotive, engineering machinery, aerospace, and more. Angle sensors are part of a number of systems that can help determine the position of objects.
Type of angle sensor
Angle sensors can be divided into various types based on their working principles and application scenarios, including optical, resistive, pressure, magnetic, and inertial types. Each type has its unique characteristics, and the appropriate product can be selected based on the characteristics of different types of angle sensors during application.
1. Optical Angle Sensor
Optical angle sensors are sensors that use optical principles to measure changes in the angle of an object. They utilize optical devices (such as photodiodes or lasers) to make this measurement. They are highly accurate and are commonly used in applications where precise angle measurements are critical, such as in robotics, industrial automation, aerospace, and medical devices.
Working principle of Optical Angle Sensor
Optical angle sensors typically use light sources such as photodiodes or lasers to shine onto a reflective surface, and then collect the reflected light.
The sensor analyzes the characteristics of the collected reflected light (such as the position and intensity of the light) to calculate the angle change of an object. When the angle of the object changes, the reflected light will shift accordingly, and the sensor determines the angle of the object by measuring this shift.
Advantages
-
Optical angle sensors offer very high resolution and accuracy, essential for precision applications.
-
Due to the extremely fast speed of light, optical angle sensors typically have fast response times, making them suitable for applications that require real-time reactions.
-
Optical angle sensors are ideal for non-contact measurement, as they don’t need direct contact with the object, preventing damage or interference.
-
They also adapt well to different surfaces and lighting conditions, making them versatile in various environments.
Limitation
- Optical angle sensors are often more expensive than other types.
Application
- Due to its high precision and fast response characteristics, optical angle sensors are widely used in industrial automation, robot control, aerospace, and other fields, and are also commonly found in consumer products such as game controllers, phone gyroscopes, etc.
2. Resistive Angle Sensor
A resistive angle sensor is a type of angle sensor that measures the angular position of an object by detecting changes in electrical resistance,
Resistive angle sensors have a low cost and high reliability, making them suitable for applications where high precision is not required, such as knob controls in household appliances.
Rotary potentiometers and spring-loaded resistive elements are commonly used types.
Working principle of Resistive Angle Sensor
A rotary potentiometer is one common type of resistive angle sensor, which consists of a fixed resistor and a rotatable sliding contact.
As the sliding contact rotates with the angle of an object, the position of the contact point between the contact and the resistor changes, resulting in a change in resistance value.
The angle sensor measures the resistance value corresponding to the position of the sliding contact point to reflect the angle change of the object. Typically, there is a linear relationship between resistance value and angle, or it can be converted according to specific calibration methods.
A spring-loaded resistor is another type of angle sensor used for measuring angles, for example in knobs, potentiometers, and other control devices.
This sensor’s structure includes a rotating spring spiral and a fixed resistive element, often a carbon film resistor, which maintain physical contact. When a user rotates the spring-loaded resistor, the rotation of the spring spiral changes the contact area between the spring and the resistor device, thereby affecting the resistance value. When the contact area increases, the resistance value decreases; conversely, when the contact area decreases, the resistance value increases. By measuring the resistance value, the rotation angle can be inferred, thus enabling corresponding angle measurement.
Advantages
-
Resistive angle sensors are cost-effective to manufacture, making them popular in cost-sensitive applications.
-
Their simple structure and resistance to external interference enhance their reliability.
-
The straightforward design makes resistive angle sensors easy to install and use.
Limitation
- Compared to some other types, resistive angle sensors may experience wear over time, requiring regular maintenance and replacement for prolonged use.
Application
- Resistive angle senser are Ideal for applications that do not require high measurement accuracy, such as:
-
Knob controls in household appliances
-
Angle monitoring in mechanical devices
3. Pressure Angle Sensor
Pressure angle sensors are sensors that use pressure changes to infer changes in the angle of an object. Common types, such as piezoelectric and piezoresistive sensors, are used in applications requiring resistance to high pressure and high temperature environments, such as angle sensors in car engines.
Working principle of Pressure Angle Sensor
Piezoelectric sensor is a common type of pressure angle sensor. It contains piezoelectric material, which generates a change in electric charge when external pressure is applied. The angle change of an object can be inferred by measuring this change in electric charge.
Another type is the Resistive pressure sensor, which measures angle changes by utilizing the effect of pressure on resistance. When an object undergoes an angle change, the resistance of the resistive pressure sensor will change accordingly, reflecting the angle change.
Advantages
-
Pressure angle sensors are highly resistant to high pressure and temperature, making them ideal for harsh environmental conditions, such as in car engine angle sensors.
-
Pressure angle sensors offer quick response capabilities, making them suitable for applications that require rapid feedback.
-
These sensors are known for their reliability, being less susceptible to external interference, ensuring stable operation.
Important Considerations: When using pressure angle sensors, it is crucial to consider the sensor’s pressure range and ensure that the pressure variations of the measured object are accounted for in the design.
Application
- Due to their robust characteristics, pressure angle sensors are used in various industries, including automotive, marine shipping, and construction engineering.
4. Magnetic Angle Sensor
Magnetic angle sensors utilize the principle of magnetic field induction to measure changes in the angle of an object, including magnetoresistive, Hall effect, and magnetostrictive sensors.
Magnetic angle sensors offer several advantages over traditional mechanical sensors, such as durability, high resolution, and resistance to external environmental factors like dust, dirt, and moisture.
Working principle of Magnetic Angle Sensor
A magnetostrictive angle sensor utilizes the magnetostrictive effect to measure changes in angle. It consists of a magnetic field source and a magnetostrictive device. When an object undergoes an angle change, the direction and intensity of the magnetic field will change accordingly, affecting the resistance value of the magnetostrictive device. The sensor infers angle changes by measuring the resistance value variations.
The Hall effect angle sensor utilizes Hall devices to sense changes in magnetic fields. These sensors detect the magnetic field generated by the rotating magnet. When an object undergoes an angle change, the direction and strength of the magnetic field will change. The Hall device detects this magnetic field change and generates a corresponding voltage change. The sensor infers the angle change by measuring the voltage change.
Advantages
-
Magnetic angle sensors offer precise measurement of small angular changes.
-
Some magnetic angle sensors respond quickly, making them suitable for dynamic applications that require rapid feedback.
-
These sensors are not easily affected by external environmental factors, making them reliable in challenging conditions. Since magnetic sensors do not rely on light, they perform well in environments with strong or variable lighting.
Limitation
-
While they offer significant advantages, magnetic angle sensors can be more expensive than other types of angle sensors, such as resistive sensors.
-
Magnetic angle sensors can be susceptible to interference from external magnetic fields, which can affect accuracy.
Application
- Due to their characteristics, magnetic angle sensors are suitable for a variety of industrial, mechanical, aerospace, and other fields, such as automotive steering systems, unmanned aerial vehicle attitude control, etc.
5. Inertial angle sensor
An inertial angle sensor measures angles based on inertial sensing technology, primarily using accelerometers, gyroscopes, or a combination of both. These sensors are especially helpful for applications that need accurate angle measurements, even in dynamic environments where external factors like movement, tilt, or vibration can affect the object’s orientation.
Working Principle of Inertial Angle Sensors
Inertial angle sensors typically use fusion algorithms (such as Kalman filters) to integrate data from gyroscopes and accelerometers to improve the accuracy and stability of angle measurements.
An accelerometer is type of inertial sensor used to measure the acceleration of an object.
These detect changes in gravitational force and can determine tilt or static angles relative to the earth’s gravitational field. When the object moves, the accelerometer detects the change in acceleration, and this change is then used to calculate the angle of movement.
Gyroscopes are a key part of inertial angle sensors, using the gyro effect to measure the angular velocity of an object. When the object rotates, the gyroscope captures this rotational speed, and generates a corresponding output signal, which can be used to calculate the angle change.
Many inertial angle sensors combine accelerometers and gyroscopes to enhance accuracy. This setup provides both static angle (tilt) and dynamic angle (rotation) measurements, which are essential for applications with both stationary and moving components.
Advantages
-
Inertial angle sensors have rapid response capabilities, enabling real-time sensing and quick reactions to changes in an object’s angle, ideal for high-speed dynamic control applications.
-
Inertial sensors do not rely on external factors such as light or magnetic fields, making them stable and less affected by external interference.
-
Built to last in various environments, they can operate reliably over long periods, maintaining stable performance.
Limitation
-
Inertial sensors often require regular calibration to maintain precise readings, especially in high-accuracy applications.
-
Small errors can build up in gyroscopes, making them less accurate for long-term measurements.
Application
- Inertial angle sensors are Suitable for applications like drone flight control and virtual reality, where constant, accurate tracking of angles is essential.
Angle Sensors from DigiKey
Angle Sensors and Sensor Evaluation Boards
Key Tips and Considerations for Selecting an Angle Sensor
There are many different types of angle sensors with various product characteristics.
-
Accuracy: the first thing to consider is the requirement for angle measurement accuracy in the application scenario. Some applications may require very high accuracy, while others may be able to accept lower accuracy. Choose a sensor with accuracy suited to your specific needs.
-
Dynamic Response Capability: For applications needing real-time response to dynamic changes, consider sensors with high dynamic performance (e.g., inertial angle sensors). For static measurements, other types may be more appropriate.
-
Environmental Suitability: Choose angle sensors based on the work environment:
- High Temperature and Vibration Resistance are necessary for sensors inside car engines.
- Waterproofing, Pressure, and Corrosion Resistance are Needed for outdoor or harsh conditions.
-
Range and Accuracy Matching: Ensure the sensor’s measurement range and accuracy align with the application’s needs. Choosing an angle sensor with a range that is too large or too small may lead to inaccurate measurement results or failure to meet your requirements.
-
Signal-to-Noise Ratio and Stability: A good signal-to-noise ratio improves measurement accuracy, while stability is key for reliable, long-term performance.
-
Cost vs. Performance Balance: Finally, it is necessary to consider the cost and performance of angle sensors comprehensively. High-performance sensors may be costly, and lower-cost options may lack precision or durability for demanding environments. Balance cost with performance based on your needs.
Common problems and solutions of application angle sensors
When using angle sensors from an application perspective, common issues may include accuracy problems, calibration issues, external interference, dynamic response, etc.
Accuracy Issues: Insufficient accuracy can lead to inaccurate measurements. Solutions include using a high-precision angle sensor or combining data from multiple sensors (e.g., Kalman filter) to enhance accuracy.
Calibration Needs: Regular calibration is essential to avoid measurement deviations. Follow the manufacturer’s calibration methods to ensure consistent accuracy.
Durability Concerns: Harsh environments may damage some sensors. When purchasing, it is advisable to choose durable sensors and provide appropriate protection, such as waterproofing and heat resistance, based on the application needs.
External Interference: Environmental factors (magnetic fields, light, vibrations) can affect accuracy and stability. Choose angle sensors with good anti-interference capabilities, or mitigate interference during installation, such as shielding magnetic fields and avoiding strong light.
Conclusion
Angle sensors are essential for precise measurement and tracking in various industries. With types like optical, resistive, pressure, magnetic, and inertial, each sensor has its own strengths and is suited to specific applications. Choosing the right sensor depends on factors like accuracy, environmental conditions, and dynamic response needs.
To ensure reliable performance, it’s crucial to address issues like calibration, accuracy, and external interference, along with regular maintenance. By considering these factors, users can select the best sensor for their application, ensuring accurate and efficient results.
Check more article on Angle Sensors
How to Choose and Use Angle Sensors for Power Steering, Motors and Robotics
Inertial Sensor Overview-Performance, Size, and Power Advantages
Applicable Part Numbers
| DigiKey Part Number | Manufacturer Part Number |
|---|---|
| TLE5009E1000FUMA1TR-ND,TLE5009E1000FUMA1CT-ND,TLE5009E1000FUMA1DKR-ND | TLE5009E1000FUMA1 |
| TLE5501E0002XUMA1TR-ND,TLE5501E0002XUMA1CT-ND,TLE5501E0002XUMA1DKR-ND | TLE5501E0002XUMA1 |
| HAL3725DJ-ATR-ND,HAL3725DJ-ACT-ND,HAL3725DJ-ADKR-ND | HAL3725DJ-A |
| 342-1008-2-ND,342-1008-1-ND,342-1008-6-ND | HMC1501-TR |
| HAL3727DJ-ATR-ND,HAL3727DJ-ACT-ND,HAL3727DJ-ADKR-ND | HAL3727DJ-A |
| 342-1010-2-ND,342-1010-1-ND,342-1010-6-ND | HMC1512-TR |
| AS5601-ASOMTR-ND,AS5601-ASOMCT-ND,AS5601-ASOMDKR-ND | AS5601-ASOM |
| 620-AAS33001LLEATR-5TR-ND,620-AAS33001LLEATR-5CT-ND,620-AAS33001LLEATR-5DKR-ND | AAS33001LLEATR-5 |
| 223-1255-2-ND,223-1255-1-ND,223-1255-6-ND | G-MRCO-016 |
| AS5600-ASOTTR-ND,AS5600-ASOTCT-ND,AS5600-ASOTDKR-ND | AS5600-ASOT |
| AS5600-ASOMTR-ND,AS5600-ASOMCT-ND,AS5600-ASOMDKR-ND | AS5600-ASOM SOIC8 LF T&RDP |
| AS5601-ASOTTR-ND,AS5601-ASOTCT-ND,AS5601-ASOTDKR-ND | AS5601-ASOT |
| 1589-MA782GGU-ZTR-ND,1589-MA782GGU-ZCT-ND,1589-MA782GGU-ZDKR-ND | MA782GGU-Z |
| TLI5012BE1000XUMA1TR-ND,TLI5012BE1000XUMA1CT-ND,TLI5012BE1000XUMA1DKR-ND | TLI5012BE1000XUMA1 |
| 1589-1516-2-ND,1589-1516-1-ND,1589-1516-6-ND | MA702GQ-Z |
| 1589-1517-2-ND,1589-1517-1-ND,1589-1517-6-ND | MA730GQ-Z |
| 1589-1502-2-ND,1589-1502-1-ND,1589-1502-6-ND | MA702GQ-P |
| 1589-MA732GQ-ZTR-ND,1589-MA732GQ-ZCT-ND,1589-MA732GQ-ZDKR-ND | MA732GQ-Z |
| 391-1065-2-ND,391-1065-1-ND,391-1065-6-ND | AAT001-10E |
| 391-1069-2-ND,391-1069-1-ND,391-1069-6-ND | AAT003-10E |
| 1589-MAQ470GQE-AEC1-ZTR-ND,1589-MAQ470GQE-AEC1-ZCT-ND,1589-MAQ470GQE-AEC1-ZDKR-ND | MAQ470GQE-AEC1-Z |
| 1589-MA330GQ-ZTR-ND,1589-MA330GQ-ZCT-ND,1589-MA330GQ-ZDKR-ND | MA330GQ-Z |
| 1833-IPS2550DE1RTR-ND,1833-IPS2550DE1RCT-ND,1833-IPS2550DE1RDKR-ND | IPS2550DE1R |
| 4991-AS5055A-BQFMQFN16LFT&RDPTR-ND,4991-AS5055A-BQFMQFN16LFT&RDPCT-ND,4991-AS5055A-BQFMQFN16LFT&RDPDKR-ND | AS5055A-BQFM QFN16 LF T&RDP |
| AS5048B-HTSP-500TR-ND,AS5048B-HTSP-500CT-ND,AS5048B-HTSP-500DKR-ND | AS5048B-HTSP-500 |
| AS5162-HSOMTR-ND,AS5162-HSOMCT-ND,AS5162-HSOMDKR-ND | AS5162-HSOM |
| AS5048B-HTSPTR-ND,AS5048B-HTSPCT-ND,AS5048B-HTSPDKR-ND | AS5048B-HTSP |
| AS5048A-HTSP-500TR-ND,AS5048A-HTSP-500CT-ND,AS5048A-HTSP-500DKR-ND | AS5048A-HTSP-500 |
| 4991-AS5048A-HTSPTR-ND,4991-AS5048A-HTSPCT-ND,4991-AS5048A-HTSPDKR-ND | AS5048A-HTSP TSSOP14 LF T&RDP |
| 1993-1011-ND | PST360G2-1A-C0000-ERA360-05K |
| 1993-PS2P-ARC-CE-M008-A-110S-05-ND | PS2P-ARC-CE-M008-A-110S-05 |
| 620-A1333LLETR-TTR-ND,620-A1333LLETR-TCT-ND,620-A1333LLETR-TDKR-ND | A1333LLETR-T |
| TLE5501E0001XUMA1TR-ND,TLE5501E0001XUMA1CT-ND,TLE5501E0001XUMA1DKR-ND | TLE5501E0001XUMA1 |
| 620-2016-2-ND,620-2016-1-ND,620-2016-6-ND | A1330LLETR-T |
| 1589-MA735GGU-ZTR-ND,1589-MA735GGU-ZCT-ND,1589-MA735GGU-ZDKR-ND | MA735GGU-Z |
| HAL3737DJ-ATR-ND,HAL3737DJ-ACT-ND,HAL3737DJ-ADKR-ND | HAL3737DJ-A |
| TLE5009E1010FUMA1TR-ND,TLE5009E1010FUMA1CT-ND,TLE5009E1010FUMA1DKR-ND | TLE5009E1010FUMA1 |
| 620-A1333LLETR-5-TTR-ND,620-A1333LLETR-5-TCT-ND,620-A1333LLETR-5-TDKR-ND | A1333LLETR-5-T |
| 1589-1501-2-ND,1589-1501-1-ND,1589-1501-6-ND | MA302GQ-P |
| 505-ADA4571BRZ-R7TR-ND,505-ADA4571BRZ-R7CT-ND,505-ADA4571BRZ-R7DKR-ND | ADA4571BRZ-R7 |
| 1589-MA780GQ-ZTR-ND,1589-MA780GQ-ZCT-ND,1589-MA780GQ-ZDKR-ND | MA780GQ-Z |
| 620-1766-2-ND,620-1766-1-ND,620-1766-6-ND | A1335LLETR-T |
| TLE5012BE1000XUMA1TR-ND,TLE5012BE1000XUMA1CT-ND,TLE5012BE1000XUMA1DKR-ND | TLE5012BE1000XUMA1 |
| TLE5012BE3005XUMA1TR-ND,TLE5012BE3005XUMA1CT-ND,TLE5012BE3005XUMA1DKR-ND | TLE5012BE3005XUMA1 |
| TLE5012BE5000XUMA1TR-ND,TLE5012BE5000XUMA1CT-ND,TLE5012BE5000XUMA1DKR-ND | TLE5012BE5000XUMA1 |
| 1589-MA734GQ-ZTR-ND,1589-MA734GQ-ZCT-ND,1589-MA734GQ-ZDKR-ND | MA734GQ-Z |
| TLE5012BDE1200XUMA1TR-ND,TLE5012BDE1200XUMA1CT-ND,TLE5012BDE1200XUMA1DKR-ND | TLE5012BDE1200XUMA1 |
| 445-175080-2-ND,445-175080-1-ND,445-175080-6-ND | TAS2143-AAAA |
| 2190-105040402-01-ND | 105040402-01 |
| 1993-PS2P-CON-CE-M001-2AA-C0002-ERA360-05-ND | PS2P-CON-CE-M001-2AA-C0002-ERA360-05 |
| 1993-PS2P-CON-CE-M001-1A0-C0007-ERA180-05-ND | PS2P-CON-CE-M001-1A0-C0007-ERA180-05 |
| 1993-1003-ND | PSC360G2-F1A-C0000-ERA360-05K |
| 1993-PST360G2-B-1A-C0000-ERA360-05K-ND | PST360G2-B-1A-C0000-ERA360-05K |
| CH927-ND | CU103602 |
| 1993-PST360G2-2AA-C0123-ERA040-05K-ND | PST360G2-2AA-C0123-ERA040-05K |
| TLE5009E2000FUMA1TR-ND,TLE5009E2000FUMA1CT-ND,TLE5009E2000FUMA1DKR-ND | TLE5009E2000FUMA1 |
| HAL3736DJ-ATR-ND,HAL3736DJ-ACT-ND,HAL3736DJ-ADKR-ND | HAL3736DJ-A |
| TLE5009E2010FUMA1TR-ND,TLE5009E2010FUMA1CT-ND,TLE5009E2010FUMA1DKR-ND | TLE5009E2010FUMA1 |
| 505-ADA4570BRZ-ND | ADA4570BRZ |
| 223-1562-2-ND,223-1562-1-ND,223-1562-6-ND | G-MRCO-037 |
| 505-ADA4571BRZ-ND | ADA4571BRZ |
| 1589-MA736GGU-ZTR-ND,1589-MA736GGU-ZCT-ND,1589-MA736GGU-ZDKR-ND | MA736GGU-Z |
| 391-1084-2-ND,391-1084-1-ND,391-1084-6-ND | AAT101-10E |
| TLE5012BE5020XUMA1TR-ND,TLE5012BE5020XUMA1CT-ND,TLE5012BE5020XUMA1DKR-ND | TLE5012BE5020XUMA1 |
| 1589-MA782GGU-PTR-ND,1589-MA782GGU-PCT-ND,1589-MA782GGU-PDKR-ND | MA782GGU-P |
| 505-ADA4571WHRZ-R7TR-ND,505-ADA4571WHRZ-R7CT-ND,505-ADA4571WHRZ-R7DKR-ND | ADA4571WHRZ-R7 |
| 1589-MA730GQ-PTR-ND,1589-MA730GQ-PCT-ND,1589-MA730GQ-PDKR-ND | MA730GQ-P |
| 391-1082-2-ND,391-1082-1-ND,391-1082-6-ND | AAT006-10E |
| 391-1070-2-ND,391-1070-1-ND,391-1070-6-ND | AAT009-10E |
| TLE5009A16DE1210XUMA1TR-ND,TLE5009A16DE1210XUMA1CT-ND,TLE5009A16DE1210XUMA1DKR-ND | TLE5009A16DE1210XUMA1 |
| 445-175079-2-ND,445-175079-1-ND,445-175079-6-ND | TAS2141-AAAB |
| MLX90366LVS-ADU-250-TU-ND | MLX90366LVS-ADU-250-TU |
| MLX90333KDC-BCT-000-RETR-ND,MLX90333KDC-BCT-000-RECT-ND,MLX90333KDC-BCT-000-REDKR-ND | MLX90333KDC-BCT-000-RE |
| TLE5012BDE9200XUMA1TR-ND,TLE5012BDE9200XUMA1CT-ND,TLE5012BDE9200XUMA1DKR-ND | TLE5012BDE9200XUMA1 |
| CH1000-ND | ANG-21HAW1 |
| 1993-PSC360G2-F1A-C0006-ERA060-05K-ND | PSC360G2-F1A-C0006-ERA060-05K |
| 1993-PST360G2-1A-C0011-ERA090-REK-ND | PST360G2-1A-C0011-ERA090-REK |
| 1993-PST360G2-1S-C0000-ERA360-05K-ND | PST360G2-1S-C0000-ERA360-05K |
| 1993-1009-ND | PSC360G2-F2AA-C0002-ERA360-05K |
| 1589-1503-2-ND,1589-1503-1-ND,1589-1503-6-ND | MA800GQ-P |
| 620-AAS33001LLEATR-ND,620-AAS33001LLEATRCT-ND,620-AAS33001LLEATRDKR-ND | AAS33001LLEATR |
| TLE5109A16E2210XUMA1TR-ND,TLE5109A16E2210XUMA1CT-ND,TLE5109A16E2210XUMA1DKR-ND | TLE5109A16E2210XUMA1 |
| 505-ADA4570WHRZ-ND | ADA4570WHRZ |
| 505-ADA4571BRZ-RLTR-ND,505-ADA4571BRZ-RLCT-ND,505-ADA4571BRZ-RLDKR-ND | ADA4571BRZ-RL |
| 1589-MAQ430GQE-AEC1-ZTR-ND,1589-MAQ430GQE-AEC1-ZCT-ND,1589-MAQ430GQE-AEC1-ZDKR-ND | MAQ430GQE-AEC1-Z |
| 1589-MA736GGU-PTR-ND,1589-MA736GGU-PCT-ND,1589-MA736GGU-PDKR-ND | MA736GGU-P |
| 1589-MA735GGU-PTR-ND,1589-MA735GGU-PCT-ND,1589-MA735GGU-PDKR-ND | MA735GGU-P |
| 1589-MA734GQ-PTR-ND,1589-MA734GQ-PCT-ND,1589-MA734GQ-PDKR-ND | MA734GQ-P |
| TLE5014S16XUMA1TR-ND,TLE5014S16XUMA1CT-ND,TLE5014S16XUMA1DKR-ND | TLE5014S16XUMA1 |
| TLE5014C16XUMA1TR-ND,TLE5014C16XUMA1CT-ND,TLE5014C16XUMA1DKR-ND | TLE5014C16XUMA1 |
| AS5172B-HTSTTR-ND,AS5172B-HTSTCT-ND,AS5172B-HTSTDKR-ND | AS5172B-HTST |
| 480-APS00BTR-ND,480-APS00BCT-ND,480-APS00BDKR-ND | APS00B |
| 1589-MA732GQ-PTR-ND,1589-MA732GQ-PCT-ND,1589-MA732GQ-PDKR-ND | MA732GQ-P |
| TLE5309DE5201XUMA1TR-ND,TLE5309DE5201XUMA1CT-ND,TLE5309DE5201XUMA1DKR-ND,2156-TLE5309DE5201XUMA1-ND | TLE5309DE5201XUMA1 |
| 505-ADA4571-2WHRZ-RLTR-ND,505-ADA4571-2WHRZ-RLCT-ND,505-ADA4571-2WHRZ-RLDKR-ND | ADA4571-2WHRZ-RL |
| TLE5014P16DXUMA1TR-ND,TLE5014P16DXUMA1CT-ND,TLE5014P16DXUMA1DKR-ND | TLE5014P16DXUMA1 |
| TLE5014S16DXUMA1TR-ND,TLE5014S16DXUMA1CT-ND,TLE5014S16DXUMA1DKR-ND | TLE5014S16DXUMA1 |
| 1993-1006-ND | PSC360G2-F1A-C0007-ERA180-05K |
| 1790-IQS7221E001QFRTR-ND,1790-IQS7221E001QFRCT-ND,1790-IQS7221E001QFRDKR-ND | IQS7221E001QFR |
| 620-CT310LS-ID8TR-ND,620-CT310LS-ID8CT-ND,620-CT310LS-ID8DKR-ND | CT310LS-ID8 |
| 620-CT310LS-HD8TR-ND,620-CT310LS-HD8CT-ND,620-CT310LS-HD8DKR-ND | CT310LS-HD8 |
| 620-CT310LS-HT8TR-ND,620-CT310LS-HT8CT-ND,620-CT310LS-HT8DKR-ND | CT310LS-HT8 |
| 296-TMAG6180EDGKRQ1TR-ND,296-TMAG6180EDGKRQ1CT-ND,296-TMAG6180EDGKRQ1DKR-ND | TMAG6180EDGKRQ1 |
| 1589-MA800GQ-ZTR-ND,1589-MA800GQ-ZCT-ND,1589-MA800GQ-ZDKR-ND | MA800GQ-Z |
| 296-TMAG6181EDGKRQ1TR-ND,296-TMAG6181EDGKRQ1CT-ND,296-TMAG6181EDGKRQ1DKR-ND | TMAG6181EDGKRQ1 |
| 1589-MAQ850GQE-AEC1-PTR-ND,1589-MAQ850GQE-AEC1-PCT-ND,1589-MAQ850GQE-AEC1-PDKR-ND | MAQ850GQE-AEC1-P |
| 1589-MAQ820GQE-AEC1-PTR-ND,1589-MAQ820GQE-AEC1-PCT-ND,1589-MAQ820GQE-AEC1-PDKR-ND | MAQ820GQE-AEC1-P |
| 1589-MAQ800GQE-AEC1-PTR-ND,1589-MAQ800GQE-AEC1-PCT-ND,1589-MAQ800GQE-AEC1-PDKR-ND | MAQ800GQE-AEC1-P |
| 413-MLX90427GDC-AAC-900-RETR-ND,413-MLX90427GDC-AAC-900-RECT-ND,413-MLX90427GDC-AAC-900-REDKR-ND | MLX90427GDC-AAC-900-RE |
| 246-HAL3970DJ-A-ND | HAL3970DJ-A |
| 620-A1330LLETR-DD-TTR-ND,620-A1330LLETR-DD-TCT-ND,620-A1330LLETR-DD-TDKR-ND | A1330LLETR-DD-T |
| 505-ADA4570WHRZ-R7TR-ND,505-ADA4570WHRZ-R7CT-ND,505-ADA4570WHRZ-R7DKR-ND | ADA4570WHRZ-R7 |
| TLE5012BE9000XUMA1TR-ND,TLE5012BE9000XUMA1CT-ND,TLE5012BE9000XUMA1DKR-ND | TLE5012BE9000XUMA1 |
| 246-HAL3930DJ-A-ND | HAL3930DJ-A |
| 246-HAL3980DJ-A-ND | HAL3980DJ-A |
| 448-TLE5014SP16E0001XUMA1TR-ND,448-TLE5014SP16E0001XUMA1CT-ND,448-TLE5014SP16E0001XUMA1DKR-ND | TLE5014SP16E0001XUMA1 |
| 620-CT310LS-AT8TR-ND,620-CT310LS-AT8CT-ND,620-CT310LS-AT8DKR-ND | CT310LS-AT8 |
| 620-CT310LS-FD8TR-ND,620-CT310LS-FD8CT-ND,620-CT310LS-FD8DKR-ND | CT310LS-FD8 |
| 246-HAR3927DJ-A-ND | HAR3927DJ-A |
| 620-CT310LS-FT8TR-ND,620-CT310LS-FT8CT-ND,620-CT310LS-FT8DKR-ND | CT310LS-FT8 |
| 413-MLX90427GGO-AAC-300-RETR-ND,413-MLX90427GGO-AAC-300-RECT-ND,413-MLX90427GGO-AAC-300-REDKR-ND | MLX90427GGO-AAC-300-RE |
| 246-HAC3930UF-A-ND | HAC3930UF-A |
| 246-HAC3980UF-ACT-ND,246-HAC3980UF-ADKR-ND,246-HAC3980UF-ATR-ND | HAC3980UF-A |
| 620-A33003LLUBTR-DDCT-ND,620-A33003LLUBTR-DDDKR-ND,620-A33003LLUBTR-DDTR-ND | A33003LLUBTR-DD |
| 1589-MA600GQE-0000-PTR-ND,1589-MA600GQE-0000-PCT-ND,1589-MA600GQE-0000-PDKR-ND | MA600GQE-0000-P |
| TLE5309DE1211XUMA1TR-ND,TLE5309DE1211XUMA1CT-ND,TLE5309DE1211XUMA1DKR-ND | TLE5309DE1211XUMA1 |
| 445-TAS4142-BAACTR-ND,445-TAS4142-BAACCT-ND,445-TAS4142-BAACDKR-ND | TAS4142-BAAC |
| 119-286CC3DAABA1-ND | 286CC3DAABA1 |
| 1993-PST360G2-2OO-C0002-ERA360-RE-ND | PST360G2-2OO-C0002-ERA360-RE |
| 3542-AMR3008-ND | AMR3008 |
| 3542-AMR3013P-ND | AMR3013P |
| 3542-TMR3081TP-ND | TMR3081TP |
| 448-TLE5014SP16E0002XUMA1TR-ND,448-TLE5014SP16E0002XUMA1CT-ND,448-TLE5014SP16E0002XUMA1DKR-ND | TLE5014SP16E0002XUMA1 |
| 1589-MAQ473GQE-AEC1-ZTR-ND,1589-MAQ473GQE-AEC1-ZCT-ND,1589-MAQ473GQE-AEC1-ZDKR-ND | MAQ473GQE-AEC1-Z |
| 620-1767-2-ND,620-1767-1-ND,620-1767-6-ND | A1335LLETR-DD-T |
| 1589-MAQ473GQE-AEC1-PTR-ND,1589-MAQ473GQE-AEC1-PCT-ND,1589-MAQ473GQE-AEC1-PDKR-ND | MAQ473GQE-AEC1-P |
| 3542-TMR4007-ND | TMR4007 |
| 3542-TMR4011-ND | TMR4011 |
| 3542-TMR4M03BG-ND | TMR4M03BG |
| 3542-TMR4M04BG-ND | TMR4M04BG |
| 3542-TMR4M05BG-ND | TMR4M05BG |
| 3542-TMR4M02BG-ND | TMR4M02BG |
| 2266-AN820032-ND,CH202-ND | AN820032 |
| CH161-ND,2266-AN920036-ND | AN920036 |
| CH187-ND | AN820002 |
| 2608-BWL000F-ND | BWL000F |
| 2156-KMZ80J-ND | KMZ80J |
| 5750-iST8210TR-ND | iST8210 |
| 3542-TMR4003-ND | TMR4003 |
| 3542-TMR4013-ND | TMR4013 |
| 3542-TMR4M08BG-ND | TMR4M08BG |
| HAL3726DJ-ATR-ND,HAL3726DJ-ACT-ND,HAL3726DJ-ADKR-ND | HAL3726DJ-A |
| 2190-100080101-01-ND | 100080101-01 |
| 478-9102000020-ND | 9102000020 |
| CH999-ND | ANG-11HAW1 |
| 1993-1013-ND | PST360G2G2-1A-C0007-ERA180-05K |
| 1993-1014-ND | PST360G2-1A-C0011-ERA090-05K |
| 17-V23401-T1079-B101-ND | V23401-T1079-B101 |
| 1993-PSC360G2-F1J-C0000-ERA360-RE-ND | PSC360G2-F1J-C0000-ERA360-RE |
| 480-5605-ND | SPS-A100D-HAWS |
| 4-1393048-6-ND | 4-1393048-6 |
| 480-5691-ND | SPS-A100X-LAAS0401 |
| 1993-1019-ND | PS2P-CON-CE-1A0-C0000-ERA360-05 |
| 1993-1004-ND | PSC360G2-F1A-C0000-ERA360-RE-K |
| 1993-1008-ND | PSC360G2-F1P-C0000-ERA360-05K-200 |
| 1993-1015-ND | PST360G2-1A-C0000-ERA360-RE |
| 478-9168100100-ND | 9168100100 |
| 1993-1017-ND | PST360G2-2AA-C0002-ERA360-05K |
| 2171-SRBS-Q12-12-E270-EP-1-S-M8-ND | SRBS-Q12-12-E270-EP-1-S-M8 |
| 17-V23401-T1071-B101-ND | V23401-T1071-B101 |
| TLE5014P16XUMA1TR-ND,TLE5014P16XUMA1CT-ND,TLE5014P16XUMA1DKR-ND | TLE5014P16XUMA1 |
| AS5172B-HTSMTR-ND,AS5172B-HTSMCT-ND,AS5172B-HTSMDKR-ND | AS5172B-HTSM |
| TLE5014C16DXUMA1TR-ND,TLE5014C16DXUMA1CT-ND,TLE5014C16DXUMA1DKR-ND | TLE5014C16DXUMA1 |
| 1993-PSC360G2-F1A-C0007-ERA180-REK-ND | PSC360G2-F1A-C0007-ERA180-REK |
| 1993-PSE-290-A-ERA270-I-05-ND | PSE-290-A-ERA270-I-05 |
| 1993-PSE-360-A-ERA270-S-05-ND | PSE-360-A-ERA270-S-05 |
| 1993-PSE-360-A-ERA180-S-05-ND | PSE-360-A-ERA180-S-05 |
| 1993-PSE-360-A-ERA120-S-05-ND | PSE-360-A-ERA120-S-05 |
| 1993-PSE-360-A-ERA360-S-05-ND | PSE-360-A-ERA360-S-05 |
| 1993-PSE-360-A-ERA090-S-05-ND | PSE-360-A-ERA090-S-05 |
| 1993-PSC360G2-F1A-C0150-ERA070-05K-ND | PSC360G2-F1A-C0150-ERA070-05K |
| 1993-PSC360G2-F1A-C0208-ERA270-05K-ND | PSC360G2-F1A-C0208-ERA270-05K |
| 1993-PSC360G2-F1A-C0024-ERA120-05K-ND | PSC360G2-F1A-C0024-ERA120-05K |
| 1993-PSC360G2-F1A-C0150-ERA070-REK-ND | PSC360G2-F1A-C0150-ERA070-REK |
| 1993-PSC360G2-F1A-C0208-ERA270-REK-ND | PSC360G2-F1A-C0208-ERA270-REK |
| 1993-PSC360G2-F1A-C0006-ERA060-REK-ND | PSC360G2-F1A-C0006-ERA060-REK |
| 1993-PSC360G2-F1A-C0024-ERA120-REK-ND | PSC360G2-F1A-C0024-ERA120-REK |
| 1993-PST360G2-1A-C0026-ERA040-05K-ND | PST360G2-1A-C0026-ERA040-05K |
| 1993-PST360G2-1A-C0007-ERA180-REK-ND | PST360G2-1A-C0007-ERA180-REK |
| 1993-PSC360G2-F1A-C0011-ERA090-REK-ND | PSC360G2-F1A-C0011-ERA090-REK |
| 374-MFM7-APS090-LACD4-ND | MFM7-APS090-LACD4 |
| 374-MFM7-APS360-LACD4-ND | MFM7-APS360-LACD4 |
| 374-MFM7-APS180-LACD4-ND | MFM7-APS180-LACD4 |
| 374-A63-APS360-LACB1E-ND | A63-APS360-LACB1E |
| 2171-SRBS-Q12-6-E270-EP-1-S-M8-ND | SRBS-Q12-6-E270-EP-1-S-M8 |
| 17-V23401-T2072-B101-ND | V23401-T2072-B101 |
| 1993-MSX360-1A-C0004-ERA360-05K-ND | MSX360-1A-C0004-ERA360-05K |
| 1993-MSX360-1A-C0304-ERA270-05K-ND | MSX360-1A-C0304-ERA270-05K |
| 1993-MSX360-1A-C0022-ERA090-05K-ND | MSX360-1A-C0022-ERA090-05K |
| 1993-MSX360-1A-C0250-ERA180-05K-ND | MSX360-1A-C0250-ERA180-05K |
| 119-286CC3DAAAA1-ND | 286CC3DAAAA1 |
| 1993-PSC360G2-F2OO-C0002-ERA360-RE-ND | PSC360G2-F2OO-C0002-ERA360-RE |
| 1993-PST360G2-2JJ-C0002-ERA360-RE-ND | PST360G2-2JJ-C0002-ERA360-RE |
| 1993-PS2P-ARC-CE-M008-A-45S-05-ND | PS2P-ARC-CE-M008-A-45S-05 |
| 1993-PS2P-ARC-CE-M009-A-45S-05-ND | PS2P-ARC-CE-M009-A-45S-05 |
| 1993-PSCM-A-02S-05-ND | PSCM-A-02S-05 |
| 1993-PSC360G2-F1O-C0000-ERA360-RE-ND | PSC360G2-F1O-C0000-ERA360-RE |
| 1993-PST360G2-1O-C0000-ERA360-RE-ND | PST360G2-1O-C0000-ERA360-RE |
| 1993-PSC360G2-F2JJ-C0002-ERA360-RE-ND | PSC360G2-F2JJ-C0002-ERA360-RE |
| 1993-PST360G2-1J-C0000-ERA360-RE-ND | PST360G2-1J-C0000-ERA360-RE |
| 2-1393047-2-ND,2266-2-1393047-2-ND | 2-1393047-2 |
| 1993-PS2P-ARC-CE-M009-A-110S-05-ND | PS2P-ARC-CE-M009-A-110S-05 |
| 1993-PSCM-A-03S-05-ND | PSCM-A-03S-05 |
| 1993-PSCM-A-10S-05-ND | PSCM-A-10S-05 |
| 1993-PSCM-A-06S-05-ND | PSCM-A-06S-05 |
| 1993-PSCM-A-32S-05-ND | PSCM-A-32S-05 |
| 17-1411006-1-ND | 1411006-1 |
| 2330-OPL200-ND | OPL200 |
| 3542-TMR4001-ND | TMR4001 |
| AS5270A-HMFMTR-ND,AS5270A-HMFMCT-ND,AS5270A-HMFMDKR-ND | AS5270A-HMFM |
| 2608-BWL000R-ND | BWL000R |
| 2608-BWL0019-ND | BWL0019 |
| 2330-MVQ201-ND | MVQ201 |
| CH926-ND | CU103601 |
| 17-V23401-T2071-B101-ND | V23401-T2071-B101 |
| 17-V23401-T2715-B101-ND | V23401-T2715-B101 |
| TLE5109A16E1210XUMA1TR-ND,TLE5109A16E1210XUMA1CT-ND,TLE5109A16E1210XUMA1DKR-ND | TLE5109A16E1210XUMA1 |
| TLE5009A16DE2210XUMA1TR-ND,TLE5009A16DE2210XUMA1CT-ND,TLE5009A16DE2210XUMA1DKR-ND | TLE5009A16DE2210XUMA1 |
| 1589-MA330GQ-PTR-ND,1589-MA330GQ-PCT-ND,1589-MA330GQ-PDKR-ND | MA330GQ-P |
| TLE5309DE2211XUMA1TR-ND,TLE5309DE2211XUMA1CT-ND,TLE5309DE2211XUMA1DKR-ND | TLE5309DE2211XUMA1 |
| 1993-1007-ND | PSC360G2-F1A-C0011-ERA090-05K |
| 1993-PSE-290-A-ERA270-S-05-ND | PSE-290-A-ERA270-S-05 |
| 17-V23401-T2079-B101-ND | V23401-T2079-B101 |
| 17-V23401-T2074-B101-ND | V23401-T2074-B101 |
| 620-CT310LS-IT8TR-ND,620-CT310LS-IT8CT-ND,620-CT310LS-IT8DKR-ND | CT310LS-IT8 |
| 448-TLE49SRI3XTMA1TR-ND,448-TLE49SRI3XTMA1CT-ND | TLE49SRI3XTMA1 |
| 448-TLE49SRP3XTMA1TR-ND,448-TLE49SRP3XTMA1CT-ND | TLE49SRP3XTMA1 |
| 478-4115302470-ND | 4115302470 |
| 1790-IQS7221E101QFRTR-ND | IQS7221E101QFR |
| 1790-IQS7221E001QNR-ND | IQS7221E001QNR |
| X3G-OH048,005-ND | X3G-OH048,005 |
| X3G-OH047,005-ND | X3G-OH047,005 |
| A1330LLETR-P-T-ND | A1330LLETR-P-T |
| 620-A1330LLETR-T-C02TR-ND | A1330LLETR-T-C02 |
| 246-HAL830PUT-A-ND | HAL830PUT-A |
| MA820GQ-Z-ND | MA820GQ-Z |
| MA850GQ-Z-ND | MA850GQ-Z |
| 246-HAL835PUT-A-ND | HAL835PUT-A |
| A1338LLETR-T-ND | A1338LLETR-T |
| MA102GQ-Z-ND | MA102GQ-Z |
| 1589-MAQ820GQE-AEC1-ZTR-ND | MAQ820GQE-AEC1-Z |
| 1589-MAQ850GQE-AEC1-ZTR-ND | MAQ850GQE-AEC1-Z |
| 1589-MAQ800GQE-AEC1-ZTR-ND | MAQ800GQE-AEC1-Z |
| 505-ADA4570BRZ-RLTR-ND | ADA4570BRZ-RL |
| 620-A33003LLUATR-125TR-ND | A33003LLUATR-125 |
| 223-G-MRCO-048-ND | G-MRCO-048 |
| A1338LLETR-P-T-ND | A1338LLETR-P-T |
| 505-ADA4570BRZ-R7TR-ND | ADA4570BRZ-R7 |
| MA820GQ-P-ND | MA820GQ-P |
| MA850GQ-P-ND | MA850GQ-P |
| A1330LLETR-P-DD-T-ND | A1330LLETR-P-DD-T |
| 246-HAL3900DJ-2300TR-ND | HAL3900DJ-2300 |
| 356-1082-5-ND | G-MRCO-015 |
| 505-ADA4570WHRZ-RLTR-ND | ADA4570WHRZ-RL |
| 246-HAC3736UF-A-ND | HAC3736UF-A |
| 246-HAC3737UF-A-ND | HAC3737UF-A |
| 246-HAC3727UF-A-ND | HAC3727UF-A |
| TLE5009A16E2200XUMA1-ND | TLE5009A16E2200XUMA1 |
| 246-HAL3930DJ-2300TR-ND | HAL3930DJ-2300 |
| 246-HAL3980DJ-2300TR-ND | HAL3980DJ-2300 |
| AAS33051LLEATR-ND | AAS33051LLEATR |
| 246-HAL3960DJ-2300TR-ND | HAL3960DJ-2300 |
| HAL3725UP-A-ND | HAL3725UP-A |
| HAL3726UP-A-ND | HAL3726UP-A |
| HAL3727UP-A-ND | HAL3727UP-A |
| HAL3735UP-A-ND | HAL3735UP-A |
| HAL3736UP-A-ND | HAL3736UP-A |
| HAL3737UP-A-ND | HAL3737UP-A |
| MA102GQ-P-ND | MA102GQ-P |
| A1333LLPTR-DD-T-ND | A1333LLPTR-DD-T |
| A1339LLETR-5-T-ND | A1339LLETR-5-T |
| A1339LLETR-T-ND | A1339LLETR-T |
| AS5170A-HSOT-ND | AS5170A-HSOT |
| AAS33001LLPBTR-DD-ND | AAS33001LLPBTR-DD |
| 620-AAS33001LLPBTR-5-DD-ND | AAS33001LLPBTR-5-DD |
| 620-AAS33051LLEATR-5TR-ND | AAS33051LLEATR-5 |
| 620-A33003LLUBTR-DD-125-ND | A33003LLUBTR-DD-125 |
| 246-HAR3736DJ-A-ND | HAR3736DJ-A |
| 246-HAR3737DJ-A-ND | HAR3737DJ-A |
| 246-HAR3727DJ-A-ND | HAR3727DJ-A |
| 246-HAR3726DJ-A-ND | HAR3726DJ-A |
| 1589-MA600GQE-0000-ZTR-ND | MA600GQE-0000-Z |
| 568-KMA321/AZTR-ND | KMA321/AZ |
| 390-ASR012-10E-ND | ASR012-10E |
| 390-ASR022-10E-ND | ASR022-10E |
| HAL3735DJ-ATR-ND,HAL3735DJ-ACT-ND,HAL3735DJ-ADKR-ND | HAL3735DJ-A |
| 4991-AS5055A-BQFTQFN16LFT&RDPTR-ND | AS5055A-BQFT QFN16 LF T&RDP |
| 1589-MAQ470GQE-AEC1-PTR-ND | MAQ470GQE-AEC1-P |
| 568-KMA310/AZTR-ND | KMA310/AZ |
| 246-HAR3927DJ-4301TR-ND | HAR3927DJ-4301 |
| AAS33051LLPBTR-DD-ND | AAS33051LLPBTR-DD |
| 356-1081-1-ND | G-MRCO-014 |
| 1589-MAQ430GQE-AEC1-PTR-ND | MAQ430GQE-AEC1-P |
| 246-HAR3930GU-2300TR-ND | HAR3930GU-2300 |
| A1339LLPTR-DD-T-ND | A1339LLPTR-DD-T |
| 620-A1339LLPTR-5-DD-TTR-ND | A1339LLPTR-5-DD-T |
| 356-1084-2-ND,356-1084-1-ND,356-1084-6-ND | G-MRCO-021 |
| 620-AAS33051LLPBTR-5-DDTR-ND | AAS33051LLPBTR-5-DD |
| MLX90366LVS-ADU-250-RE-ND | MLX90366LVS-ADU-250-RE |
| MLX90366LVS-ADU-253-RE-ND | MLX90366LVS-ADU-253-RE |
| 568-KMA320/AZTR-ND | KMA320/AZ |
| AS5270A-HMFT-ND | AS5270A-HMFT |
| AS5270B-HMFM-ND | AS5270B-HMFM |
| AS5270B-HMFT-ND | AS5270B-HMFT |
| AS5161-HSOPTR-ND | AS5161-HSOP |
| AS5162-HSOPTR-ND | AS5162-HSOP |
| AS5170A-HSOMCT-ND,AS5170A-HSOMDKR-ND | AS5170A-HSOM |
| AS5170B-HSOMTR-ND,AS5170B-HSOMCT-ND,AS5170B-HSOMDKR-ND | AS5170B-HSOM |
| 1833-ZMID4200AI1RTR-ND | ZMID4200AI1R |
| 1589-MA780GQ-PTR-ND,1589-MA780GQ-PCT-ND,1589-MA780GQ-PDKR-ND | MA780GQ-P |
| MLX90366LVS-ADU-250-SP-ND | MLX90366LVS-ADU-250-SP |
| MLX90366LVS-ADU-253-SP-ND | MLX90366LVS-ADU-253-SP |
| TLE5109A16DE1210XUMA1TR-ND,TLE5109A16DE1210XUMA1CT-ND,TLE5109A16DE1210XUMA1DKR-ND | TLE5109A16DE1210XUMA1 |
| AS5261-HMFPTR-ND | AS5261-HMFP |
| AS5262-HMFPTR-ND | AS5262-HMFP |
| 4991-AS5715R-ZTSTTR-ND,4991-AS5715R-ZTSTCT-ND,4991-AS5715R-ZTSTDKR-ND | AS5715R-ZTST TSSOP14 LF T&RDP |
| AS5161-HSOMTR-ND,AS5161-HSOMCT-ND,AS5161-HSOMDKR-ND | AS5161-HSOM |
| AS5261-HMFMTR-ND,AS5261-HMFMCT-ND,AS5261-HMFMDKR-ND | AS5261-HMFM |
| AS5262-HMFMTR-ND,AS5262-HMFMCT-ND,AS5262-HMFMDKR-ND | AS5262-HMFM |
| CH163-ND | AN820001 |
| CH200-ND | AN820031 |
| CH203-ND | AN920031 |
| CH204-ND | AN920032 |
| CH928-ND | CU103603 |
| 716-ECS78RBB502-ND | ECS78RBB502 |
| 480-SC2CC1A103W007-ND | SC2CC1A103W007 |
| 716-981HE0A1WA8H01-ND | 981HE0A1WA8H01 |
| 716-981HE0A2WA8H01-ND | 981HE0A2WA8H01 |
| 716-981HE0A5WA8H01-ND | 981HE0A5WA8H01 |
| 716-981HE0A1WD8H01-ND | 981HE0A1WD8H01 |
| 716-981HE2A5WB8H00-ND | 981HE2A5WB8H00 |
| 716-981HE3A1WA8H01-ND | 981HE3A1WA8H01 |
| 1724-9800-697-1-ND | 9800-697-1 |
| 716-981HE2B1WA8H01-ND | 981HE2B1WA8H01 |
| 716-981HE2B5WA8H00-ND | 981HE2B5WA8H00 |
| 716-981HE3B5WA8H01-ND | 981HE3B5WA8H01 |
| 716-981HE3B1WB8H01-ND | 981HE3B1WB8H01 |
| 716-981HE2B5WA8H01-ND | 981HE2B5WA8H01 |
| 716-981HE2B5WB8H01-ND | 981HE2B5WB8H01 |
| 716-981HE0A5WC1F16-ND | 981HE0A5WC1F16 |
| 716-981HE0A1WA1F16-ND | 981HE0A1WA1F16 |
| 716-981HE0A2WD1F16-ND | 981HE0A2WD1F16 |
| 716-981HE0A3WA1F16-ND | 981HE0A3WA1F16 |
| 716-981HE0A2WA1F16-ND | 981HE0A2WA1F16 |
| 716-981HE0A2WC1F16-ND | 981HE0A2WC1F16 |
| 716-981HE0A5WB1F16-ND | 981HE0A5WB1F16 |
| 716-981HE0A1WB1F16-ND | 981HE0A1WB1F16 |
| 716-981HE2A5WB1F16-ND | 981HE2A5WB1F16 |
| 716-981HE2B5WA1F16-ND | 981HE2B5WA1F16 |
| 716-981HE2B1WB1F16-ND | 981HE2B1WB1F16 |
| 716-981HE3B5WA1F16-ND | 981HE3B5WA1F16 |
| 118-HES38U-RS485-SC2F-ND | HES38U-RS485-SC2F |
| 1882-1113979-ND | 1113979 |
| 2330-OPL201-ND | OPL201 |
| 1724-8360360-ND | 8360360 |
| 2046-PMI360DV-F130-IU-V15-ND | PMI360DV-F130-IU-V15 |
| 2046-PMI360D-F130-IE8-V15-ND | PMI360D-F130-IE8-V15 |
| 2046-PMI360DV-F130-3E2-V15-ND | PMI360DV-F130-3E2-V15 |
| 2046-PMI360DV-F130-IU2E2-V15-ND | PMI360DV-F130-IU2E2-V15 |
| 2046-PMI90DV-F130-I2E2-V15-ND | PMI90DV-F130-I2E2-V15 |
| 480-3331-ND | SPS-A180D-HAMS |
| 2266-SPS-A100D-HAMS-ND,480-3329-ND | SPS-A100D-HAMS |
| 480-3332-ND | SPS-A180D-VAMS |
| 480-D30P12XGASNTB-ND | D30P12XGASNTB |
| 480-D30D12XGASNTB-ND | D30D12XGASNTB |
| 3542-AMR4100-ND | AMR4100 |
| 568-KMA310/ATR-ND | KMA310/A |
| 568-KMA320/ATR-ND | KMA320/A |
| 568-KMA210/ATR-ND | KMA210/A |
| 568-KMZ49/AJTR-ND | KMZ49/AJ |
| 3542-TMR3105AP-ND | TMR3105AP |
| 1589-MA600GQ-ZTR-ND | MA600GQ-Z |