We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
The Quad serves as a small NAS serving media from an HDD connected to the SATA port to a Squeezebox Touch and to my desktop computer. As I say it was working fine, but suddenly it began refusing all connections (it does respond to a ping with no problem). Until now I have been connecting to the board using SSH from my desktop computer. The last thing I was able to do, as I recall, was to change the Locale from the default “C” to EN-US-utf8. But now every time I try to connect I get the “Connection refused” message. To me this implies that the board has booted.
So I tried connecting the board to a monitor via the HDMI port and plugging in a keyboard via the USB port. When I power on the Quad, I get the Wandboard.org logo on the screen, but after that nothing except a flashing HDMI port icon and then a “No Signal” message from the monitor. The keyboard seems to be responding, because when I hit Ctrl-Alt-Delete the board restarts and I see the Wandboard logo again, but after that “No Signal” again.
Any suggestions as to how I can troubleshoot would be appreciated. I’m ready to provide any information anyone might need.
I wouldn’t expect that change to break that either.
Can you login over serial console?
The original Wandboard quad’s has a bug in the EDID hardware circuit, you need to modify your boot arguments to append a your selected video resolution. Something like:
cmdline=video=HDMI-A-1:1024x768@60e
or
cmdline=video=HDMI-A-1:1920x1080@60e
Is what i recommend for my Debian instructions, but for ARCH it’s probably similar but different. It also helps, if your monitor has a built-in usb hub, to connect that directly to the Wandboard to help share the GND plane between both devices.
Thanks! No, I haven’t tried to connect via the serial port. Is there an advantage to that? Would it bypass the problem connecting via HDMI?
As I mentioned, the board was working when it was operating headless just as a server.
I can plug the card in with an SD card reader and make changes via my Linux desktop PC. Is there a setting I can change that way to make the video work?
@Lestrad, you should be able to login over serial, it’ll be the same experience as ssh, so you should be able to login into the system.
Sadly, I mostly support Debian on these SBC’s, so no personal experience with ARCH, but it should have a configuration file u-boot loads on bootup, where you could set the video parameters. If you plug in a serial adapter, you should see u-boot either load-up something, or allow you to override the bootargs.
Thanks a million. I’ve had so many problems with Arch that I was contemplating switching to Debian. Also, help is simply not forthcoming from the Arch and Arch-ARM forums, although I’ve struggled to do the homework and try to ask informed questions (and to be forthcoming with help where I can). As for the Wandboard forum, it seems to be pretty much a ghost town, except for the fact that it’s full of spam. (In fairness, Wand was supposed to be a volunteer project.) Anyway you, Sir, are truly a godsend.
I have a USB->null modem cable on order. I’ll post here as soon as I get it and give it a try.
Meanwhile, any ideas as to what could be refusing connections would be much appreciated.