What are countermeasures to silicone for a basic switch?

Question:

What are countermeasures to silicone for a basic switch?

Block

Answer:

As stated in the catalog, we do not recommend using the products in an atmosphere with silicone gas. Unless you remove the silicone gas from the environment, it is difficult to eliminate the problem for switches with contacts.

Block

Explanation:

When electrical switching is performed in an atmosphere with silicone gas, silicon dioxide may accumluate on the contacts and cause contact failure. An oxide silicon is generated on contact surface when a gas released from a silicone based materials existing around switch reacts to ark heat at load switching. The followings are examples of a source of generating a silicone gas.

  • Silicone based coating agents
  • Slicone based adhesive
  • Silicone rubber
  • Silicone oil/grease
  • Silicone based mold lubricant
  • Silicone filler
  • Silicone wire, etc.

If there is a source of generating a silicone gas, be sure to eliminate the source around the switch or change to the other materials.
Silicone based mold lubricant in die may be used in molding, so make sure not to use it. In addition, if using under environment where a source of generating a silicone gas exists, be sure to implement the periodical check or replacement.

We have D2QW and D2AW basic switches with sliding contacts. They are only for a microload type, but silicon dioxide can be removed to some extent by the sliding contacts. The evaluatation with your actual equipment must be performed.

Block

Quick tips

Please refer to the following table for information on electrical switching in environments with silicone gas. There is also a suppression effect depending on switching voltage and current. The evaluatation with your actual equipment must be performed.


Product category

Switches Basic Switches


Classification

Trouble shootings


Related keywords

Basic Switch
Atmosphere with Silicone Gas
Oxide Silicon
Contact Failure
Ark Heat
Source of Generating of Silicone Gas
Silicone Based Mold
Lubricant

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20043