What are the differences between soldering terminals and #187 tab terminals for a basic switch?

Question:

What are the differences between soldering terminals and #187 tab terminals for a basic switch?

Block

Answer:

Soldering terminals and #187 tab terminals have the same outline and can be connected to #187 connectors. However, if the product requires conformity to the safety standards, do not use the soldering terminal as a #187 tab; otherwise the product cannot be guaranteed for the safety standards. The hole shape of the soldering terminal is not approved as a tab terminal according to the safety sta

Block

Explanation:

The soldering terminals of our V type basic switch have a “keyhole” shape, which combines the 2 holes of φ2.4 mm for easy insertion of lead wires and φ1.6 mm for the #187 connector. As a result, both soldering terminals can be connected, and the solder can flow easily with silver plating.

Block

Product category

Switches Basic Switches


Classification

Trouble shootings


Related keywords

Basic Switch
Soldering Terminal
#187 Tab
#187 Connector
V Type Basic Switch

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20044