Hi, I’m needing in some help in finding what exact chip to replace this with. It’s 0.1 Ohm.
Hello tech18,
Without knowing what the physical size is, Click here for all the 0.1 ohm (100mOhm) resistors, that we have available. If you can measure the size, that will help to narrow down the choices.
Hi David, it is 6.9 X 3.3 mm. Thank you for the help! Any one that’s more specific come to mind, now with these measurements?
tech18,
I would look at CSR2512JTR100CT-ND, which is 6.40mm X 3.20mm, 100 mOhms (0.1 ohms), 2W, 5%.