What is AEC-Q200 Automotive Grade?

As an added note for a related Frequently Asked Question, we often get asked what the difference is between a part that has AEC Qualifications and one that doesn’t. Since the temperature range and all the other important specifications tend to be the same, the only difference is simply that the AEC qualified component has certification saying it was tested a specific way according to the standard number referenced (example: AEC-Q200 and AEC-Q100).