Got a Chefman air fryer for Christmas that displayed an ‘E1’ error. Chefman support was great and sent a replacement, but they let me keep the old on. Upon opening, I found a cable that appears to have a flex open. The cable is between 6"-8", and has the below connector on each side of the cable. Can anyone help me identify this connector, and maybe I can end up with 2 Chefman air fryer’s n_n;
Hello usfcollegeguy ,
A103944-ND is the closest option found, unfortunately it looks like there are some differences however. Another technician may be able to provide a better solution and add to this thread.