We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I setting up a home theatre room which will be a reading room in the day.
Since Tunable white led’s mix warm and a cool white color channels to create different kelvin light, ive noticed there is some “Bleed” where the partially unmixed parts of light can be visible, when reflected on a floor or wall.
Is a more uniform light produced if the mix of warm and cool temperature range is smaller?
IE a 2700+5000K CCT White Led will produce more uniform light than a 2700+6500 CCT Led?
A smaller temperature range like 2700K + 5000K should indeed produce a more uniform light compared to 2700K + 6500K. It’s all about minimizing that “bleed” effect. So go for the one with a closer match in temperatures for a smoother overall lighting experience in your home theater/reading room.
The “bleed” effect one might encounter with tunable light fixtures isn’t really a function of the CCT spread of the emitters used, so much as it’s a result of geometry and the fact that the two emitters are physically separate. Reducing the distance between them is the primary means by which one would go about reducing it.