Description
This project sets up a Seeed Wio Terminal to read it’s internal light sensor, show and graph the data on it’s LCD display and post the data to machinechat’s JEDI One IoT data platform. Arduino is used to implement the Wio Terminal application and JEDI One is installed and running on a Raspberry Pi 4.
Hardware
- RASPBERRY PI 4B/4GB
Raspberry PI 4 Model B with 4GB SDRAM - Seeed Wio Terminal
SAMD51-based Evaluation Platform with WiFi/LCD/Sensors
Software
- JEDI One
JEDI One is a ready-to-use IoT data management software solution. Capabilities include: collect data from sensors, devices and machines; build intuitive real-time and historical data and system view dashboards; create rules to monitor and respond to data conditions automatically; receive alert notifications by email and SMS. - Arduino
Arduino is an open-source electronics platform based on easy-to-use hardware and software.
Implementation
Wio Terminal is a standalone Arduino/MicroPython compatible SAMD51-based microcontroller evaluation platform with WiFi/Bluetooth powered by a Realtek RTL8720DN. It is equipped with a 2.4” LCD Screen, onboard IMU(LIS3DHTR), Microphone, Buzzer, microSD card slot, Light sensor, and Infrared Emitter(IR 940nm). For this project, Arduino is used to implement a simple IoT sensor that reads the internal light sensor, displays and graphs the sensor data on the Wio Terminal’s integrated LCD display and HTTP posts the data to machinechat’s JEDI One IoT data platform. JEDI One is configured to display the light sensor data on the Sensor Dashboard.
Set up the Wio Terminal platform for the Arduino application
1 - Set up Arduino on the Wio Terminal. See link Getting started with Wio Terminal
note: make sure Realtek RTL8720DN firmware is updated per Update the Wireless Core Firmware
2 - Install libraries needed for application. Add these libraries thru Arduino’s Library Manager:
- Adafruit Zero DMA
- Seeed_Arduino_Linechart
- ArduinoJson
Libraries needed for WiFi - Seeed_Arduino_rpcWiFi
- Seeed_Arduino_rpcUnified
- Seeed_Arduino_mbedtls
- Seeed_Arduino_FS
- Seeed_Arduino_SFUD
note: add “Free_Fonts.h” and “arduino_secrets.h” files to project directory (Free_Fonts.h is located in ~/Arduino/libraries/Seeed_LCD_master/examples/320 x 240/All_Free_Fonts_Demo)
3 - Code walkthrough (filename: WioTerminalLightSensorGraphWiFi.ino)
Initial setup and connect to Wifi network
#include <rpcWiFi.h>
#include <HTTPClient.h>
#include "arduino_secrets.h"
#include <ArduinoJson.h>
#include"seeed_line_chart.h" //include the library
#include"TFT_eSPI.h"
#include"Free_Fonts.h" //include the header file
TFT_eSPI tft;
// for LCD line chart
#define max_size 50 //maximum size of data
doubles data; //Initilising a doubles type to store data
TFT_eSprite spr = TFT_eSprite(&tft); // Sprite
// Create a unique ID for the data from Wio Terminal running this code
const char* jediID = "WioTerminalLightSensor";
///////please enter your sensitive data in the Secret tab/arduino_secrets.h
char ssid[] = SECRET_SSID; // your network SSID (name)
char password[] = SECRET_PASS; // your network password (use for WPA, or use as key for WEP)
// Change the following IP to your computer's IP running the server, make sure the Port also match
// IP address of server or Raspberry Pi running Machinechat JEDI software
// If you changed the JEDI port number, replace 8100 with the new port
const char* yourLocalIp = "http://192.168.1.7:8100/v1/data/mc";
void setup() {
tft.begin();
tft.setRotation(3);
tft.fillScreen(TFT_WHITE); //Black background
spr.createSprite(320,120); //try half screen
tft.setFreeFont(FF19); //select font
tft.setTextColor(TFT_BLACK);
tft.drawString("Light Sensor",10,120);//prints string at (10,10)
pinMode(WIO_LIGHT, INPUT); //Wio Terminal internal light sensor
Serial.begin(115200);
WiFi.begin(ssid, password);
while (WiFi.status() != WL_CONNECTED) { //Check for the connection
delay(500);
Serial.println("Connecting..");
}
Serial.print("Connected to the WiFi network with IP: ");
Serial.println(WiFi.localIP());
}
Display /chart light sensor on LCD display and set up sensor data in JSON format and send to JEDI One using HTTP post
void loop() {
//prep for sending HTTP to JEDI One
String postData1; //Json string
tft.setFreeFont(FF24); //select font
tft.setTextColor(TFT_RED);
int light = analogRead(WIO_LIGHT);
char value[7] = " ";
Serial.print("Light value: "); //debug, can be commented out
Serial.println(light);
itoa(light,value,10); //convert light sensor integer value to character
tft.drawString(value,60,170);//prints data at (x,y)
spr.fillSprite(TFT_WHITE);
if (data.size() == max_size) {
data.pop();//this is used to remove the first read variable
}
data.push(1.0 * light); //read variables and store in data
//Settings for the line graph
auto content = line_chart(20, 10); //(x,y) where the line graph begins
content
.height(tft.height() - 140) //header.height() * 1.5) //actual height of the line chart
.width(tft.width() - content.x() * 2) //actual width of the line chart
.based_on(0.0) //Starting point of y-axis, must be a float
.show_circle(false) //drawing a cirle at each point, default is on.
.value(data) //passing through the data to line graph
.color(TFT_PURPLE) //Setting the color for the line
.draw();
spr.pushSprite(0, 0);
//Following code creates the serialized JSON string to send to JEDI One
//using ArduinoJson library
StaticJsonDocument <200> doc;
JsonObject context = doc.createNestedObject("context");
context["target_id"] = String(jediID);
JsonObject data = doc.createNestedObject("data");
data["lightSen"] = light;
serializeJson(doc, postData1);
Serial.println(postData1); //debug, can be commented out
// http post code
if(WiFi.status()== WL_CONNECTED){ //Check WiFi connection status
HTTPClient http;
http.begin(yourLocalIp); //Specify destination for HTTP request
http.addHeader("Content-Type", "application/json"); //Specify content-type header
int httpResponseCode = http.POST(postData1); //Send the actual POST request
if(httpResponseCode>0){
Serial.print("HTTP Response Code: ");
Serial.println(httpResponseCode); //Print return code
}else{
Serial.print("Error on sending request: ");
Serial.println(httpResponseCode);
}
http.end(); //Free resources
}else{
Serial.println("Error in WiFi connection");
}
delay(5000);
tft.setTextColor(TFT_WHITE); //"clear" old light sensor data value
tft.drawString(value,60,170);
}
4 - Latest source code for the WioTerminalLightSensorGraphWiFi.ino application is on github at below link:
Set up the JEDI One
1 - If machinechat JEDI One is not already installed on the Raspberry Pi see below:
- Get Raspberry Pi version of JEDI One DK-JEDIONE-RP
- Install on Pi, see Raspberry Pi - Installing JEDI One as a Service
2 - Set up the JEDI One dasboard
In the JEDI One, select “Dashboards” tab, then select “+” to add a new chart and configure.
Name the chart, select “Chart Type”, select “Source” (WioTerminalLightSensor), select "Property (lightSen), and enter “Refresh Interval”. When complete the dashboard should liook similar to below.
Conclusion
Seeed’s Wio Terminal makes it easy to implement a low cost full color graphical sensor display. The built-in WiFi provides additionally capability to send and receive information over a WiFi network. Using WiFi, the sensor data can easily be sent to machinechat’s JEDI One IoT data management software for additional processing, alerts or other actions.
References
- Seeed - Wio Terminal Product Page
- Seeed - Wio Terminal Wiki
- Seeed - Wio Terminal LCD Linecharts
- Seeed - Wio Terminal LCD Fonts
- Getting Started with machinechat’s JEDI One IoT Platform