X01-T1 Discontinued Limit Switch

Hello All,

I’ve been hunting for a replacement to a discontinued limit switch that we’ve had requested, the model number is X01-T1, and it was produced by a company called Miltac. As a side note, sometimes folks misspell it as Xo1-T1 due to the way the label is printed.

At time of writing it seems we don’t carry any viable alternates, but maybe this will help someone looking up this topic in the future. I’ve seen it misidentified before as a “T85 5E4” again because of the markings, but this is a temperature rating code and unrelated to the model number or series designation. It is SPST, rated for max voltage/current of 380VAC/20A (though some lots seem to be rated 400VAC), 85 degrees C max temperature, with a roller lever and two screw terminals or lugs for the wire termination. This was all the technical information I could find in terms of specifications on this switch.

Typo on my part, thanks for pointing that out. Fixed in the original post.