I have a DC Electronic Load 8602, the two knobs on the front don’t have an opening to put a banana plug in it. Which parts on DigiKey can I purchase to modify this be insert banana plugs?
Greetings,
I suspect that the 8602 is not provisioned with banana plugs because the ratings/capabilities of that interconnect style was thought marginal relative to the unit’s operational range.
That said, a set of semi-permanent adapter leads made from some free-hanging banana jacks and ring terminals of a suitable size might be a reasonable answer for using the unit in a banana-friendly environment. Some suggested test lead materials can be found here if cordage is also needed.