Hi Everyone I have 4 x Beolab 3 speakers from Europe. In the service manual and other blogs you can convert these speakers to 110v by adding this jumper 1722-1489-ND. There are no B&O stores for a thousand km from here. Is installing a jumper something that I might be able to do myself? I have a multimeter and have a basic knowledge of electronics and wiring? Thank you Fred
Hell Fred,
Thank you for contacting DigiKey Technical support and using our forum.
I would consider installing jumper wires an easy electronics project.
PN 1722-1489-ND went in as a board spacer not a jumper wire.
Do you know the wire awg of the jumper wire you need?
How do you attach the jumper wire to your device?
Incorrect: that DigiKey part number simply happens to look like the OEM P/N mentioned by the manual.
A suitable alternative would likely be found in the Shunts and Jumpers family.
Found a picture of the power supply board.
Looks like you have what is probably a 0.1inch spaced male header (2.54mm)
If it is 2.54mm, something like this should work for that:
You want the jumper installed if you’re using this in the US, Canada, Japan, or anywhere else that uses 100 to 120VAC