Bezel/Frame for C&K switch

I need a frame/Bezel for my C&K 7201J90ZGE2 switches
digikey nr [CKN9947-ND]

Which should fit?

The panel thickness will determine the bezel. Please see the two options below.

CKN12249-ND

CKN1744-ND

Thanks.

My problem is that I’m changing front plate and the new one have a cut out for a bezel not the old one.

Will the bezel you recomended slide onto the old switch?



Picture nr 2 is the new front plate but I’m holding it 180 degres to be able to show the cut out:)

The switch is fully seated in the plate as seen in photo 3. There is no room for the bezel to fit on the switch.

ok. but if I extend the original cut out the bezel would fit?

Or is it another part that will do the job?
I need some sort of frame part to hide the switch seating as the new front plate has a bigger cut out

Here is the mounting hole diagram for the bezel panel cutout and the cutout for the switch.

The holes size increase is 0.1 and 0.2 mm for the bezel to be added to the panel around the switch. You will have the make the choice of increasing the hole size, or manage without a bezel.

Hello dagbadd,

You may have to try both the bezels that are recommended, and they may have to be modified to fit tight with the other panel. You may be able to trim off the latches, and attach the bezel with a double sided VHB tape, like 1067-F9460PCSQ-12(6)-ND or 1067-4646SQ-1(5)-ND.
You may be able to also attach it with some type of epoxy.