Cameras

This Product Selection Guide contains information to help select products in the Cameras category on DigiKey.com

A Camera is optical equipment that produces digital images or record moving images saved to an SD card. The camera types are CCD 1/1.8”, CCD ½”, CCD 1/3”, CMOS ½’, CMOS 1/2.5”, CMOS 1/2.8”, CMOS 1/3”, and CMOS ¼” with a megapixels of 0.9, 1.3, 1.4, 1.5, 2, 3, 3.1, 3.3, and 5 and frames per second being 5, 6, 11, 12, 15, 28, 30, 45, or 60.


SelectionCharacteristics

Camera Type: Relates information describing a device’s image sensor as provided by the manufacturer. May include output resolution, optical format, and the sensor technology used.

Megapixels: The image resolution of the camera sensor, expressed as a total number of sensor elements divided by a factor of one million.

Resolution: The level of detail captured by the camera, typically measured in terms of number of pixels.

Frames per Second: Indicates the maximum number of still images per second that a camera is capable of transferring in video mode.

Interface: Indication of which interface(s) or protocol(s) are used by the device to communicate with other components in the system.

ProductExamples
Image

MFR PART # 26700-218
DIGIKEY PART # 243-26700-218-ND
MANUFACTURER Aven Tools
DESCRIPTION Optical Inspection Camera CMOS 1/2.8" 1920 x 1080 HDMI, USB 2.0
DATASHEET Click Here

Image

MFR PART # 26100-259
DIGIKEY PART # 243-26100-259-ND
MANUFACTURER Aven Tools
DESCRIPTION Optical Inspection Camera 2592 x 1944 HDMI, USB
DATASHEET Click Here

Image

MFR PART # FIT0819
DIGIKEY PART # 1738-FIT0819-ND
MANUFACTURER DFRobot
DESCRIPTION Optical Inspection Camera 1280 x 720 Micro USB, USB, USB C

If you have any general questions on the specifications for selecting Cameras, please reply using the button below. If you have questions on specific Cameras please post those questions in the Automation and Control category.