We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I tried to create the simplest block diagram using two Counters. Connecting one to the other with a line yields a curve and an end arrow is impossible to use.
The reason is the connection points are not lined up between left and right hand sides of the Counter and other symbols. Please can you correct these please?
Are you using a custom symbol or a symbol found in the System Blocks menu? If you are using the latter, there is an option to change the endpoints and line path of your connection in the line properties tab of the right menu. This is available when the line is selected.
Your suggestion does improve the arrow orientation but I still don’t get a straight line plus I have to do this for every line I draw. The route cause remains.
@kier Thanks for pointing this out, now I can see that the connection points are slightly offset. 2 workarounds you can use in the meantime:
use the center yellow arrow. This will give you a straight connection from one to the other without utilizing the individual connection points.
Flip one of the symbols horizontally. This can be done by right-clicking the symbol or by using the shortcut “H”. this will mirror the symbol and align the individual connection points.