Hi @alex_lee and welcome to the forum!
According to a few electrolytic cap datasheets - it appears a standard would be to have the middle line be a capacitance value. So I would venture to say that those caps could potentially be 27uF / 80V and 68 uF / 35V respectively.
Here’s a 27uF / 100V option: 10-EEE-FN2A270UVCT-ND - You can see it here:
And for the 68uF / 35V: 493-2289-1-ND - You can see it here:
I’d recommend taking a micrometer and measuring the footprints to make sure these two options would fit the pads on the PCB prior to ordering. Its always good practice too to check over the specs on the parts I recommended to make sure it will work for your application.
Regards,
Lindsay
Lindsay Foy
Senior Applications Engineering Technician
Applications Engineering
DIGIKEY ELECTRONICS