I am trying to identify the DigiKey part numbers for a few capacitors that I need to order. Two of the capacitors are marked ‘220 HHB KN6’. I “think” this is a Panasonic capacitor with a Panasonic part # EEEHBH221UAP, but could use some confirmation. The third capacitor is marked ‘E69N 47 10V’. Also, when eventually ordering I don’t understand the difference between ordering ‘Cut Tape’ vs ‘Digi-Reel’. Any clarification there would be appreciated. Thank you for any help!
Hi @matticulous ,
Welcome to DigiKey TechForum and thanks for your inquiry.
According to the marking “220 HHB KN6” you provided, it apperas to be the part number EEE-HBH221UAP for Panasonic HB series Aluminum Electrolytic Capacitor.
Unfortunately, I can’t identify the part number marked as “E69N 47 10V”.
It appears to be a 47uF and 10V capacitor. Here are some 47uF and 10V Aluminum Electrolytic Capacitors for your refereence:
Aluminum Electrolytic Capacitors | Electronic Components Distributor DigiKey
It would be very helpful if you could provide more information for us to verify.
For the difference between the Cut Tape and Digi-Reel packaging, please refer to the following post:
What do the DigiKey suffixes TR, CT, DKR, and ND mean?
@Angus_Lai Thank you for your response. This is a picture of the capacitor in question (blue markings). It looks to have a diameter of 5.22mm and is ~5.9mm tall.
Since I will be ordering very small quantities, it sounds like I should be ordering CT packaging, correct?
Hello matticulous
Here is a link to options which are in stock for 5mm diameter, 47uf, 10V.
If you are ordering in small quantities, cut tape packaging would be correct option.