I am replacing some capacitors in an older Viking sewing machine. i have figured out all but three, and here are questions i have about them.
Picture 1: this is labelled 220uM. I assume this means 220 microfarads but what does the M signify? Is this referring to the tolerance?
Picture 2: this is labelled 200G. if i understand correctly, this means 20 picofarads, with the G meaning a tolerance of 2%. is this correct? if so, i only find replacements with a tolerance of 5%. is it OK to use a capacitor with 5% tolerance to replace a capacitor with 2% tolerance?
Picture 3: this is labelled 4u7. does this mean 4.7 or 47 microfarads (or something different)?
thanks!