Capacitor

We are looking for a booklet of ceramic capacitors in the 0.1 pF to 1 pF range, with increments of 0.01 pF (e.g., 0.2 pF, 0.21 pF, etc.). The capacitors should be in 0402 size. Can you help us find these?

@Ranjitha

I see options that have the ~ 0.1 to 1pf range. But I did not see an option with the 0.01pf stepping.
An example item found.

The requested 0.01pF value increment is smaller than the tolerances available for capacitors in that value range, and of the same order as the capacitance introduced by the mounting pads for an 0402-sized device.

A device assortment of the kind requested is very unlikely to be found for sale for these reasons.

1 Like

Makes sense. Thank you!