Chip on Glass Graphic Display Driver with Lattice MachXO2 (VHDL)

Logic Home

Features

The MachXO2 breakout board is a low cost programmable logic device (PLD) development board. The MachXO2 is a low power FPGA with a hardened, ASIC-gate based, embedded function block (EFB). It is worth noting that the device used in this design was a 1200ZE device (Digi-Key Part number 220-1298-ND), it has been replaced by a 7000HE device (Digi-Key Part number 220-2625-ND). This design will work with either device. The Newhaven chip on glass display (Digi-Key Part number NHD-C12864LZ-FSW-FBW-3V3-ND) is interfaced through a custom board with a capacitor array to support the display’s on-board charge pump. The display is a 128x64 pixel LCD display with a built-in ST7565R-G controller. The following design topics will be covered:

• Chip on glass (COG) graphic display application introduction and overview
• Instantiation of VHDL modules in a top-level hierarchy as seen in RTL diagram
• Active-HDL Test Bench simulation
• COG display state machine overview

Introduction

This reference design uses the MachXO2 low cost FPGA to drive parallel data and control signals through a custom interface board to a chip on glass graphical display. In many human-machine interface (HMI) applications displays are commonly used to convey system status and user information.

Background

The MachXO2 breakout board is a low-cost and low-power solution for many input and control applications. In this application two state machines are employed to configure the chip on glass display, write commands and data bits to the display, and control the flow of stored data and commands from a data ROM to display and scroll the displayed word “Digi-Key” from the top to the bottom of the display. The display and MachXO2 breakout board can be seen below in figures 1 and 2 with two different display setting, normal and inverted respectively.

Figure 1 – Display Normal Setting

Figure 2 – Display Inverted Setting

The data FSM has states for clearing the display, setting the page and column position and either displaying the image static or continuously scrolling the image. The state flow can be customized by simply changing the flow of the state machine from the current to the next state. For instance to scroll the display, state_next within the write_data state is set to scroll. To display a static image, state_next can be set to static.

The Software required for the design:
• Lattice Diamond Design Software version 2.0.1 with third party software Synplify Pro for Lattice and Active-HDL Lattice Edition.

Application

Building the Circuit

The two state machines are synchronized with a two signal handshake. This keeps the Data_FSM from trying to write to the COG_Parallel_Driver while it is busy. The two signals used in the handshake are “write_en” from the Data_FSM and “busy” from the COG_Parallel_Driver state machine. See Figure 3 below for an RTL diagram. The hand shake can be seen in simulation below in Figure 4.

Figure 3 – RTL diagram for Chip on Glass Display Driver

Figure 4 – Two Signal Handshake for Synchronization

The test-bench for the simulation is included. The clock period can be varied within the test-bench file. The on-chip oscillator is not simulated; some signals in the top level file need to be un/commented for simulation. Refer to the commented ports, signals, instantiations and continuous assignments within the Chip_on_Glass_Top file for guidance. The design hierarchy can be seen below in Figure 5.

Figure 5 – Chip on Glass Display Driver Design Hierarchy

The state flow diagram for the COG_Parallel_Driver is seen below in Figure 6.

Figure 6 – State Flow Diagram for COG_Parallel_Driver FSM

The first 13 states control the initialization of the display. The initialization states include each of the following:

  • Bias control set to 1/9th bias
  • ADC select set to normal
  • Com output reverse set to normal
  • Display all points set to off
  • Display start line set to X”40”, top line
  • Internal voltage converter set to on
  • Internal voltage regulator set to on
  • Internal voltage follower set to on
  • Built in resistor ratio set to 6
  • Middle of range voltage reference mode set to X”81”
  • Reference voltage resistor set to set to X”09”
  • Display set to reverse (for inverse display setting)
  • Set display to on

After it is initialized the display sits in idle until a “write_en” signal is asserted from the Data_FSM. This will cause the COG_Parallel_Driver FSM to either start a write or command cycle depending on the state of the RegSel signal from the Data_FSM. A simulated output can be seen in figure 7 and 8 below.

Figure 7 – Aldec Testbench Output for Clearing the Screen

Figure 7 shows the page set and column set commands followed by the write signals used to clear each page of the display.

Figure 8 – Aldec Testbench Output for Displaying “Digi-Key”

Figure 8 shows the parallel data stream used to construct the “Digi-Key” word. The Data_FSM can be altered and customized to display multiple lines of data to construct a graphic, or delete specific sections of the delay to prepare for new pixel writes. Additional ROM files can be loaded in the same manner as the existing “Digi-Key” ROM. The pin assignments used in the design can be seen below in Figure 9.

Figure 9 – Pin Assignments for MachXO2

Capabilities, Limitations, and Alterations

Lattice Diamond version 2.0.1 was used to develop this tutorial with supporting software from Synopsis (Synplify Pro for Lattice) and Aldec (Active-HDL Lattice Edition). Diamond can be used as a stand alone development environment with alternative synthesis and simulation software.

Conclusion

This reference design demonstrates how to use the Lattice MachXO2 (PLD) to run a Newhaven Chip on Glass graphic display module. The Data_FSM can easily be modified to drive customized display data using the carefully commented example given.

Additional Information

Further design support, product tutorials, application notes, user’s guides and other documentation can be found on the Lattice website at: Lattice Semiconductor | The Low Power FPGA Leader

Appendix: Downloads

The complete, MachXO2 SPI Peripheral Expansion for HMI Applications, VHDL files can be downloaded here.

COG_Parallel_Driver.vhd (18.6 KB)
Data_FSM.vhd (18.7 KB)
Chip_on_Glass_Top.vhd (6.6 KB)
chip_on_glass_top_tb.vhd (3.5 KB)