Clarification on Dimension Issue – D09P33E4GV00LF

We would like to request your assistance regarding item D09P33E4GV00LF, which we previously purchased from DigiKey. We have observed that its dimensions do not fully align with our drawing specifications. Our engineering team has also noted that the drawing requirement is strict, and the variation (even if slightly wider) does not affect the assembly or functionality of the product.

With this, may we kindly request your support in confirming the following:

  • If there is any explanation or supporting documentation regarding the dimension discrepancy

  • If the current condition is acceptable from the maker’s perspective

12.6 ± 0.1 in drawing

But our sample D09P33E4GV00L is wider than the torelance.

Hello @chihiro,

Thank you for your post.

I have a different drawing for D09P33E4GV00LFwhere I have listed the measurements and tolerances.

Based on the drawing that part number should have the following measurements.

A - 30.81mm with a tolerance of 0.38
B - 24.99mm with a tolerance of 0.12
C - 16.96mm with a tolerance of 0.1
D - 16.79mm with a tolerance of 0.25
E - 10.96mm with a tolerance of 0.07
G - 5.9mm with a tolerance of 0.25

Hello

Thank you for reply.

The dimension we want to confirm is this part.

Our stock is not 12.60 ± 0.12 in this area. Is there any info from Maker ?

Is it acceptable even not within this dimension?

Hello @chihiro,

Thank you for the follow-up.

Other than the drawing you have and the drawing I mentioned, I do not see any other dimensional data that matches the dimensions you are seeing on your pieces.

If that dimension is not matching up with your parts and it is causing an issue with your assembly please contact our Customer Resolution Team through our return process on this link - Returns

Please make sure to include your Invoice or Salesorder number and you can even reference this conversation on the Forum.

Our Customer Resolution Team will work to get those pieces refunded or replaced, whichever you would prefer.