We built dv/dt filter units that incorporate a terminal block in the design. Each unit has six input wires (AWG 6 Cu) from three coils and six stranded wires (AWG 14) that need to be connected. In total, there are 12 input wires (6 bare copper and 6 stranded), but only 6 output spots for customer connections. I need to find a terminal block that allows two conductors per input connection point.
Hello,
Thank you for your post.
It looks like our closest option would be something like more of a standard barrier block.
but they all take up only one conductor in each slot, I am looking to find two conductors in one slot or with a jumper connection./
I believe these are what you are looking for however we do not carry one that will accommodate the 6 AWG wire.
Headers, Plugs and Sockets | Terminal Blocks | Electronic Components Distributor DigiKey
Could you use barrier blocks, like one of these plus one or more of these?
Here are some additional options from our Power Distribution category.