Hi,
I drive five servo motors with an arduino. The arduino is in a main box and the servo motor is 2 meters away. I am looking for a 3 pin low voltage waterproof plug (external) to be able to connect or disconnect the wires of the servo motor to the control box.
Can you help me ?
Look like this one ?
Greetings,
Take a look at 21003515-01 and 21003211-01 as one possibility.
Most environmentally sealed connectors are of a circular format, due to the relative ease of sealing things and making holes in panels in which one would want to mount things. “circular connector” would thus be a good search term if the above suggestion doesn’t work for some reason.