Connector Identification (LEMO look alike)

Hi everyone, I’m having a really hard time trying to identify the manufacturer of the connector in the images below

As far as I know the connector is a push pull connector with a shallow guiding mark, its external body measures around 8.5mm and connector itself around 7mm. The pitch between each pin is around 2 mm and is a straight connector.

As additional information it has solder cups terminations

Thanks for any help provided

Hi pvergili,

That looks a lot like the 2057-MMI-M1PG04S52-ND from Adam Tech.

Other similar ones look to be in Circular Connector Assemblies | Circular Connectors | Electronic Components Distributor DigiKey but there is still a lot of options to sift through.

You might have to review some data sheets on ones you find there similar to verify for certain.

Indeed it is very similar and was my first candidate, I have purchased and tried it and they are slightly different

I’m sorry, I’m not finding a better one than that.

No worries, thanks for the support. I suspect that this connector belongs to a chinese manufacturer that will not be listed in digikey

Hi pvergili ,

I think I might have found it. It looks like it might be the “T” series water-proof connector from Finecables.

From the Finecables Push-Pull catalog:

I think the part number would be PSG-0T-304-CLACxx with xx representing a code for cable diameter.

I could not identify a water-proof equivalent connector from ODU or Adam Tech.

However, I’d say there’s a pretty good chance (though I cannot definitively say so) that it’s a knock-off of the LEMO “T” series, as the form-factors look very similar and the part numbering is practically the same. Unfortunately, we do not stock this series, but a comparable part number would be something like:

  • FGG.0T.304.CLACxx – With “xx” calling out a cable diameter code

The one option from this series that we list in our system is the FGG.0T.304.CLAC35Z. This one is meant to use a 3.1 to 3.5mm diameter cable, as defined by the “C35”, and is intended to have a strain relief added (indicated by the trailing “Z”), such as part number GMA.0B.035.DN.

The FGG.0T.304.CLAC35Z could be ordered from us either as a non-stocking part with a fairly significant lead-time or from our Marketplace supplier with an MOQ of 5 pieces.

@David_1528 I think that may be the connector, thanks for your help!!