CTF pa66
Hello Rushivyas, welcome to the Digi-Key TechForum.
We have a lot of similar connectors, but there are many different sizes, for the spacing on the contacts. Can you measure the distance from the center of one contact to the center of the other contact? This will give us the Pitch (spacing) of the connector.
I did not find one that looks identical, but you can Click here for the closest matches. These options include the pitches of 3.50mm, 3.81mm and 5.08mm.
For future reference:
I just searched for this same connector, which is used by some ekey equipment, e.g. the ekey multi SE REG 4.
If it’s 3.5mm pitch, it’s this one, specifically: https://www.sauro.net/products/CTF02008/?product_id=CTF02008
Hello,
We also have these options listed for 3.5mm pitch: 3.5mm pitch terminal