We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I am looking to make a precooler for air entering my CPAP so that after the machine increases the pressure it isn’t so warm on my face. I know that CPAP machines only increase the pressure enough to make the temp rise a degree or two, but it seems like more on the face. My pressure rate is 8.9 cmH2O at a volume of 17 l/min. What capacity of peltier chip would I need to get a 5-15 degree F temp drop?
If I’ve figured correctly, assuming dry air and no condensation you’d need about 2W of thermal power to achieve a 10°c temp change. So probably at least a 10W rated peltier.
It’s unlikely that the unpleasant sensation you describe is a result of heating due to compression. Many CPAP devices incorporate a heating element for humidity control, and if a mask-type interface is being used, that in itself can produce unpleasant sensations of warmth due to exhaled moisture and air being held close to the face.
Thank you. I have the heating all turned off, so it isn’t that. I could see the warmth of exhaled air as being problematic. Should one have some sort of thermostat system to control cooling?