Hello,
I am looking for a Data Logger that can measure temperature and pressure for a research project. Currently we are using a DATAQ DI-2008, with 7 Thermocouples in different channels, and one pressure sensor, a Futeck PMP300 (FSH03382), 25 PSIA, whose output can be up to 10 Volts. It works fine, but with a slight offset and it shuts off whenever our computer restarts (as it is powered only by USB). I was wondering if there were any data loggers with a battery, like VersaLog, that can continuously record data even when the computer is off.
The VersaLog we have now is a TC model that can only handle DC millivolt outputs. Our current pressure sensor output is up to 10 Volts, which does not work with that model.
I was wondering if there are any data loggers with the capabilities of the DATAQ 2008, but with a battery or external power supply port and can continuously record data.
Thank you.