This is a page about ST’s STM32MP1 series of Cortex-A7 based Development Kits.
Availability
Boards:
- Discovery kit with STM32MP157D MPU at DigiKey
- Discovery kit with STM32MP157F MPU at DigiKey
- Evaluation board with STM32MP157D MPU at DigiKey
- Evaluation board with STM32MP157F MPU at DigiKey
Vendor Documentation
- ST Documentation: https://www.st.com
- STM32 Arm Cortex MPUs: https://www.st.com/en/microcontrollers-microprocessors/stm32-arm-cortex-mpus.html
- STM32MP1 Series: https://www.st.com/en/microcontrollers-microprocessors/stm32mp1-series.html
Basic Requirements
- Running a recent supported release of Debian, Fedora or Ubuntu on a x86 64bit based PC; without OS Virtualization Software.
- Many of the listed commands assume /bin/bash as the default shell.
- Kernel.org Cross Compilers – https://mirrors.edge.kernel.org/pub/tools/crosstool/
- Bootloader
- Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
- Source: https://github.com/u-boot/u-boot/
- Linux Kernel
- Linus’s Mainline tree: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
- ARM based rootfs
- Debian: https://www.debian.org
Cross Compiler: GCC
This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:
#user@localhost:~$
wget -c https://mirrors.edge.kernel.org/pub/tools/crosstool/files/bin/x86_64/11.3.0/x86_64-gcc-11.3.0-nolibc-arm-linux-gnueabi.tar.xz
tar -xf x86_64-gcc-11.3.0-nolibc-arm-linux-gnueabi.tar.xz
export CC32=`pwd`/gcc-11.3.0-nolibc/arm-linux-gnueabi/bin/arm-linux-gnueabi-
Test Cross Compiler:
#user@localhost:~$
${CC32}gcc --version
#Test Output:
arm-linux-gnueabi-gcc (GCC) 11.3.0
Copyright (C) 2021 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Bootloader: U-Boot
Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
Depending on your Linux Distribution, you will also need a host gcc and other tools, so with Debian/Ubuntu start with installing the build-essential meta package.
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y bc bison build-essential flex libgnutls28-dev ; \
sudo apt-get install -y libssl-dev python3-dev python3-minimal ; \
sudo apt-get install -y python3-setuptools swig uuid-dev
Download:
#user@localhost:~$
git clone -b v2025.04 https://github.com/u-boot/u-boot --depth=1
Configure and Build:
#user@localhost:~$
make -C ./u-boot/ CROSS_COMPILE=${CC32} distclean
make -C ./u-boot/ CROSS_COMPILE=${CC32} stm32mp15_trusted_defconfig
Build for: stm32mp157a-dk1
#user@localhost:~$
make -C ./u-boot/ CROSS_COMPILE=${CC32} DEVICE_TREE=stm32mp157a-dk1 all
Build for: stm32mp157c-dk2
#user@localhost:~$
make -C ./u-boot/ CROSS_COMPILE=${CC32} DEVICE_TREE=stm32mp157c-dk2 all
Bootloader: OP-TEE Trusted OS
OP-TEE Trusted OS: https://github.com/OP-TEE/optee_os
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y build-essential python3-cryptography python3-pyelftools
Download:
#user@localhost:~$
git clone -b 4.5.0 https://github.com/OP-TEE/optee_os.git --depth=1
Configure and Build: stm32mp157a-dk1
#user@localhost:~$
make -C ./optee_os/ CROSS_COMPILE=${CC32} ARCH=arm PLATFORM=stm32mp1 CFG_EMBED_DTB_SOURCE_FILE=stm32mp157a-dk1.dts
Configure and Build: stm32mp157c-dk2
#user@localhost:~$
make -C ./optee_os/ CROSS_COMPILE=${CC32} ARCH=arm PLATFORM=stm32mp1 CFG_EMBED_DTB_SOURCE_FILE=stm32mp157c-dk2.dts
Bootloader: Trusted Firmware A (TF-A)
Trusted Firmware A (TF-A): https://github.com/TrustedFirmware-A/trusted-firmware-a
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y build-essential device-tree-compiler
Download:
#user@localhost:~$
git clone -b lts-v2.10 https://github.com/TrustedFirmware-A/trusted-firmware-a.git --depth=1
Configure and Build: stm32mp157a-dk1
#user@localhost:~$
make -C ./trusted-firmware-a/ CROSS_COMPILE=${CC32} realclean
make -C ./trusted-firmware-a/ CROSS_COMPILE=${CC32} PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 DTB_FILE_NAME=stm32mp157a-dk1.dtb STM32MP_SDMMC=1
make -C ./trusted-firmware-a/ CROSS_COMPILE=${CC32} PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 AARCH32_SP=optee DTB_FILE_NAME=stm32mp157c-dk2.dtb BL33=../u-boot/u-boot-nodtb.bin BL33_CFG=../u-boot/u-boot.dtb BL32=../optee_os/out/arm-plat-stm32mp1/core/tee-header_v2.bin BL32_EXTRA1=../optee_os/out/arm-plat-stm32mp1/core/tee-pager_v2.bin BL32_EXTRA2=../optee_os/out/arm-plat-stm32mp1/core/tee-pageable_v2.bin fip
Copy tf-a-stm32mp157a-dk1.stm32 for stm32mp157a-dk1
#user@localhost:~$
mkdir -p ./input/
cp -v ./trusted-firmware-a/build/stm32mp1/release/tf-a-stm32mp157a-dk1.stm32 ./input/
cp -v ./trusted-firmware-a/build/stm32mp1/release/fip.bin ./input/
Configure and Build: stm32mp157c-dk2
#user@localhost:~$
make -C ./trusted-firmware-a/ CROSS_COMPILE=${CC32} realclean
make -C ./trusted-firmware-a/ CROSS_COMPILE=${CC32} PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 DTB_FILE_NAME=stm32mp157c-dk2.dtb STM32MP_SDMMC=1
make -C ./trusted-firmware-a/ CROSS_COMPILE=${CC32} PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 AARCH32_SP=optee DTB_FILE_NAME=stm32mp157c-dk2.dtb BL33=../u-boot/u-boot-nodtb.bin BL33_CFG=../u-boot/u-boot.dtb BL32=../optee_os/out/arm-plat-stm32mp1/core/tee-header_v2.bin BL32_EXTRA1=../optee_os/out/arm-plat-stm32mp1/core/tee-pager_v2.bin BL32_EXTRA2=../optee_os/out/arm-plat-stm32mp1/core/tee-pageable_v2.bin fip
Copy tf-a-stm32mp157c-dk2.stm32 for stm32mp157c-dk2
#user@localhost:~$
mkdir -p ./input/
cp -v ./trusted-firmware-a/build/stm32mp1/release/tf-a-stm32mp157c-dk2.stm32 ./input/
cp -v ./trusted-firmware-a/build/stm32mp1/release/fip.bin ./input/
Linux Kernel
This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:
#user@localhost:~$
git clone https://github.com/RobertCNelson/armv7-lpae-multiplatform ./kernelbuildscripts
cd kernelbuildscripts/
For v6.12.x (Longterm 6.12.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/v6.12.x -b tmp
Build:
#user@localhost:~/kernelbuildscripts$
./build_kernel.sh
Root File System
Debian 12
| User | Password |
|---|---|
| debian | temppwd |
Download:
#user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-12.11-minimal-armhf-2025-05-28.tar.xz
Verify:
#user@localhost:~$
sha256sum debian-12.11-minimal-armhf-2025-05-28.tar.xz
#sha256sum output:
805d892548d199bcca75d7cad5feb55b304fa09ee20978b285c315a20a1b8423 debian-12.11-minimal-armhf-2025-05-28.tar.xz
Extract:
#user@localhost:~$
tar xf debian-12.11-minimal-armhf-2025-05-28.tar.xz
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------
Copy and paste that “export kernel_version=5.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=5.X.Y-Z
Create Root File System with genimage:
The genimage https://github.com/pengutronix/genimage tool is now used to generate a sdcard.img vs directly interfacing with the microSD.
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y dosfstools genimage mtools
Create working directory for genimage:
#user@localhost:~$
sudo mkdir -p ./input/.rootfs
Copy Root File System
#Debian; Root File System: user@localhost:~$
sudo tar xfvp ./debian-*-*-armhf-*/armhf-rootfs-*.tar -C ./input/.rootfs/
sync
Enable first boot customization
#user@localhost:~$
sudo mkdir -p ./input/.rootfs/boot/firmware/
sudo cp ./input/.rootfs/etc/bbb.io/templates/sysconf.txt ./input/.rootfs/boot/firmware/
Open ./input/.rootfs/boot/firmware/sysconf.txt in your text editor and change any user setting.
- user_name=
- user_password=
- hostname=
#user@localhost:~$
sudo nano ./input/.rootfs/boot/firmware/sysconf.txt
Setup extlinux.conf
#user@localhost:~$
sudo mkdir -p ./input/.rootfs/boot/extlinux/
sudo sh -c "echo 'label Linux ${kernel_version}' > ./input/.rootfs/boot/extlinux/extlinux.conf"
sudo sh -c "echo ' kernel /boot/vmlinuz-${kernel_version}' >> ./input/.rootfs/boot/extlinux/extlinux.conf"
sudo sh -c "echo ' fdtdir /boot/dtbs/${kernel_version}/' >> ./input/.rootfs/boot/extlinux/extlinux.conf"
sudo sh -c "echo ' append console=ttySTM0,115200 root=/dev/mmcblk0p4 ro rootfstype=ext4 rootwait net.ifnames=0' >> ./input/.rootfs/boot/extlinux/extlinux.conf"
Copy Kernel Image
Kernel Image:
#user@localhost:~$
sudo cp -v ./kernelbuildscripts/deploy/${kernel_version}.zImage ./input/.rootfs/boot/vmlinuz-${kernel_version}
Copy Kernel Device Tree Binaries
#user@localhost:~$
sudo mkdir -p ./input/.rootfs/boot/dtbs/${kernel_version}/
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-dtbs.tar.gz -C ./input/.rootfs/boot/dtbs/${kernel_version}/
Copy Kernel Modules
#user@localhost:~$
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-modules.tar.gz -C ./input/.rootfs/usr/
File Systems Table (/etc/fstab)
#user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk0p4 / auto errors=remount-ro 0 1' >> ./input/.rootfs/etc/fstab"
WiFi
#user@localhost:~$
wget -c https://raw.githubusercontent.com/STMicroelectronics/meta-st-stm32mp/refs/heads/scarthgap/recipes-kernel/linux-firmware/linux-firmware/brcmfmac43430-sdio.txt
sudo mkdir -p ./input/.rootfs/usr/lib/firmware/brcm/
sudo cp -v ./brcmfmac43430* ./input/.rootfs/usr/lib/firmware/brcm/
Check partition size
Verify Root File partition size, this can be used to modify the seek value below for size tweaking.
#user@localhost:~$
sudo du -sh ./input/.rootfs/
Create rootfs.ext4
#user@localhost:~$
sudo dd if=/dev/zero of=./input/rootfs.ext4 bs=1 count=0 seek=1600M
sudo mkfs.ext4 -F ./input/rootfs.ext4 -d ./input/.rootfs/
Create sdcard.img with genimage
The genimage https://github.com/pengutronix/genimage tool is now used to generate a sdcard.img vs directly interfacing with the microSD.
Create genimage.cfg file
#user@localhost:~$
nano genimage.cfg
#genimage.cfg
image sdcard.img {
hdimage {
partition-table-type = "gpt"
}
partition fsbl1 {
image = "tf-a-stm32mp157c-dk2.stm32"
}
partition fsbl2 {
image = "tf-a-stm32mp157c-dk2.stm32"
}
partition fip {
image = "fip.bin"
size = 2M
}
partition rootfs {
image = "rootfs.ext4"
bootable = "yes"
}
}
Run genimage on genimage.cfg
#user@localhost:~$
genimage --config genimage.cfg
genimage output
sdcard.img can be flashed to a microSD using rpi-imager https://github.com/raspberrypi/rpi-imager or your favorite image writing software.
#user@localhost:~$
tree images/
images/
└── sdcard.img
1 directory, 1 file
Final Tweaks (extend rootfs partition)
Extend the rootfs partition to fill available space on drive.
Use growpart to extend a partition in a partition table
sudo growpart /dev/mmcblk0 4
voodoo@stm32mp1:~$ sudo growpart /dev/mmcblk0 4
CHANGED: partition=4 start=4954 old: size=2048000 end=2052953 new: size=15518853 end=15523806
First Reboot
sudo reboot
Use resize2fs to enlarge the existing filesystem
sudo resize2fs /dev/mmcblk0p4
voodoo@stm32mp1:~$ sudo resize2fs /dev/mmcblk0p4
resize2fs 1.47.0 (5-Feb-2023)
Filesystem at /dev/mmcblk0p4 is mounted on /; on-line resizing required
old_desc_blocks = 1, new_desc_blocks = 1
The filesystem on /dev/mmcblk0p4 is now 1939856 (4k) blocks long.
Second Reboot
This last reboot will take awhile as fsck is checking the partition on bootup.
sudo reboot
Comments
Any questions or comments please go to our TechForum: TechForum