Debounce Logic Circuit (Verilog)

Logic Home

Example Verilog Code

DeBounce_v.v (2.5 KB)
DeBounce_tf.v (1.5 KB)

Introduction

Note: The information on this page is largely taken from the Debounce Logic Circuit (VHDL) page; the design concepts pertain to both Verilog and VHDL implementations.

Using mechanical switches for a user interface is a ubiquitous practice. However, when these switches are actuated, the contacts often rebound, or bounce, off one another before settling into a stable state. Several methods exist to deal with this temporary ambiguity, using either hardware or software. Here, we look at correcting this problem with a simple digital logic circuit (a common task when interfacing FPGAs or CPLDs with pushbuttons or other switches). Generic Verilog code for the DeBounce module and the test fixture is included.

Theory of Operation

Figure 1 illustrates the debounce circuit in question. The circuit continuously clocks the button’s logic level into FF1 and subsequently into FF2. So, FF1 and FF2 always store the last two logic levels of the button. When these two values remain identical for a specified time, then FF3 is enabled, and the stable value is clocked through to the result output.

The XOR gate and N-bit counter accomplish the timing. If the button’s level changes, the values of FF1and FF2 differ for a clock cycle, clearing the N-bit counter via the XOR gate. If the button’s level is unchanging (i.e. if FF1 and FF2 are the same logic level), then the XOR gate releases the counter’s synchronous clear, and the counter begins to count. The counter continues to increment in this manner until it (1) reaches the specified time and enables the output register or (2) is interrupted and cleared by the XOR gate because the button’s logic level is not yet stable.

The counter’s size determines the time required to validate the button’s stability. When the counter increments to the point that its carry out bit is asserted, it disables itself from incrementing further and enables the output register FF3. The circuit remains in this state until a different button value is clocked into FF1, clearing the counter via the XOR gate.

Figure 1. Debounce Circuit

Sizing the Counter

The size of the counter and the clock frequency together determine the time period P that validates the button’s stability. Equation 1 describes this relationship.

equation_1

In typical applications, the number of clock cycles is large, so the additional two clock cycles from loading FF2 and FF3 can safely be disregarded.

Most switches reach a stable logic level within 10ms of the actuation. Supposing we have a 50MHz clock, we need to count 0.01*50,000,000 = 500,000 clock cycles to reach 10ms. A 19-bit counter fulfills this requirement. Using the counter’s carry out pin, as shown in Figure 1, eliminates the requirement of evaluating the entire output bus of the counter. With this method, the actual time implemented is (219+2) / 50,000,000 = 10.49ms.

Debouncing typically does not require a high level of resolution, so the relatively small error introduced by using the carry out pin to identify the validation time is adequate for most applications. However, if greater time resolution is desired, the logical “AND” of some of the counter’s most significant bits achieves this with minimal additional logic usage.

Example Code and Simulation

The example code DeBounce_v.v available here instantiates the circuit in Figure 1. The parameter “N” defines the size of the counter. Figure 2 shows a simulation for this design with the counter size set as 11 bit, or a count of 1024 for demonstration and readability purposes. This amounts to a delay of 2^11/100MHz = 20.48 us. This is unreasonable for practical use, but ideal for illustrative purposes.

Figure 2. ActiveHDL Simulation Results

Conclusion

This simple logic circuit addresses mechanical switch debouncing for programmable logic.

Additional Information

Further design support, product tutorials, application notes, user’s guides and other documentation can be found on the Lattice website at: Lattice Semiconductor | The Low Power FPGA Leader