Hello thank you so much in advance. I just wanted to ask what would be the best Smart Dimmer compatible with XLG-20-H-B. But the catch is, i need the most EFFICIENT. electricity costs 0.50usd per kwh so even if it saved 3 watts it would be worth paying more for it. It supports 3 in 1 dimming. Cheapest possible would be great if if the smart features are going to be a lot theyre not important. Ideally around 10 dollars. It doesnt have to be smart if its going to go over 10 or 15 bucks. If theres like an efficient 5 dollar dimmer i will take that and connect to a wifi outlet thank you so much. The XLG-20-H-B LED driver supports three dimming control options:
0-10V analog dimming signal
10V PWM signal with a frequency range of 100Hz to 3kHz
Resistance dimming using an additive resistance