Hello,
I am looking for an equivalent to a Dimmable LED Driver used throughout our clinic. I was hoping to find something that would be an exact match to the drivers used now, or if not then something that would be a good replacement. I’ve tried reaching out to the Well-Lit company that produced our driver, but sadly I never received a response back. I also tried using an LED Driver (non-dimmable) from Amazon, but since it did not have 4 Output wires it did not work with our lights. I have attached an image of the original driver that came with our LED lights. Any feedback or advice would be greatly appreciated.
Thank you
Brand: Well-Lit
Model: LT-2L-HD6536-YA2
Input: 100-240v~50/60Hz 0.6A Max
Output: 27~40VDC —850mA 40W Max
Dimming: 0-10V or 1-10V & 10%-100%
Input Wires: N-White, L-Black
Output Wires: LED+Red, LED-Black, Dim+Purple, Dim-Gray