Filter caps

i am looking for these two caps

Add images

Add images

Hello @mikecasey,

Welcome to the DigiKey TechForum.

Out of curiosity what type of equipment are you restoring?

Unfortunately, you are unlikely to find a drop-in replacement with these chassis mount dual electrolytic capacitors. Options:

  • Instead, install discrete units inside the chassis.
    2 ea 22 uF type UCY2H220MHD by Nichicon
    2 ea 39 uF typr UCY2H390MHD by Nichicon

  • If you are a purest, and wish to preserve the unit’s look, you may be able to carefully open the capacitor can and install the new units. This takes considerable care and a lathe to open the can without destroying the metal.

Note that capacitors have loose 20 % tolerance. The selected 22 and 39 uF values are generally within this specification.

Best wishes,

APDahlen

P.S. You may want to use terminal strips as a new home for yor capacitors.

Thanks for your email. I am not a purist at all. So I just want to make this 40 year old amp work. So i would like to buy the necessary parts please.

Excellent, @mikecasey!

Please use:

Happy soldering!

Aaron

P.S. Please let us know if you were successful.

1 Like

I always have a problem with the verification code. Why is this happening. Why can’t I just login.?……

mikecasey,

You can also call us to place an order. The phone number 1-800-344-4539 will get you right to the sales department.