I need a male pin shunt to short pins on a female connector on my pcb, I found the Harwin 952-1865-ND, but i can’t find the right female mating connector for this to use on my pcb
Hello farhad,
Welcome to the DigiKey TechForum.
952-1865-ND will have a 5.08mm pitch or spacing of the 2 pins. But the pins are 1mm diameter, and will not plug into a normal size header on a PCB board.
The associated sockets listed on the manufacture’s website, include ones like 952-1468-ND, 952-1466-ND, and 952-2205-ND.
Please check these sockets, and see if they will work for you.
Hi David, thank you for the reply. The issue is that these socket pins have exposed metal. My application requires switching jumper to choose 120 vs 220 for the primary of a transformer. I want a female socket with a male shunt/jumper so that the socket on the pcb do not expose high voltage when no jumpered