This board is from a GE Refrigerator and this resistor is on the evaporator fan circuit.
Thank you
Hi @afges, welcome to the forum! Those look to be a pair of 2 ohm, 5% tolerance resistors. The exact power rating is hard to guess, but I would think that this part number will work as a good replacement, based on the appearance and size of the resistors:
PPC2.0W-1CT-ND
Thank you very much!
I would like to replace the 2 capacitors shown in that picture as well. They are clearly marked with the rating, but I’m not sure what the appropriate replacement would be since you have so many available. Would you also be able to guide me on the best replacement? I’m attaching another picture so that you can see all the markings on them. Thank you.
The capacitors are 470uF 25V from Rubycon. I was able to find these options that should work for you. You can select the dimensions for a part that is similar size.
Thank you very much Steven!