Help finding a mating connector

We have a PCB with a 10-pin connector, 3M-D2510-6002. (This is the connector commonly used for JTAG connectors although that’s not what we are using it for).

I am having trouble finding a board-mounted female connector that can mate to this (all I’m finding are cable mounts).

Can anyone help me find an alternative?

Thank you so much!

Hello Zoppina!

Welcome to the TechForum!

I was able to locate these options that may be what you are looking for: https://www.digikey.com/short/mtw85z39

the only thing to be weary of is with D2510-6002, it is classified as a “Board to cable” connector. This means that the mates meant for it are designed for cable mount. That doesn’t mean these won’t work, it’s just a bit more difficult to locate a solid option.

Also if you look under the Mating Products for the D2510-6002 there is this Board mount mating option as well. It is MSPV10-ND
Another possible option.