Help identify diode

I’m trying to replace this diode. Can anyone help me identify the part number or code of this diode? I have been told there is a smaller version of this diode and the looks and colour is the same but only smaller in size. Is there any difference?

Hi, cclementchong.
This is my answer - V03G.

V03G.pdf (54,8 КБ)

Thanks for the reply! But I have been told got different sizes. But the colour code is the same. Does it make any difference?

Hello cclementchong,

Since the Red color is calling out the voltage rating of 600V, a smaller one with the same color will probably be rated for the same voltage, but maybe a lower amperage. Will be a different manufacture or series, as the V03G on Adam7 linked to, lists only the one size 3.5mm Diameter max X 5mm Long max. If it is just slightly smaller, it may be the same item, as the dimensions are listed as Maximum, and do not list a Minimum.