Help Identifying This Pin

Hello,
I would greatly appreciate some help in identifying this pin, so I can order some.
It looks like a JST-XH but the dimensions are different. For instance my understanding is that the JST-XH is 6.5mm long and 1.95mm wide, but this one is 11mm long and 3mm wide. See pics.
Thanks in advance for any assistance!
Rob




[/grid]

Hello Roblogan69 and welcome to the DigiKey TechForum.

Based just on measurements, it is possible you are looking at the VA series from JST, such as 455-2964-1-ND. Or the VH series from JST, such as SVH-21GH-P1.1-ND.
The one from the VA series is 11.6mm long, 3mm wide, and 3.8mm tall.
The one from the VH series is 10.6mm long, 3mm wide, and 3.8mm tall.
I wouldn’t know for certain, without knowing the housing or mate that these are working with. But looking just at measurements, they do seem to be close.

Nick, thanks so much!
I believe either of these would work as they are very close.
The connector housing looks like this:


Much appreciated!
Now I need to find out how to order a smaller quantity as this shows MOQ of 4500.

Hi roblogan69,

For the VH option, try the BVH-21T-P1.1. Here’s the VH housing for that one:

VHR-4N.

Awesome, thanks David!