We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I have some LED lights that I’m mounting underneath the cabinets in my garage. I’m trying to daisy chain them together. Each light has a IEC 320-C5 input connector and output connector. Unfortunately I can’t seem to find a double ended female cable with two of these connectors with the right length.
What I’m looking to do is just join them together with wires and crimp connectors.
Can someone here help me select a female bullet-type crimp connector with a 2mm diameter that would work? If it’s a little smaller I can probably open it up a bit.
Thank you for contacting DigiKey , Sorry we do not have any bullet connectors that size to offer , I would suggest using two cable assemblies and cutting off one end on each and using butt splices to connect them to gether here are links for the cables we have to offer and the butt splices . From the cable link you can narrow down the search by applying the filter for the length you need to make these assemblies .
If you do not want to use the butt splices you could solder and heat shrink the wires and then put another piece of heat shrink over everything to get a nicer finish .