Help to find this

Hello to all

I am trying to find this product on the sote but to no success. Can ypu guys help to know if you have this item.

View picture

Hello and welcome to the forum @PS26! It looks like we don’t carry product from the manufacturer who made this, however I did find what looks like a drop in replacement. Part number is 338-2745-ND made by Cornell Dublier/Knowles. 161-193uF, which is marked on your photo, could also be written as 161uF with a tolerance of +20%, -0%. It’s the same range of values either way, just written in a different notation. Voltage rating looks good at 125VAC max.

I recommend double checking the terminal types and the size to make sure they match, especially if it already has mating terminals in your system and/or room is a concern. Our is 1.438" diameter by 2.810" tall, with 1/4" quick-connect terminals. Hope this helps!

Thank you so much