How USB-C Integration Enhances Parallel Battery Charging?

In our previous article, we explored the fundamentals of parallel battery charging, explaining how configuring batteries in parallel increases capacity and extends battery life. Now that we understand the basics, let’s dive into how USB-C technology takes parallel charging to the next level.

USB-C ports are becoming the standard for consumer devices because they offer much more flexibility than previous USB ports. Among the key benefits driving their popularity are higher power delivery and longer battery life. As a result, the need to charge devices at higher power levels is becoming increasingly important. This article will cover the integration, benefits, and drawbacks of parallel battery charging and USB-C in the consumer market.

USB-C’s Integration into Modern Parallel Battery Charging

As mentioned earlier, USB-C ports and devices have the ability to be charged at higher power levels compared to previous USB 2.0 and USB 3.0.
The most recent version of the USB-C spec, Power Delivery 3.1, can deliver up to 240 W, While this may be more than most consumer products require, it highlights the increased robustness of USB-C technology.

Example: Analog DevicesMAX77958 is a USB-C PD controller that handles PD 3.0 negotiation, cable detection, and even drives external chargers—making it ideal for smart, dynamic power distribution in parallel battery charging systems.

image

More Power, More Performance

As the battery capacity of a consumer device increases due to the parallel battery configuration, so does the power requirement for the charger supplying power to the device.
The higher power from USB-C ports allows consumers to charge their device faster than before and results in more time for them to use the device, without the attachment to a charging cable.

Benefits and Drawbacks

Parallel battery charging with USB-C has already made its way into many applications and will continue to spread throughout consumer applications.
While USB-C ports and cables will be largely beneficial to the consumer market in terms of power, cost, and simplicity, there are some drawbacks that need to be pointed out.

Table 1. Benefits of USB-C and Parallel Battery Charging

Today’s consumers want long battery life and less time tethered to a charger. USB-C helps make this possible with:

Single cable Power and data are on the same cable, which is beneficial in space constrained applications
High power levels Increased capacity and higher charging levels allow for a larger range of possible applications, including both low power consumer devices and high power tools and computers
Time savings­ The high charge current capabilities of USB-C allow for charging batteries in parallel, which results in more usable capacity in the amount of time it takes to charge just one battery
Simple integration A USB-C cable is reversible and can be plugged in either way, while adding additional batteries in parallel simply requires connecting the power source to the terminals of the new battery
Reduced electronic waste over time Using a common USB-C charger for multiple devices would reduce electronic waste around the world

Table 2. Drawbacks of USB-C and Parallel Battery Charging

Despite all the benefits, there are a few challenges when combining USB-C and parallel battery charging:

Differences in ports Complications over power levels can occur if both ports do not match. The multiple ports include Thunderbolt, Power Delivery 3.1, and Power Delivery 3.0
More expensive Additional batteries along with ports and cables that allow for faster charging require advanced technology, which is more expensive than previous versions
Cable replacement New USB-C cables will force USB-A, USB-B, and micro-USB cables to be replaced and the older cables will become obsolete
Larger size Adding an additional battery is going to take up extra space, which can become an issue in applications where size is a critical specification
Increased complexity Including an additional battery introduces a few complex issues, such as the need to balance aging across the batteries and ensuring charge cycles begin at similar voltages so the batteries or wiring is not damaged

USB Type-C PD controllers

image

USB Type-C® Power Delivery Connectors

image

What’s Next?

So far, we’ve discussed the basics of parallel battery charging and how USB-C enhances its performance. But how does this all work in the real world? Check out our next article: “Real-World Applications and Design Tips

Related Article

Parallel Battery Charging – and Why Does It Matter?
Implementing USB-C Parallel Charging Systems with MAX17330

Applicable Part Numbers
DigiKey Part Number Manufacturer Part Number
175-MAX17262HEWL+TTR-ND,175-MAX17262HEWL+TCT-ND,175-MAX17262HEWL+TDKR-ND MAX17262HEWL+T
175-MAX17260SEWL+TTR-ND,175-MAX17260SEWL+TCT-ND,175-MAX17260SEWL+TDKR-ND MAX17260SEWL+T
175-MAX17262REWL+TTR-ND,175-MAX17262REWL+TCT-ND,175-MAX17262REWL+TDKR-ND MAX17262REWL+T
505-MAX17260SETD±ND MAX17260SETD+
175-MAX17260SETD+TTR-ND,175-MAX17260SETD+TCT-ND,175-MAX17260SETD+TDKR-ND MAX17260SETD+T
MAX17048G+T10TR-ND,MAX17048G+T10CT-ND,MAX17048G+T10DKR-ND MAX17048G+T10
MAX17055EWL+TTR-ND,MAX17055EWL+TCT-ND,MAX17055EWL+TDKR-ND MAX17055EWL+T
MAX17055ETB+TTR-ND,MAX17055ETB+TCT-ND,MAX17055ETB+TDKR-ND MAX17055ETB+T
175-MAX17303X+TTR-ND,175-MAX17303X+TCT-ND,175-MAX17303X+TDKR-ND MAX17303X+T
MAX17201G+TTR-ND,MAX17201G+TCT-ND,MAX17201G+TDKR-ND MAX17201G+T
175-MAX17261METD+TTR-ND,175-MAX17261METD+TCT-ND,175-MAX17261METD+TDKR-ND MAX17261METD+T
MAX17261METD±ND MAX17261METD+
MAX6778XK+TTR-ND,MAX6778XK+TCT-ND,MAX6778XK+TDKR-ND MAX6778XK+T
MAX17201G±ND MAX17201G+
MAX17205G+00E-ND MAX17205G+00E
MAX17205G+TTR-ND,MAX17205G+TCT-ND,MAX17205G+TDKR-ND MAX17205G+T
175-MAX17330X22+TTR-ND,175-MAX17330X22+TCT-ND,175-MAX17330X22+TDKR-ND MAX17330X22+T
DS2745U+TR-ND,DS2745U+CT-ND,DS2745U+DKR-ND DS2745U+T&R
175-DS2786G+T&RTR-ND,175-DS2786G+T&RCT-ND,175-DS2786G+T&RDKR-ND DS2786G+T&R
175-DS2782E+T&RTR-ND,175-DS2782E+T&RCT-ND,175-DS2782E+T&RDKR-ND DS2782E+T&R
175-MAX38888ATD+TTR-ND,175-MAX38888ATD+TCT-ND,175-MAX38888ATD+TDKR-ND MAX38888ATD+T
DS2438Z+T&RTR-ND,DS2438Z+T&RCT-ND,DS2438Z+T&RDKR-ND DS2438Z+T&R
175-DS2788E+T&RTR-ND,175-DS2788E+T&RCT-ND,175-DS2788E+T&RDKR-ND DS2788E+T&R
DS2788E±ND DS2788E+
DS2777G±ND DS2777G+
175-MAX14680EWC+TTR-ND,175-MAX14680EWC+TCT-ND,MAX14680EWC+TCT-ND,175-MAX14680EWC+TDKR-ND MAX14680EWC+T
175-MAX17048X+T10TR-ND,175-MAX17048X+T10CT-ND,175-MAX17048X+T10DKR-ND MAX17048X+T10
175-MAX17260BEWL+TTR-ND,175-MAX17260BEWL+TCT-ND,175-MAX17260BEWL+TDKR-ND MAX17260BEWL+T
MAX6776XKC+TR-ND,MAX6776XKC+CT-ND,MAX6776XKC+DKR-ND MAX6776XKC+T
MAX6775XKB+TTR-ND,MAX6775XKB+TCT-ND,MAX6775XKB+TDKR-ND MAX6775XKB+T
505-MAX17303G±ND MAX17303G+
MAX17201G+00E-ND MAX17201G+00E
MAX6777XK+TR-ND,MAX6777XK+CT-ND,MAX6777XK+DKR-ND MAX6777XK+T
505-MAX17320G20±ND MAX17320G20+
505-MAX17320G22±ND MAX17320G22+
MAX17205G±ND MAX17205G+
175-MAX17301X+TTR-ND,175-MAX17301X+TCT-ND,175-MAX17301X+TDKR-ND MAX17301X+T
DS2745U±ND DS2745U+
DS2782G±ND DS2782G+
175-DS2756E+T&RTR-ND,175-DS2756E+T&RCT-ND,175-DS2756E+T&RDKR-ND DS2756E+T&R
DS2756E±ND DS2756E+
DS2438AZ+TR-ND,DS2438AZ+CT-ND,DS2438AZ+DKR-ND DS2438AZ+T&R
DS2438Z±ND DS2438Z+
505-MAX17841BGUE/V±ND MAX17841BGUE/V+
DS2782E±ND DS2782E+
DS2764AE±ND DS2764AE+
DS2780E±ND DS2780E+
175-DS2762AE+T&RTR-ND,175-DS2762AE+T&RCT-ND,175-DS2762AE+T&RDKR-ND DS2762AE+T&R
MAX20303BEWN+TTR-ND,MAX20303BEWN+TCT-ND,MAX20303BEWN+TDKR-ND MAX20303BEWN+T
MAX17843ACB/V±ND MAX17843ACB/V+
175-MAX14634EWC+TTR-ND,175-MAX14634EWC+TCT-ND,175-MAX14634EWC+TDKR-ND MAX14634EWC+T
MAX16915AUB±ND MAX16915AUB+
MAX16914AUB±ND MAX16914AUB+
175-MAX17261MEWL+TTR-ND,175-MAX17261MEWL+TCT-ND,175-MAX17261MEWL+TDKR-ND MAX17261MEWL+T
175-MAX17201X+TTR-ND,175-MAX17201X+TCT-ND,175-MAX17201X+TDKR-ND MAX17201X+T
MAX17215G+00E-ND MAX17215G+00E
175-MAX17320X20+TTR-ND,175-MAX17320X20+TCT-ND,175-MAX17320X20+TDKR-ND MAX17320X20+T
MAX6775XKC+TTR-ND,MAX6775XKC+TCT-ND,MAX6775XKC+TDKR-ND MAX6775XKC+T
175-MAX6775XKA+TTR-ND,175-MAX6775XKA+TCT-ND,175-MAX6775XKA+TDKR-ND MAX6775XKA+T
DS2786BG±ND DS2786BG+
505-MAX17320G10±ND MAX17320G10+
175-MAX6433UK+TTR-ND,175-MAX6433UK+TCT-ND,175-MAX6433UK+TDKR-ND MAX6433UK+T
DS2746G±ND DS2746G+
MAX14653EWC+TTR-ND,MAX14653EWC+TCT-ND,MAX14653EWC+TDKR-ND MAX14653EWC+T
505-MAX17320G12±ND MAX17320G12+
DS2786G±ND DS2786G+
DS2781E+TR-ND,DS2781E+CT-ND,DS2781E+DKR-ND DS2781E+T&R
DS2781G±ND DS2781G+
DS2438AZ±ND DS2438AZ+
DS2764BE±ND DS2764BE+
DS2778G±ND DS2778G+
DS2776G±ND DS2776G+
DS2781E±ND DS2781E+
DS2762BE±ND DS2762BE+
DS2762AE±ND DS2762AE+
MAX14920ECB±ND MAX14920ECB+
MAX14921ECS±ND MAX14921ECS+
505-MAX17823BGCB/V±ND MAX17823BGCB/V+
175-MAX14921ECS+TTR-ND,175-MAX14921ECS+TCT-ND,175-MAX14921ECS+TDKR-ND MAX14921ECS+T
175-MAX14670EWL+TTR-ND,175-MAX14670EWL+TCT-ND,175-MAX14670EWL+TDKR-ND MAX14670EWL+T
MAX14606EWL+TTR-ND,MAX14606EWL+TCT-ND,MAX14606EWL+TDKR-ND MAX14606EWL+T
175-MAX6776XKB+TTR-ND,175-MAX6776XKB+TCT-ND,175-MAX6776XKB+TDKR-ND MAX6776XKB+T
175-MAX6776XKA+TTR-ND,175-MAX6776XKA+TCT-ND,175-MAX6776XKA+TDKR-ND MAX6776XKA+T
MAX6775LTA+TTR-ND,MAX6775LTA+TCT-ND,MAX6775LTA+TDKR-ND,2156-MAX6775LTA+T-ND MAX6775LTA+T
MAX17211G+00E-ND MAX17211G+00E
MAX6436UT+TTR-ND,MAX6436UT+TCT-ND,MAX6436UT+TDKR-ND MAX6436UT+T
175-MAX6434UK+TTR-ND,175-MAX6434UK+TCT-ND,175-MAX6434UK+TDKR-ND MAX6434UK+T
175-MAX17215G+TTR-ND,175-MAX17215G+TCT-ND,175-MAX17215G+TDKR-ND MAX17215G+T
DS2782G+TR-ND,DS2782G+CT-ND,DS2782G+DKR-ND DS2782G+T&R
MAX1538ETI+TR-ND,MAX1538ETI+CT-ND,MAX1538ETI+DKR-ND MAX1538ETI+T
175-MAX17841BGUE/V+TTR-ND,175-MAX17841BGUE/V+TCT-ND,175-MAX17841BGUE/V+TDKR-ND MAX17841BGUE/V+T
MAX1538ETI±ND MAX1538ETI+
DS2780G±ND DS2780G+
MAX1259CWE±ND MAX1259CWE+
175-MAX14920ECB+TTR-ND,175-MAX14920ECB+TCT-ND,175-MAX14920ECB+TDKR-ND MAX14920ECB+T
505-MAX17853ACB/V±ND MAX17853ACB/V+
175-MAX17823BGCB/V+TTR-ND,175-MAX17823BGCB/V+TCT-ND,175-MAX17823BGCB/V+TDKR-ND MAX17823BGCB/V+T
505-MAX17300G±ND MAX17300G+
505-MAX17310G±ND MAX17310G+
MAX17215G±ND MAX17215G+
175-MAX77972EWX+TTR-ND,175-MAX77972EWX+TCT-ND,175-MAX77972EWX+TDKR-ND MAX77972EWX+T
175-MAX14525ETA+TTR-ND,175-MAX14525ETA+TCT-ND,175-MAX14525ETA+TDKR-ND MAX14525ETA+T
505-MAX20095ATIA/VY±ND MAX20095ATIA/VY+
505-MAX17330X22±ND MAX17330X22+
505-MAX17301G±ND MAX17301G+
505-MAX17841BGUE±ND MAX17841BGUE+
505-ADES1756GCB/V±ND ADES1756GCB/V+
505-MAX1259CPE±ND MAX1259CPE+
505-ADES1755GCB/V±ND ADES1755GCB/V+
505-ADES1754GCB/V±ND ADES1754GCB/V+
505-MAX17823BGCB±ND MAX17823BGCB+
MAX17830GUN±ND MAX17830GUN+
MAX17830GUN/V±ND MAX17830GUN/V+
175-MAX17830GUN/V+TTR-ND,175-MAX17830GUN/V+TCT-ND,175-MAX17830GUN/V+TDKR-ND MAX17830GUN/V+T
2156-MAX1707ETG±ND MAX1707ETG+
2156-MAX6787TA±ND MAX6787TA+
2156-MAX1786EUI±ND MAX1786EUI+
2156-MAX17130ETL±ND MAX17130ETL+
2156-MAX1786AEUI+T-ND MAX1786AEUI+T
2156-MAX8629ETI+T-ND MAX8629ETI+T
2156-MAX8618ETL±ND MAX8618ETL+
2156-MAX8617ETL±ND MAX8617ETL+
2156-MAX6781LTC±ND MAX6781LTC+
2156-MAX1906VEGE-ND MAX1906VEGE
2156-MAX1906SEGE-ND MAX1906SEGE
2156-MAX6789TB±ND MAX6789TB+
2156-MAX6790TB±ND MAX6790TB+
2156-MAX4921BETD±ND MAX4921BETD+
2156-MAX4920BETD±ND MAX4920BETD+
2156-MAX6428ORUR±ND MAX6428ORUR+
2156-MAX6428MQUR±ND MAX6428MQUR+
2156-MAX6427DHUR-ND MAX6427DHUR
2156-MAX6436UT-T-ND MAX6436UT-T
2156-MAX6438UT-T-ND MAX6438UT-T
2156-MAX6431EHUS-T-ND MAX6431EHUS-T
2156-MAX6431FJUS-T-ND MAX6431FJUS-T
2156-MAX6432EIUS-T-ND MAX6432EIUS-T
2156-MAX6431CIUS-T-ND MAX6431CIUS-T
2156-MAX6431DHUS-T-ND MAX6431DHUS-T
2156-MAX6431CHUS-T-ND MAX6431CHUS-T
2156-MAX6432DHUS-T-ND MAX6432DHUS-T
2156-MAX6430ORUS-T-ND MAX6430ORUS-T
2156-MAX6432FJUS-T-ND MAX6432FJUS-T
2156-MAX6430EGUS-T-ND MAX6430EGUS-T
2156-MAX6432MRUS-T-ND MAX6432MRUS-T
2156-MAX6432EHUS-T-ND MAX6432EHUS-T
2156-MAX6430PQUS-T-ND MAX6430PQUS-T
2156-MAX6432ORUS-T-ND MAX6432ORUS-T
2156-MAX8629CETI±ND MAX8629CETI+
2156-MAX1829ETL±ND MAX1829ETL+
2156-MAX6429DHUR-T-ND MAX6429DHUR-T
2156-MAX6429MRUR-T-ND MAX6429MRUR-T
2156-MAX6427EHUR-T-ND MAX6427EHUR-T
2156-MAX6428AGUR-T-ND MAX6428AGUR-T
2156-MAX6429KTUR-T-ND MAX6429KTUR-T
2156-MAX6428MRUR-T-ND MAX6428MRUR-T
2156-MAX6427KQUR-T-ND MAX6427KQUR-T
2156-MAX6429EHUR-T-ND MAX6429EHUR-T
2156-MAX6429ORUR-T-ND MAX6429ORUR-T
2156-MAX6429EIUR-T-ND MAX6429EIUR-T
2156-MAX6786TA±ND MAX6786TA+
2156-MAX6788TA±ND MAX6788TA+
2156-MAX6847KASD3-ND MAX6847KASD3
2156-MAX6440UTEHRD3-ND MAX6440UTEHRD3
2156-MAX6847KARD3-T-ND MAX6847KARD3-T
2156-MAX6440UTEHRD3-T-ND MAX6440UTEHRD3-T
2156-MAX6847KASD3-T-ND MAX6847KASD3-T
2156-MAX6846KAWD3-T-ND MAX6846KAWD3-T
2156-MAX6440UTFJTD7-T-ND MAX6440UTFJTD7-T
2156-MAX6440UTKQSD3-T-ND MAX6440UTKQSD3-T
2156-MAX6439UTDHSD3-T-ND MAX6439UTDHSD3-T
2156-MAX17817EUI+T-ND MAX17817EUI+T
2156-MAX6849KAVD7-T-ND MAX6849KAVD7-T
2156-MAX6848KARD7-T-ND MAX6848KARD7-T
2156-MAX6849KASD3-T-ND MAX6849KASD3-T
2156-MAX6848KATD3-T-ND MAX6848KATD3-T
2156-MAX1827ETL-ND MAX1827ETL
2156-MAX1827ETL±ND MAX1827ETL+
2156-MAX6848KATD3-ND MAX6848KATD3
505-MAX6775LTB+TTR-ND,2156-MAX6775LTB+T-ND MAX6775LTB+T
2156-MAX8568BETE-ND MAX8568BETE
2156-MAX6775LTA±ND MAX6775LTA+
2156-MAX6442KAEISD3-T-ND MAX6442KAEISD3-T
2156-MAX6441KAEISD3-T-ND MAX6441KAEISD3-T
2156-MAX6441KAEHRD3-T-ND MAX6441KAEHRD3-T
2156-MAX6441KAKQVD3-T-ND MAX6441KAKQVD3-T
2156-DS2746G-C02+TR-ND DS2746G-C02+TR
2156-MAX1526ETM+G104-ND MAX1526ETM+G104
2156-MAX1906XEGE-ND MAX1906XEGE
2156-MAX6428AGUR-ND MAX6428AGUR
2156-MAX6431FJUS-ND MAX6431FJUS
2156-MAX6432MRUS-ND MAX6432MRUS
2156-MAX6431MRUS-ND MAX6431MRUS
2156-MAX6432DHUS-ND MAX6432DHUS
2156-MAX6429MRUR-ND MAX6429MRUR
2156-MAX6439UTDHSD3-ND MAX6439UTDHSD3
2156-MAX6429KTUR-ND MAX6429KTUR
2156-MAX6432EHUS-ND MAX6432EHUS
2156-MAX6441KAEISD3-ND MAX6441KAEISD3
2156-MAX6432FJUS-ND MAX6432FJUS
2156-MAX6432ORUS-ND MAX6432ORUS
2156-MAX6430PQUS-ND MAX6430PQUS
2156-MAX6430EIUS-ND MAX6430EIUS
2156-MAX6431CIUS-ND MAX6431CIUS
2156-MAX6430DHUS-ND MAX6430DHUS
2156-MAX6846KAWD3-ND MAX6846KAWD3
2156-MAX6430EHUS-ND MAX6430EHUS
2156-MAX6431EIUS±ND MAX6431EIUS+
2156-MAX6431EHUS-ND MAX6431EHUS
2156-MAX6429ORUR-ND MAX6429ORUR
2156-MAX6428ORUR-ND MAX6428ORUR
2156-MAX6431ORUS-ND MAX6431ORUS
2156-MAX6429DHUR-ND MAX6429DHUR
2156-MAX6427EIUR-ND MAX6427EIUR
2156-MAX6435UK-ND MAX6435UK
2156-MAX6428EHUR-ND MAX6428EHUR
2156-MAX6432EIUS-ND MAX6432EIUS
2156-MAX6431CHUS-ND MAX6431CHUS
2156-MAX6440UTFJTD7-ND MAX6440UTFJTD7
2156-MAX6848KARD7-ND MAX6848KARD7
2156-MAX6431EIUS-ND MAX6431EIUS
2156-MAX6429EHUR-ND MAX6429EHUR
2156-MAX6442KAKQSD3-ND MAX6442KAKQSD3
2156-MAX6849KAVD7-ND MAX6849KAVD7
2156-MAX6431DHUS-ND MAX6431DHUS
2156-MAX6441KAKQVD3-ND MAX6441KAKQVD3
2156-MAX6437UT-ND MAX6437UT
2156-MAX6439UTEISD3-ND MAX6439UTEISD3
2156-MAX6849KASD3-ND MAX6849KASD3
2156-MAX1526ETM-ND MAX1526ETM
2156-MAX8695PELR+T-ND MAX8695PELR+T
2156-MAX1612EEE±ND MAX1612EEE+
2156-MAX1666AEEP±ND MAX1666AEEP+
2156-MAX1773AEUP-ND MAX1773AEUP
2156-MAX1773EUP±ND MAX1773EUP+
2156-MAX17050X-C01+T10-ND MAX17050X-C01+T10
2156-MAX1894XEEE-ND MAX1894XEEE
175-MAX17047G+T10TR-ND,175-MAX17047G+T10CT-ND MAX17047G+T10
505-MAX17320X20±ND MAX17320X20+
2156-DS2437S/TR/-ND DS2437S/T&R/
2156-MAX17077ETM±ND MAX17077ETM+
MAX6780LTB+TTR-ND,MAX6780LTB+TCT-ND,MAX6780LTB+TDKR-ND,2156-MAX6780LTB+T-ND MAX6780LTB+T
2156-MAX1613EEE±ND MAX1613EEE+
2156-MAX8697SEWQ+T-ND MAX8697SEWQ+T
2156-MAX1781ETM+C6D-ND MAX1781ETM+C6D
2156-MAX1789EUI+T-ND MAX1789EUI+T
2156-MAX1789EUI+CBH-ND MAX1789EUI+CBH
2156-MAX6430ORUS-ND MAX6430ORUS
2156-DS1610-ND DS1610
2156-MAX1787EUI+GH8-ND MAX1787EUI+GH8
MAX17049G±ND MAX17049G+
MAX38888ATD±ND MAX38888ATD+
MAX17301X±ND MAX17301X+
505-MAX17300X±ND MAX17300X+
2156-MAX6777LT±ND MAX6777LT+
2156-MAX4919BETD±ND MAX4919BETD+
2156-MAX6780LTB±ND MAX6780LTB+
2156-MAX6427EIUR±ND MAX6427EIUR+
2156-MAX6427DHUR±ND MAX6427DHUR+
2156-MAX6778LT±ND MAX6778LT+
2156-MAX6775LTB±ND MAX6775LTB+
2156-MAX6437UT±ND MAX6437UT+
175-MAX77972EWX±ND MAX77972EWX+
DS2784G±ND DS2784G+
DS2775G±ND DS2775G+
2156-MAX1666VEEP±ND MAX1666VEEP+
505-MAX38886ATD±ND MAX38886ATD+
MAX17303X±ND MAX17303X+
175-MAX17320G20+TTR-ND,175-MAX17320G20+TCT-ND,175-MAX17320G20+TDKR-ND MAX17320G20+T
175-MAX17335X22+TTR-ND,175-MAX17335X22+TCT-ND,175-MAX17335X22+TDKR-ND MAX17335X22+T
MAX14607EWL+TTR-ND,MAX14607EWL+TCT-ND,MAX14607EWL+TDKR-ND MAX14607EWL+T
MAX17211G±ND MAX17211G+
MAX6430EGUS+TTR-ND,MAX6430EGUS+TCT-ND,MAX6430EGUS+TDKR-ND MAX6430EGUS+T
MAX8682ETM±ND MAX8682ETM+
175-MAX17332X22+TTR-ND,175-MAX17332X22+TCT-ND,175-MAX17332X22+TDKR-ND MAX17332X22+T
MAX17048G±ND MAX17048G+
MAX14671EWL+T-ND MAX14671EWL+T
MAX16914AUB+T-ND MAX16914AUB+T
MAX16915AUB+T-ND MAX16915AUB+T
DS2703U+T&R-ND DS2703U+T&R
505-MAX6778LT+TTR-ND MAX6778LT+T
505-MAX17313X+TTR-ND MAX17313X+T
505-MAX17303G+TTR-ND MAX17303G+T
505-MAX17313G+TTR-ND MAX17313G+T
505-MAX17313G±ND MAX17313G+
MAX17201X+T0E-ND MAX17201X+T0E
MAX17211X+T-ND MAX17211X+T
MAX17211X+T0E-ND MAX17211X+T0E
MAX17211G+T-ND MAX17211G+T
MAX17201G+T0E-ND MAX17201G+T0E
MAX17211G+T0E-ND MAX17211G+T0E
505-MAX6427EIUR+TTR-ND MAX6427EIUR+T
505-MAX17320X10+TTR-ND MAX17320X10+T
505-MAX6780LTA+TTR-ND MAX6780LTA+T
505-MAX6779LTB+TTR-ND MAX6779LTB+T
505-DS2703U±ND DS2703U+
MAX16916GUB/V+T-ND MAX16916GUB/V+T
505-MAX17320X22+TTR-ND MAX17320X22+T
505-MAX17320G10+TTR-ND MAX17320G10+T
505-MAX17320X12+TTR-ND MAX17320X12+T
MAX17205X+T-ND MAX17205X+T
MAX17205X+T0E-ND MAX17205X+T0E
MAX17215X+T-ND MAX17215X+T
MAX17215X+T0E-ND MAX17215X+T0E
505-MAX17300G+TTR-ND MAX17300G+T
505-MAX17310G+TTR-ND MAX17310G+T
505-MAX6427ORUR+TTR-ND MAX6427ORUR+T
MAX17205G+T0E-ND MAX17205G+T0E
MAX17215G+T0E-ND MAX17215G+T0E
505-MAX17302X+TTR-ND MAX17302X+T
505-MAX17312X+TTR-ND MAX17312X+T
505-MAX17312G+TTR-ND MAX17312G+T
505-MAX17302G+TTR-ND MAX17302G+T
MAX14654EWC+T-ND MAX14654EWC+T
MAX14655EWC+T-ND MAX14655EWC+T
505-MAX17320G22+TTR-ND MAX17320G22+T
505-MAX17320G12+TTR-ND MAX17320G12+T
505-MAX17302G±ND MAX17302G+
505-MAX17312G±ND MAX17312G+
505-MAX17301G+TTR-ND MAX17301G+T
505-MAX17311G+TTR-ND MAX17311G+T
505-MAX17311X+TTR-ND MAX17311X+T
505-MAX17300X+TTR-ND MAX17300X+T
505-MAX17310X+TTR-ND MAX17310X+T
505-MAX17311G±ND MAX17311G+
MAX17040G+TTR-ND,MAX17040G+TCT-ND,MAX17040G+TDKR-ND MAX17040G+T
DS2746G+T&R-ND DS2746G+T&R
MAX8672ETD+T-ND MAX8672ETD+T
DS2786BG+T&R-ND DS2786BG+T&R
505-MAX17205X±ND MAX17205X+
175-MAX17049G+T10TR-ND,175-MAX17049G+T10CT-ND,175-MAX17049G+T10DKR-ND MAX17049G+T10
505-MAX20095ATIA/VY+TTR-ND MAX20095ATIA/VY+T
DS2780G+T&R-ND DS2780G+T&R
DS2764AE+T&R-ND DS2764AE+T&R
MAX6776LTA+TTR-ND,MAX6776LTA+TCT-ND,MAX6776LTA+TDKR-ND MAX6776LTA+T
505-ADES1756GCB/V+TTR-ND ADES1756GCB/V+T
MAX20335BEWX+T-ND MAX20335BEWX+T
DS2780E+T&R-ND DS2780E+T&R
DS2777G+T&R-ND DS2777G+T&R
DS2776G+T&R-ND DS2776G+T&R
DS2778G+T&R-ND DS2778G+T&R
DS2775G+T&R-ND DS2775G+T&R
DS2764BE+T&R-ND DS2764BE+T&R
505-ADES1755GCB/V+TTR-ND ADES1755GCB/V+T
505-ADES1754GCB/V+TTR-ND ADES1754GCB/V+T
MAX17841BGUE+T-ND MAX17841BGUE+T
DS2762BE+T&R-ND DS2762BE+T&R
DS2784G+T&R-ND DS2784G+T&R
MAX20303CEWN+T-ND MAX20303CEWN+T
MAX20303DEWN+T-ND MAX20303DEWN+T
MAX20303HEWN+T-ND MAX20303HEWN+T
MAX20303AEWN+T-ND MAX20303AEWN+T
MAX20303EEWN+T-ND MAX20303EEWN+T
MAX20303GEWN+T-ND MAX20303GEWN+T
505-MAX20303LEWN+TTR-ND MAX20303LEWN+T
505-MAX20303JEWN+TTR-ND MAX20303JEWN+T
MAX1259CWE+T-ND MAX1259CWE+T
505-MAX17852ACB/V+TTR-ND MAX17852ACB/V+T
MAX17830GUN+T-ND MAX17830GUN+T
MAX17843ACB/V+T-ND MAX17843ACB/V+T
MAX6431NQUS+T-ND MAX6431NQUS+T
MAX6428BGUR+T-ND MAX6428BGUR+T
MAX11080GUU±ND MAX11080GUU+
MAX11068GUU±ND MAX11068GUU+
MAX11068GUU+T-ND MAX11068GUU+T
MAX11080GUU+T-ND MAX11080GUU+T
DS2731E±ND DS2731E+
DS2731E+T&R-ND DS2731E+T&R
DS2703G+T&R-ND DS2703G+T&R
MAX8682ETM+T-ND MAX8682ETM+T
MAX17041G+T-ND MAX17041G+T
175-MAX17043G+TTR-ND,175-MAX17043G+TCT-ND,175-MAX17043G+TDKR-ND MAX17043G+T
MAX11080GUU/V±ND MAX11080GUU/V+
MAX11080GUU/V+T-ND MAX11080GUU/V+T
MAX17044G+T-ND MAX17044G+T
MAX11081GUU/V+T-ND MAX11081GUU/V+T
MAX17040G+U-ND MAX17040G+U
MAX17043G+U-ND MAX17043G+U
MAX17040X+U-ND MAX17040X+U
MAX17048X±ND MAX17048X+
MAX17049X±ND MAX17049X+
MAX11068GUU/V+T-ND MAX11068GUU/V+T
MAX17043X±ND MAX17043X+
MAX17040X+T10-ND MAX17040X+T10
MAX17043X+T10-ND MAX17043X+T10
MAX17044X+T10-ND MAX17044X+T10
MAX17049X+T10-ND MAX17049X+T10
MAX16916GUB/V±ND MAX16916GUB/V+
MAX1924VEEE±ND MAX1924VEEE+
MAX17055EWL±ND MAX17055EWL+
MAX17840AGUN/V+T-ND MAX17840AGUN/V+T
MAX20303BEWN±ND MAX20303BEWN+
MAX17260SEWL±ND MAX17260SEWL+
MAX17262REWL±ND MAX17262REWL+
MAX6433UK/GG8-ND MAX6433UK/GG8
MAX6776XKA±ND MAX6776XKA+
MAX17302X±ND MAX17302X+
MAX17311X±ND MAX17311X+
MAX17312X±ND MAX17312X+
MAX17313X±ND MAX17313X+
505-MAX17853ACB/V+TTR-ND MAX17853ACB/V+T
505-MAX17041G+U-ND MAX17041G+U
505-MAX17201X±ND MAX17201X+
505-MAX1660EEE±ND MAX1660EEE+
505-MAX20360AEWZ±ND MAX20360AEWZ+
175-MAX17320X22+TR-ND MAX17320X22+
MAX17260XEVKIT#-ND MAX17260XEVKIT#
MAX17261GEVKIT#-ND MAX17261GEVKIT#
MAX17262XEVKIT#-ND MAX17262XEVKIT#
MAX17263GEVKIT#-ND MAX17263GEVKIT#
505-MAX17332X2EVKIT#-ND MAX17332X2EVKIT#
505-MAX17048EVKIT#-ND MAX17048EVKIT#
MAX17303XEVKIT#-ND MAX17303XEVKIT#
MAX17205GEVKIT#-ND MAX17205GEVKIT#
MAX17055GEVKIT#-ND MAX17055GEVKIT#
505-MAX17320G1EVKIT#-ND MAX17320G1EVKIT#
505-MAX17330X2EVKIT#-ND MAX17330X2EVKIT#
505-MAX17320X1EVKIT#-ND MAX17320X1EVKIT#
505-MAX17300XEVKIT#-ND MAX17300XEVKIT#
MAX17201GEVKIT#-ND MAX17201GEVKIT#
MAX17205XEVKIT#-ND MAX17205XEVKIT#
MAX17211XEVKIT#-ND MAX17211XEVKIT#
MAX17215XEVKIT#-ND MAX17215XEVKIT#
505-MAX77787JEVKIT#-ND MAX77787JEVKIT#
505-MAX77789EVKIT#-ND MAX77789EVKIT#
505-MAX17320G2EVKIT#-ND MAX17320G2EVKIT#
MAX17301XEVKIT#-ND MAX17301XEVKIT#
MAX17211GEVKIT#-ND MAX17211GEVKIT#
MAX17215GEVKIT#-ND MAX17215GEVKIT#
MAX17055XEVKIT#-ND MAX17055XEVKIT#
505-MAX17260GEVKIT#-ND MAX17260GEVKIT#
505-MAX77751CEVKIT#-ND MAX77751CEVKIT#
505-MAX20342EVKIT#-ND MAX20342EVKIT#
MAX17311XEVKIT#-ND MAX17311XEVKIT#
505-DS2788EVKIT±ND DS2788EVKIT+
505-MAX17049EVKIT#-ND MAX17049EVKIT#
MAX17313XEVKIT#-ND MAX17313XEVKIT#
175-MAX17300GEVKIT#-ND MAX17300GEVKIT#
MAX17261XEVKIT#-ND MAX17261XEVKIT#
MAX17201XEVKIT#-ND MAX17201XEVKIT#
175-MAX17335X2EVKIT#-ND MAX17335X2EVKIT#
505-MAX77963EVKIT#-ND MAX77963EVKIT#
505-MAX17049XEVKIT#-ND MAX17049XEVKIT#
505-MAX17058EVKIT#-ND MAX17058EVKIT#
505-MAX17048XEVKIT#-ND MAX17048XEVKIT#
MAX17302XEVKIT#-ND MAX17302XEVKIT#
MAX17312XEVKIT#-ND MAX17312XEVKIT#
505-MAX17310XEVKIT#-ND MAX17310XEVKIT#
505-MAX17047EVKIT#-ND MAX17047EVKIT#
505-DS2782EVKIT±ND DS2782EVKIT+
505-DS2786EVKIT±ND DS2786EVKIT+
MAX17050EVKIT#-ND MAX17050EVKIT#