Introduction:
Humidity is the amount of water vapor in the air, and devices that detect it are called humidity sensors. Humidity is typically expressed as a percentage of relative humidity (RH).
Humidity sensors contain a sensing element that measure moisture level and also frequently feature thermocouples that measure temperature. They convert data into electrical signals and report the humidity level allowing one to use this information in their application.
Humidity sensors come in two types based on how they measure humidity:
Relative Humidity (RH): This measure how much moisture is in the air compared to the maximum amount of moisture the air can hold at the same temperature. A lower RH percentage means the air is drier. These sensors always include a temperature sensing element.
Absolute Humidity (AH): This measures the actual amount of water vapor in the air, regardless of temperature, and is expressed in grams per cubic meter. This type of sensor doesn’t need temperature data to make its measurement.
Type of Humidity Sensors
Humidity sensors are available in various sizes, ranging from handheld systems to small ICs. Depending on their operating characteristics, there are several types of humidity sensors.
1. Capacitive Humidity Sensor
A capacitive humidity sensor works on the principle of capacitance. The sensor consists of two conductive plates separated by a moisture-absorbing dielectric (polymer or ceramic) material. When humidity increases, water molecules are absorbed by the dielectric material, causing a change in capacitance. This change can be measured and converted into a humidity reading.
Advantages
- Capacitive sensors are known for higher accuracy and fast response time.
- These sensors can resist contamination, allowing them to operate in environments with dust or other pollutants.
- Capacitive humidity sensors can be designed in small form factors and consume less power, making them ideal for use in portable devices and battery-powered applications.
Limitation
- Capacitive sensors can be affected by electromagnetic interference (EMI), leading to inaccurate readings. Using proper shielding and grounding can reduce the impact of EMI and improve sensor accuracy.
Capacitive Humidity Sensor from DigiKey
2. Resistive Humidity Sensor
Resistive humidity sensors measure humidity by detecting change in resistance. The principle behind resistive humidity sensors is the fact that the conductivity in non-metallic conductors is dependent on their water content.
Resistive humidity sensors have a relatively simple structure, consisting of a hygroscopic (moisture-absorbing) material. When this material absorbs moisture, it leads to a change in resistance.
Advantages
- Due to their simple structure resistive humidity sensors are less expensive.
- These sensors are capable of providing continuous humidity monitoring, making them suitable for real-time application.
- These sensors can also work in harsh environments conditions.
Limitation
- Due to the possibility of aging or contamination of the hygroscopic material, resistive humidity sensors may require periodic calibration to ensure accuracy.
- The output reading may shift with rapidly changing environments conditions.
Resistive Humidity Sensor from DigiKey
3. Optical Humidity Sensor
Optical humidity sensors measure humidity using optical principle, when light is transmitted through the fiber, it interacts with the humidity-sensitive coating, leading to a change in the intensity or wavelength of the light signal.
By measuring this change, the sensor can determine the humidity level in the surrounding environment.
Common optical humidity sensors utilize infrared light, although some may use microwaves or ultrasonic waves for humidity sensing.
Advantages
- Optical Humidity sensors provide high sensitivity and accuracy in humidity measurement, ensuring precise monitoring in critical applications.
- These sensors are immune to electromagnetic interference, making them ideal for use in environments with high levels of interference such as power plants and telecommunications infrastructure.
- Fiber optic sensors react quickly because they can detect changes instantly. This makes them ideal for places where conditions change rapidly.
- Optical humidity sensors allow non-contact, real-time measurements across a wide range of humidity levels, making them ideal for fast-response applications.
Limitation
- Optical humidity sensors typically require regular calibration to ensure measurement accuracy.
- They are more expensive than other humidity sensors due to complex components and materials.
- Fiber-optic humidity sensors can lose accuracy over time as their sensitive materials degrade, especially in tough conditions.
4. Surface Strain Humidity Sensor
A surface strain humidity sensor measures humidity by detecting physical deformation of a moisture-sensitive material. The core of this type of sensor consists of a material or coating that responds to changes in humidity by altering its shape; when these materials absorb moisture, the material undergoes physical deformation (bends or stretches) which leads to changes in surface strain.
Advantages
- Surface strain humidity sensors are typically highly sensitive to humidity changes; they are designed to detect even small changes in humidity.
- Due to their simple structure, these sensors often exhibit high reliability and can continue to function properly even in harsh conditions.
- They have fast response times, enabling them to respond in real-time to changes in humidity within the environment.
Limitation
- The materials used in these sensors can affect their performance, Different materials have varying characteristics and application ranges, which can affect sensor accuracy and suitability for specific environments.
- The reliability and lifespan of these sensors can be influenced by the environmental conditions, including exposure to extreme temperatures, chemicals, or other harsh conditions.
- Advanced materials and complex measurement methods can make these sensors more expensive and complicated than traditional ones. However, there’s ongoing work to make them more affordable and easier to use.
5. Electrochemical Humidity Sensor
An electrochemical humidity sensor measures humidity based on the principle of electrochemical reactions.
The sensor consists of an electrolyte or a conductive polymer. As humidity increases, water molecules interact with the electrolyte, changing its electrical properties, such as resistance or capacitance. This change in electrical properties is measured and converted into a corresponding humidity reading.
Advantages
- Electrochemical sensors are very sensitive and can detect even small changes in humidity.
- These sensors usually have a relatively fast response time, which make them useful for real-time monitoring and control.
- These sensors are energy-efficient, making them suitable for portable or battery-operated devices.
Limitation
- Due to the impact of electrolyte aging and other factors, electrochemical humidity sensors typically require regular calibration to ensure accuracy.
- The performance of electrochemical humidity sensors may be affected by temperature changes, requiring consideration for accuracy at different temperatures.
6. Thermal Humidity Sensor
A thermal humidity sensor measures humidity by using the principles of thermal conductivity or heat scattering. Thermal scattering utilizes the scattering effect of water vapor on heat, while thermal conductivity is based on the influence of water vapor on heat conduction.
They typically employ heating devices and sensor devices like thermocouples or thermistors to measure heat conduction or scattering, allowing inference of the surrounding environmental humidity levels.
Advantages
- Thermal humidity sensors are typically highly sensitive to humidity changes and can provide accurate humidity measurements.
- These sensors respond quickly to changes in humidity, providing real-time measurements.
- They are generally less affected by dust, chemical substances or other contaminants, allowing them to operate normally even in environments with corrosive gasses present.
Limitation
- Thermal sensors can be more expensive than other types of humidity sensors due to their complex design.
Thermal Humidity Sensor from DigiKey
7. Semiconductor IC Humidity Sensor
Semiconductor IC humidity sensors use integrated circuits (IC) to measure humidity in the air.
The sensor is made of a semiconductor material, usually with a polymer or oxide layer that absorbs moisture. As the humidity changes, the electrical properties of the material change. These changes are measured by the IC and converted into a humidity reading.
Advantages
- Semiconductor IC humidity sensors offer greater reliability and are easy to integrate into electronic devices due to their small size.
- These sensors typically offer fast response times, allowing them to provide real-time feedback on humidity changes.
- These sensors offer high accuracy and consume very little power, which is ideal for battery-operated or portable devices.
- Most semiconductor IC humidity sensors provide output digital signals, making data processing and integration easy.
Limitation
- Semiconductor IC humidity sensors may need temperature adjustment to stay accurate and may be less effective in extreme humidity or temperature conditions.
Applications of Different Humidity Sensors
| Sensor Type | Applications |
|---|---|
| Capacitive Humidity Sensor | Ideal for applications requiring high accuracy and resistance to contamination. Consumer electronics (smartphones, tablets), HVAC systems, weather stations, environmental monitoring |
| Resistive Humidity Sensor | Suitable for environments where real-time monitoring is needed and cost is a factor.Industrial processes, agricultural settings, home appliances (dehumidifiers, humidifiers) |
| Optical Humidity Sensor | Ideal for situations where high sensitivity and accuracy are required, and where electromagnetic interference is a concern. Telecommunications infrastructure, power plants, laboratories. |
| Surface Strain Humidity Sensor | Suitable for environments where fast response and high sensitivity are needed. Advanced research, aerospace and manufacturing. |
| Electrochemical Humidity Sensor | Useful for applications requiring high sensitivity and energy efficiency. Medical devices, portable electronics, environmental monitoring systems |
| Thermal Humidity Sensor | Suitable for areas where high sensitivity and resistance to contaminants are important. Industrial environments, environmental testing, HVAC systems. |
| Semiconductor IC Humidity Sensor | Ideal for applications needing compact size, low power consumption, and fast response times.Consumer electronics, wearable devices, battery-operated gadgets. |
Common issues and solutions of humidity sensors
-
Temperature Fluctuations: Opt for sensors that offer temperature compensation and try to keep the sensor environment stable.
-
Calibration: Regularly calibrate your sensors to maintain accuracy, even if they have automatic features. Use reliable calibration standards and do manual checks periodically.
-
Contaminants: Keep the sensor clean to prevent dust and pollutants from affecting its performance. Using dust covers or shields can also help.
-
Drift: Over time, sensors can drift in performance. Regular inspections and calibrations are essential. Choose sensors with adjustable calibration and follow the manufacturer’s guidelines.
-
Extreme Conditions: Be aware that sensors might not work well in very high or low humidity. Pick sensors that fit your specific humidity range and calibrate them as needed in extreme conditions.
Conclusion
In summary, humidity sensors play a vital role in many different applications. Choosing the right sensor type for your specific needs is key to getting accurate and stable readings. Each type has its own pros and cons, so knowing what each one offers helps you pick the best fit. Regularly calibrating and maintaining your sensor is also important to keep it accurate over time. By focusing on the right sensor and proper care, you’ll ensure reliable and consistent humidity measurements, no matter the environment.
Humidity Sensors and Expansion Boards, Daughter Cards from DigiKey
Applicable Part Numbers
| DigiKey Part Number | Manufacturer Part Number |
|---|---|
| 1649-SHT40I-AD1B-R3TR-ND,1649-SHT40I-AD1B-R3CT-ND,1649-SHT40I-AD1B-R3DKR-ND | SHT40I-AD1B-R3 |
| 1649-SHT40-AD1B-R2TR-ND,1649-SHT40-AD1B-R2CT-ND,1649-SHT40-AD1B-R2DKR-ND | SHT40-AD1B-R2 |
| 1649-SHT40-AD1B-R3TR-ND,1649-SHT40-AD1B-R3CT-ND,1649-SHT40-AD1B-R3DKR-ND | SHT40-AD1B-R3 |
| 1649-SHT30-DIS-B10KSTR-ND,1649-SHT30-DIS-B10KSCT-ND,1649-SHT30-DIS-B10KSDKR-ND | SHT30-DIS-B10KS |
| 1649-SHTC3-TR-2.5KSTR-ND,1649-SHTC3-TR-2.5KSCT-ND,1649-SHTC3-TR-2.5KSDKR-ND | SHTC3-TR-2.5KS |
| 1649-SHTC3-TR-10KSTR-ND,1649-SHTC3-TR-10KSCT-ND,1649-SHTC3-TR-10KSDKR-ND | SHTC3-TR-10KS |
| 296-52638-2-ND,296-52638-1-ND,296-52638-6-ND | HDC2080DMBR |
| 2618-ENS210-LQFMTR-ND,2618-ENS210-LQFMCT-ND,2618-ENS210-LQFMDKR-ND | ENS210-LQFM |
| 296-HDC2021DEBRTR-ND,296-HDC2021DEBRCT-ND,296-HDC2021DEBRDKR-ND | HDC2021DEBR |
| 296-47774-2-ND,296-47774-1-ND,296-47774-6-ND | HDC2010YPAR |
| 296-46272-2-ND,296-46272-1-ND,296-46272-6-ND | HDC1080DMBR |
| 1649-SHT41-AD1B-R3TR-ND,1649-SHT41-AD1B-R3CT-ND | SHT41-AD1B-R3 |
| 1649-SHT41-AD1B-R2TR-ND,1649-SHT41-AD1B-R2CT-ND,1649-SHT41-AD1B-R2DKR-ND | SHT41-AD1B-R2 |
| 1649-1009-2-ND,1649-1009-1-ND,1649-1009-6-ND | SHT30-DIS-B2.5KS |
| 1649-1010-2-ND,1649-1010-1-ND,1649-1010-6-ND | SHT30-ARP-B |
| 800-HS4003TR-ND,800-HS4003CT-ND,800-HS4003DKR-ND | HS4003 |
| 296-HDC3020DEFRTR-ND,296-HDC3020DEFRCT-ND,296-HDC3020DEFRDKR-ND | HDC3020DEFR |
| 223-1595-2-ND,223-1595-1-ND | HPP845E131R5 |
| 1649-SHT41I-AD1B-R2TR-ND,1649-SHT41I-AD1B-R2CT-ND,1649-SHT41I-AD1B-R2DKR-ND | SHT41I-AD1B-R2 |
| 1649-SHT41-AD1F-R2TR-ND,1649-SHT41-AD1F-R2CT-ND,1649-SHT41-AD1F-R2DKR-ND | SHT41-AD1F-R2 |
| 296-HDC3022QDEJRQ1-ND | HDC3022QDEJRQ1 |
| 296-HDC2022DEPRTR-ND,296-HDC2022DEPRCT-ND,296-HDC2022DEPRDKR-ND | HDC2022DEPR |
| 1649-1082-2-ND,1649-1082-1-ND,1649-1082-6-ND | SHT30-DIS-P2.5KS |
| 296-HDC3021DEHRTR-ND,296-HDC3021DEHRCT-ND,296-HDC3021DEHRDKR-ND | HDC3021DEHR |
| 223-1591-2-ND,223-1591-1-ND | HPP845E031R5 |
| 296-HDC3022DEJRTR-ND,296-HDC3022DEJRCT-ND,296-HDC3022DEJRDKR-ND | HDC3022DEJR |
| 1649-1065-2-ND,1649-1065-1-ND,1649-1065-6-ND | SHT30-DIS-F2.5KS |
| 1649-1011-2-ND,1649-1011-1-ND,1649-1011-6-ND | SHT31-DIS-B2.5KS |
| 1649-SHT43-ADCB-R2TR-ND,1649-SHT43-ADCB-R2CT-ND,1649-SHT43-ADCB-R2DKR-ND | SHT43-ADCB-R2 |
| 1649-1083-2-ND,1649-1083-1-ND,1649-1083-6-ND | SHT31-DIS-P2.5KS |
| 828-1063-2-ND,828-1063-1-ND,828-1063-6-ND | BME280 |
| 1649-SHT31A-DIS-B2.5KSTR-ND,1649-SHT31A-DIS-B2.5KSCT-ND,1649-SHT31A-DIS-B2.5KSDKR-ND | SHT31A-DIS-B2.5KS |
| 223-10142048-20TR-ND,223-10142048-20CT-ND,223-10142048-20DKR-ND | 10142048-20 |
| 1649-1066-2-ND,1649-1066-1-ND,1649-1066-6-ND | SHT31-DIS-F2.5KS |
| 1649-1004-2-ND,1649-1004-1-ND,1649-1004-6-ND | SHT20 |
| 1649-SHT45-AD1B-R2TR-ND,1649-SHT45-AD1B-R2CT-ND,1649-SHT45-AD1B-R2DKR-ND | SHT45-AD1B-R2 |
| 800-3830-ND | HS3001 |
| 223-1144-2-ND,223-1144-1-ND,223-1144-6-ND | HPP845E031R4 |
| 336-4348-2-ND,336-4348-1-ND,336-4348-6-ND | SI7006-A20-IM1R |
| 1649-SHT45-AD1F-R2TR-ND,1649-SHT45-AD1F-R2CT-ND,1649-SHT45-AD1F-R2DKR-ND | SHT45-AD1F-R2 |
| 1649-SHT35-DIS-B10KSTR-ND,1649-SHT35-DIS-B10KSCT-ND,1649-SHT35-DIS-B10KSDKR-ND | SHT35-DIS-B10KS |
| HPP801A031-ND | HPP801A031 |
| 1649-1007-2-ND,1649-1007-1-ND,1649-1007-6-ND | SHT21S |
| 336-3139-ND | SI7020-A20-IM1 |
| 1649-1005-2-ND,1649-1005-1-ND,1649-1005-6-ND | SHT21 |
| 1649-1062-2-ND,1649-1062-1-ND,1649-1062-6-ND | SHT35-DIS-B2.5KS |
| 336-4380-2-ND,336-4380-1-ND,336-4380-6-ND | SI7021-A20-GM1R |
| 1649-1067-2-ND,1649-1067-1-ND,1649-1067-6-ND | SHT35-DIS-F2.5KS |
| SI7013-A20-GM1RTR-ND,SI7013-A20-GM1RCT-ND,SI7013-A20-GM1RDKR-ND | SI7013-A20-GM1R |
| 1649-SHT35A-DIS-B2.5KSTR-ND,1649-SHT35A-DIS-B2.5KSCT-ND,1649-SHT35A-DIS-B2.5KSDKR-ND | SHT35A-DIS-B2.5KS |
| 235-1335-ND | CC2D23S |
| 480-5704-2-ND,480-5704-1-ND,480-5704-6-ND | HIH6030-021-001 |
| 1649-1008-2-ND,1649-1008-1-ND,1649-1008-6-ND | SHT25 |
| 1738-SEN0385-ND | SEN0385 |
| 480-3651-2-ND,480-3651-1-ND,480-3651-6-ND | HIH6130-021-001 |
| 1738-1353-ND | SEN0227 |
| 1528-4099-ND | 4099 |
| 480-5580-2-ND,480-5580-1-ND | HIH6121-021-001 |
| 480-3652-2-ND,480-3652-1-ND,480-3652-6-ND | HIH6131-021-001 |
| 2952-HYT.271.P.0.SKSAS_5GLOBTOP-ND | HYT.271.P.0.SKSAS_5 GLOBTOP |
| 480-3294-2-ND,480-3294-1-ND,480-3294-6-ND | HIH-5030-001 |
| 2952-HYT221-ND | HYT 221 |
| 235-1563-ND | T9602-3-D |
| 1597-114992867-ND | 114992867 |
| 235-1378-ND | T9602-5-D-1 |
| 480-3168-2-ND,480-3168-1-ND | HIH-4031-001 |
| 480-3284-2-ND,480-3284-1-ND,480-3284-6-ND | HIH-5031-001 |
| 235-1380-ND | T9602-5-A-1 |
| 480-2905-ND | HIH-4000-001 |
| 480-4961-ND | HIH-4021-003 |
| 480-2906-ND | HIH-4000-003 |
| 480-6987-ND | HIH8131-021-001S |
| 480-4965-ND | HIH-4602-L-CP |
| 1859-1019-ND | MNS2-9-IN-HU-RH |
| 480-3178-ND | HIH-4602-C |
| 480-4963-ND | HIH-4602-A |
| 1649-SHT40-CD1B-R3TR-ND,1649-SHT40-CD1B-R3CT-ND,1649-SHT40-CD1B-R3DKR-ND | SHT40-CD1B-R3 |
| 1649-SHT40-BD1B-R3TR-ND,1649-SHT40-BD1B-R3CT-ND,1649-SHT40-BD1B-R3DKR-ND | SHT40-BD1B-R3 |
| 1649-SHT40-BD1B-R2TR-ND,1649-SHT40-BD1B-R2CT-ND,1649-SHT40-BD1B-R2DKR-ND | SHT40-BD1B-R2 |
| 223-10142048-32TR-ND,223-10142048-32CT-ND | 10142048-32 |
| 1649-SHT41I-AD1B-R3TR-ND,1649-SHT41I-AD1B-R3CT-ND,1649-SHT41I-AD1B-R3DKR-ND | SHT41I-AD1B-R3 |
| 1649-SHT40-BD1F-R2TR-ND,1649-SHT40-BD1F-R2CT-ND,1649-SHT40-BD1F-R2DKR-ND | SHT40-BD1F-R2 |
| 1649-SHT40I-AD1B-R2TR-ND,1649-SHT40I-AD1B-R2CT-ND,1649-SHT40I-AD1B-R2DKR-ND | SHT40I-AD1B-R2 |
| 223-1592-2-ND,223-1592-1-ND | HPP845E034R5 |
| 1649-SHT30A-DIS-B10KSTR-ND,1649-SHT30A-DIS-B10KSCT-ND,1649-SHT30A-DIS-B10KSDKR-ND | SHT30A-DIS-B10KS |
| 732-2525020210002TR-ND,732-2525020210002CT-ND,732-2525020210002DKR-ND | 2.52502E+12 |
| 1649-SHT40I-HD1B-R2TR-ND,1649-SHT40I-HD1B-R2CT-ND,1649-SHT40I-HD1B-R2DKR-ND | SHT40I-HD1B-R2 |
| 1649-SHT40A-AD1B-R2TR-ND,1649-SHT40A-AD1B-R2CT-ND,1649-SHT40A-AD1B-R2DKR-ND | SHT40A-AD1B-R2 |
| 1649-SHT40I-AD1F-R2TR-ND,1649-SHT40I-AD1F-R2CT-ND,1649-SHT40I-AD1F-R2DKR-ND | SHT40I-AD1F-R2 |
| 296-44907-2-ND,296-44907-1-ND,296-44907-6-ND | HDC1010YPAR |
| 1649-SHT40I-HD1F-R2TR-ND,1649-SHT40I-HD1F-R2CT-ND,1649-SHT40I-HD1F-R2DKR-ND | SHT40I-HD1F-R2 |
| 223-10142048-31TR-ND,223-10142048-31CT-ND | 10142048-31 |
| 223-10142048-22TR-ND,223-10142048-22CT-ND,223-10142048-22DKR-ND | 10142048-22 |
| 1528-2564-ND | 3721 |
| 1649-SHT41A-AD1B-R2TR-ND,1649-SHT41A-AD1B-R2CT-ND | SHT41A-AD1B-R2 |
| 1778-1179-ND | COM1700 |
| 1649-SHT30A-DIS-B2.5KSTR-ND,1649-SHT30A-DIS-B2.5KSCT-ND,1649-SHT30A-DIS-B2.5KSDKR-ND | SHT30A-DIS-B2.5KS |
| 1528-5183-ND | 5183 |
| 800-3832-ND | HS3003 |
| 235-1449-ND | HS12SP |
| 296-HDC3020QDEFRQ1TR-ND,296-HDC3020QDEFRQ1CT-ND,296-HDC3020QDEFRQ1DKR-ND | HDC3020QDEFRQ1 |
| 223-1594-2-ND,223-1594-1-ND,223-1594-6-ND | HPP845E131R4 |
| 296-HDC3021QDEHRQ1TR-ND,296-HDC3021QDEHRQ1CT-ND,296-HDC3021QDEHRQ1DKR-ND | HDC3021QDEHRQ1 |
| 800-HS4001TR-ND,800-HS4001CT-ND,800-HS4001DKR-ND | HS4001 |
| 800-HS4011TR-ND,800-HS4011CT-ND,800-HS4011DKR-ND | HS4011 |
| 1568-SEN-18364-ND | SEN-18364 |
| 1649-SHT45-AD1B-R3TR-ND,1649-SHT45-AD1B-R3CT-ND,1649-SHT45-AD1B-R3DKR-ND | SHT45-AD1B-R3 |
| 1738-SEN0546-ND | SEN0546 |
| 336-3125-ND | SI7006-A20-IM1 |
| 1649-SHT31A-DIS-B10KSTR-ND,1649-SHT31A-DIS-B10KSCT-ND,1649-SHT31A-DIS-B10KSDKR-ND | SHT31A-DIS-B10KS |
| 235-1450-ND | HS30P |
| 336-3596-2-ND,336-3596-1-ND,336-3596-6-ND | SI7020-A20-GM1R |
| 336-3137-ND | SI7020-A20-GM1 |
| 1649-1006-2-ND,1649-1006-1-ND,1649-1006-6-ND | SHT21P |
| 235-1334-ND | CC2A23 |
| 1649-SHT33-DIS-B2.5KSTR-ND,1649-SHT33-DIS-B2.5KSCT-ND,1649-SHT33-DIS-B2.5KSDKR-ND | SHT33-DIS-B2.5KS |
| 336-4900-2-ND,336-4900-1-ND,336-4900-6-ND | SI7020-A20-IM1R |
| 336-3141-ND | SI7021-A20-GM1 |
| 235-1343-ND | CC2D33 |
| 336-4349-2-ND,336-4349-1-ND,336-4349-6-ND | SI7021-A20-IM1R |
| 336-3143-ND | SI7021-A20-IM1 |
| 1649-1111-ND | SCC30-DB |
| 235-1338-ND | CC2D25 |
| 336-4487-2-ND,336-4487-1-ND,336-4487-6-ND | SI7021-A20-YM1R |
| BC2325-ND | HUMIDITY-SENS-E |
| 480-5706-2-ND,480-5706-1-ND | HIH8120-021-001 |
| HIH7120-021-001TR-ND,HIH7120-021-001CT-ND | HIH7120-021-001 |
| 45-CC2D25-SIP-ND | CC2D25-SIP |
| 223-1244-ND | HPP808H031 |
| HPP805D033-ND | HPP805D033 |
| 480-5705-2-ND,480-5705-1-ND,480-5705-6-ND | HIH7131-000-001 |
| 1528-5182-ND | 5182 |
| 235-1564-ND | T9602-5-A |
| 480-HIH-4031-003-ND | HIH-4031-003 |
| 480-3537-ND | HIH-4010-002 |
| 445-2578-ND | CHS-UPS |
| 480-4967-ND | HIH-5031-001S |
| 480-3538-ND | HIH-4021-001 |
| 480-4959-ND | HIH-4010-004 |
| 480-4960-ND | HIH-4020-001 |
| 1859-1018-ND | MNS2-9-W2-HU-RH |
| 480-4964-ND | HIH-4602-L |
| 800-3831-ND | HS3002 |
| 223-1888-2-ND,223-1888-1-ND,223-1888-6-ND | HTU20DF |
| 223-10142048-30TR-ND,223-10142048-30CT-ND | 10142048-30 |
| 223-1887-2-ND,223-1887-1-ND,223-1887-6-ND | HTU20D |
| 223-1590-2-ND,223-1590-1-ND | HPP845E031R1 |
| 235-1341-ND | CC2D33S |
| 296-42616-2-ND,296-42616-1-ND,296-42616-6-ND,2156-HDC1050DMBR-ND | HDC1050DMBR |
| 235-1336-ND | CC2D25S |
| 336-3147-ND | SI7023-A20-IM1 |
| 45-CC2D35-ND | CC2D35 |
| 235-1361-ND | CC2D23S-SIP |
| 235-1364-ND | CC2D35-SIP |
| 235-1365-ND | CC2D33S-SIP |
| HIH7130-000-001TR-ND,HIH7130-000-001CT-ND | HIH7130-000-001 |
| 480-6383-2-ND,480-6383-1-ND,480-6383-6-ND | HIH6131-000-001 |
| 445-2576-ND | CHS-MSS |
| 2952-P142FWTHERMO_5(P0K1)-ND | P14 2FW THERMO_5 (P0K1) |
| 2952-MK33-W(300PF+/-40PF)-ND | MK33-W (300PF +/-40PF) |
| 235-1562-ND | T9602-3-A |
| 480-3536-ND | HIH-4010-001 |
| 480-3736-ND | HIH-4000-004 |
| 480-3539-ND | HIH-4021-002 |
| 480-4962-ND | HIH-4021-004 |
| 1859-1017-ND | MNS2-9-W1-HU-RH |
| 336-4542-ND | SI7020-A20-YM1 |
| 235-1589-2-ND,235-1589-1-ND,235-1589-6-ND | CC2D23S-2500 |
| 336-3145-ND | SI7022-A20-IM1 |
| 235-1333-ND | CC2A25 |
| 445-2575-ND | CHS-GSS |
| 2618-ENS211-LQFMTR-ND,2618-ENS211-LQFMCT-ND,2618-ENS211-LQFMDKR-ND | ENS211-LQFM |
| 2618-ENS210A-LQFMTR-ND,2618-ENS210A-LQFMCT-ND,2618-ENS210A-LQFMDKR-ND | ENS210A-LQFM |
| 1649-SHT40I-BD1B-R3TR-ND,1649-SHT40I-BD1B-R3CT-ND,1649-SHT40I-BD1B-R3DKR-ND | SHT40I-BD1B-R3 |
| 2618-ENS212-LQFMTR-ND,2618-ENS212-LQFMCT-ND,2618-ENS212-LQFMDKR-ND | ENS212-LQFM |
| 1649-SHT40A-FD1B-R3TR-ND,1649-SHT40A-FD1B-R3CT-ND,1649-SHT40A-FD1B-R3DKR-ND | SHT40A-FD1B-R3 |
| 1649-SHT40A-AD1B-R3TR-ND,1649-SHT40A-AD1B-R3CT-ND,1649-SHT40A-AD1B-R3DKR-ND | SHT40A-AD1B-R3 |
| 1649-SHT40A-AW1B-R3TR-ND,1649-SHT40A-AW1B-R3CT-ND,1649-SHT40A-AW1B-R3DKR-ND | SHT40A-AW1B-R3 |
| 1649-SHT40A-FD1B-R2TR-ND,1649-SHT40A-FD1B-R2CT-ND,1649-SHT40A-FD1B-R2DKR-ND | SHT40A-FD1B-R2 |
| 1649-SHT40A-AW1B-R2TR-ND,1649-SHT40A-AW1B-R2CT-ND,1649-SHT40A-AW1B-R2DKR-ND | SHT40A-AW1B-R2 |
| 1649-SHT41A-AD1B-R3TR-ND,1649-SHT41A-AD1B-R3CT-ND,1649-SHT41A-AD1B-R3DKR-ND | SHT41A-AD1B-R3 |
| 1649-SHT41A-AW1B-R3TR-ND,1649-SHT41A-AW1B-R3CT-ND,1649-SHT41A-AW1B-R3DKR-ND | SHT41A-AW1B-R3 |
| 1649-SHT41A-BD1B-R3TR-ND,1649-SHT41A-BD1B-R3CT-ND,1649-SHT41A-BD1B-R3DKR-ND | SHT41A-BD1B-R3 |
| 1649-SHT41A-FD1B-R2TR-ND,1649-SHT41A-FD1B-R2CT-ND,1649-SHT41A-FD1B-R2DKR-ND | SHT41A-FD1B-R2 |
| 1649-SHT41A-AW1B-R2TR-ND,1649-SHT41A-AW1B-R2CT-ND,1649-SHT41A-AW1B-R2DKR-ND | SHT41A-AW1B-R2 |
| 1649-SHT41A-BD1B-R2TR-ND,1649-SHT41A-BD1B-R2CT-ND,1649-SHT41A-BD1B-R2DKR-ND | SHT41A-BD1B-R2 |
| 2618-ENS215-LQFMTR-ND,2618-ENS215-LQFMCT-ND,2618-ENS215-LQFMDKR-ND | ENS215-LQFM |
| 118-BPS240-D2P0-S10ETR-ND,118-BPS240-D2P0-S10ECT-ND,118-BPS240-D2P0-S10EDKR-ND | BPS240-D2P0-S10E |
| 1649-SHT33-DIS-B10KSTR-ND,1649-SHT33-DIS-B10KSCT-ND,1649-SHT33-DIS-B10KSDKR-ND | SHT33-DIS-B10KS |
| 5621-MVH4004D-ND | MVH4004D |
| 5621-MVH4003D-ND | MVH4003D |
| 5621-MVH4002D-ND | MVH4002D |
| 5621-MVH4001D-ND | MVH4001D |
| 800-HS4013TR-ND,800-HS4013CT-ND,800-HS4013DKR-ND | HS4013 |
| 800-HS4113TR-ND,800-HS4113CT-ND,800-HS4113DKR-ND | HS4113 |
| 800-HS4111TR-ND,800-HS4111CT-ND,800-HS4111DKR-ND | HS4111 |
| 3083-LEME-24V-ND | LEME-24V |
| 2740-SD-Z1-ND | SD-Z1 |
| 2740-SD-ND | SD |
| 1597-114991730-ND | 114991730 |
| 2740-SD-RO1-ND | SD-RO1 |
| 2266-HIH6131-021-001S-ND,480-6685-ND | HIH6131-021-001S |
| 2740-SD-Z-ND | SD-Z |
| 2740-SC-R-3-ND | SC-R-3 |
| 2740-SC-10-ND | SC-10 |
| 5532-OFT005-C-ND | OFT005-C |
| 2726-EE046-T11-ND | EE046-T11 |
| 2740-SC-17-ND | SC-17 |
| 2740-SC-ZH-3-ND | SC-ZH-3 |
| 2740-SC-R-10-ND | SC-R-10 |
| 2740-SC-25-ND | SC-25 |
| 2740-SC-R-17-ND | SC-R-17 |
| 2740-SC-ZH-10-ND | SC-ZH-10 |
| 5532-OFT010-B-ND | OFT010-B |
| 3244-SEM710HM/W/HP01-ND | SEM710HM/W/HP01 |
| 2740-SC-ZH-17-ND | SC-ZH-17 |
| 2740-SC-R-25-ND | SC-R-25 |
| 2740-SC-ZH-25-ND | SC-ZH-25 |
| 2726-EE160-M1T1A6-ND | EE160-M1T1A6 |
| 2726-EE160-M1T2A6-ND | EE160-M1T2A6 |
| 2740-SC-50-ND | SC-50 |
| 2740-SC-ZH-50-ND | SC-ZH-50 |
| 2740-SC-R-50-ND | SC-R-50 |
| 2740-SC-100-ND | SC-100 |
| 2740-SC-ZH-100-ND | SC-ZH-100 |
| 2740-SC-R-100-ND | SC-R-100 |
| 5532-OFT001-C-ND | OFT001-C |
| 5532-OFT420-C-ND | OFT420-C |
| 5532-OFT010-C-ND | OFT010-C |
| 5532-OFT020-C-ND | OFT020-C |
| 5532-OFT025-C-ND | OFT025-C |
| 5532-OHT20-C-ND | OHT20-C |
| 5532-OHT20-B-ND | OHT20-B |
| 5532-OFT420-B-ND | OFT420-B |
| 5532-OFT025-B-ND | OFT025-B |
| 5532-OFT005-B-ND | OFT005-B |
| 5532-OHT20T-C-ND | OHT20T-C |
| 5532-OFT001-B-ND | OFT001-B |
| 5532-OFT020-B-ND | OFT020-B |
| 3244-SEM710HM/D/HP01-ND | SEM710HM/D/HP01 |
| 5532-OHT20T-B-ND | OHT20T-B |
| 5532-OFT020-A-ND | OFT020-A |
| 5532-OFT420-A-ND | OFT420-A |
| 5532-OFT010-A-ND | OFT010-A |
| 5532-OFT005-A-ND | OFT005-A |
| 5532-OFT025-A-ND | OFT025-A |
| 5532-OFT001-A-ND | OFT001-A |
| 5532-OHT20-A-ND | OHT20-A |
| 5532-OHT20T-A-ND | OHT20T-A |
| 2726-EE211-M1A6D2AM7-ND | EE211-M1A6D2AM7 |
| 1528-5181-ND | 5181 |
| 1738-SEN0438-ND | SEN0438 |
| 1597-101990881-ND | 101990881 |
| 2952-153435-ND | 153435 |
| 235-1377-ND | T9602-3-D-1 |
| 2170-S24AS-D-MQP-ND | S24AS-D-MQP |
| 4008-TM1SHTM4-ND | TM1SHTM4 |
| 1528-5064-ND | 5064 |
| 1528-4881-ND | 4881 |
| 336-3129-ND | SI7013-A20-GM1 |
| 2952-P14-W_5(150PF+/-50PF)-ND | P14-W_5 (150PF +/-50PF) |
| 1738-1242-ND | SEN0148 |
| 2952-P14RAPID2_5-ND | P14 RAPID 2_5 |
| 235-1565-ND | T9602-5-D |
| 2084-96PD-THS16B-ND | 96PD-THS16B |
| 2330-LDH290-ND | LDH290 |
| 45-T8700-D-ND | T8700-D |
| 45-HUMI-DP-XR-O-ND | HUMI-DP-XR-O |
| 45-HUMI-WB-XR-O-ND | HUMI-WB-XR-O |
| 1855-1052-ND | A1DU5P2CP006B |
| 235-1363-ND | CC2D33-SIP |
| 45-HS-20-ND | HS-20 |
| 235-1362-ND | CC2D25S-SIP |
| 235-1359-ND | CC2D23-SIP |
| 1528-5023-ND | 5023 |
| 445-2577-ND | CHS-UGS |
| 480-4966-ND | HIH-5030-001S |
| 2170-DX80N9Q45THA-ND | DX80N9Q45THA |
| 45-EHRH-2-I-B-ND | EHRH-2-I-B |
| 45-EHRH-2-V10-B-ND | EHRH-2-V10-B |
| 45-HUMI-DP-XR-D-ND | HUMI-DP-XR-D |
| 45-EHRHT-2-I-F-6-ND | EHRHT-2-I-F-6 |
| 45-EHRHT-2-I-B-6-ND | EHRHT-2-I-B-6 |
| 235-1340-ND | CC2A33 |
| 235-1342-ND | CC2D35S |
| 235-1366-ND | CC2D35S-SIP |
| 336-4544-ND | SI7021-A20-YM1 |
| 445-CHS-UGR-ND | CHS-UGR |
| 235-1379-ND | T9602-3-A-1 |
| 445-2579-ND | CHS-UPR |
| 1597-101990564-ND | 101990564 |
| 45-HUMI-DP-XR-S-ND | HUMI-DP-XR-S |
| 45-EHRHT-2-I-B-3-ND | EHRHT-2-I-B-3 |
| 45-EHRHT-2-I-F-3-ND | EHRHT-2-I-F-3 |
| 45-EHRHT-2-I-B-5-ND | EHRHT-2-I-B-5 |
| 45-EHRHT-2-I-F-2-ND | EHRHT-2-I-F-2 |
| 45-EHRHT-2-I-B-4-ND | EHRHT-2-I-B-4 |
| 45-HUMI-WB-XR-S-ND | HUMI-WB-XR-S |
| 45-HUMI-EN-XR-D-ND | HUMI-EN-XR-D |
| 45-EHRH-2-I-F-1-ND | EHRH-2-I-F-1 |
| 1084-1018-ND | HSM100 |
| 2952-K5_5(200PF+/-50PF)-ND | K5_5 (200PF +/-50PF) |
| 45-T8700-E-D-ND | T8700-E-D |
| 45-T8700-E-ND | T8700-E |
| 45-T8700-E-GN-ND | T8700-E-GN |
| 45-T8700-GN-ND | T8700-GN |
| 45-T8700-ND | T8700 |
| 45-T8700-E-D-GN-ND | T8700-E-D-GN |
| 223-1593-ND | HPP845E131R1 |
| 480-5581-2-ND,480-5581-1-ND | HIH6120-021-001 |
| 1737-1004-ND | S03/S04 |
| 1661-1086-ND | WBP-WL-01-3F |
| 5016-EZO-HUM-P-P-ND | EZO-HUM-P-P |
| 1661-1087-ND | WBP-SC-0015-01 |
| 2752-IMS-4820ETB-ND | IMS-4820E |
| 2266-HIH7121-021-001S-ND,HIH7121-021-001S-ND | HIH7121-021-001S |
| 2752-FGD-0052TB-ND | FGD-0052 |
| 5016-EZO-HUM-P-ND | EZO-HUM-P |
| 3588-8804000101-ND | 8804000101 |
| 2283-S3120E-ND | S3120E |
| 2752-IMS-4821ETB-ND | IMS-4821E |
| 2283-T3318-ND | T3318 |
| 2273-PR55-1E-ND | PR55-1E |
| 2283-P8611-ND | P8611 |
| 2266-HIH8120-021-001S-ND,HIH8120-021-001S-ND | HIH8120-021-001S |
| 2283-P8552-ND | P8552 |
| 2283-T3218-ND | T3218 |
| 2283-T3118-ND | T3118 |
| 2283-T3311-ND | T3311 |
| 2283-T3313-ND | T3313 |
| 2283-P8652-ND | P8652 |
| 2283-T1110-ND | T1110 |
| 2283-C3121-ND | C3121 |
| 2283-T3319-ND | T3319 |
| 2283-T3418-ND | T3418 |
| 2283-T3113-ND | T3113 |
| 2283-T0213-ND | T0213 |
| 2283-T0213D-ND | T0213D |
| 2283-U3120-ND | U3120 |
| 2283-T0211-ND | T0211 |
| 2283-T3117-ND | T3117 |
| 2283-T3111-ND | T3111 |
| 2283-T3411-ND | T3411 |
| 2283-T3413-ND | T3413 |
| 2283-D3120-ND | D3120 |
| 2283-T3417-ND | T3417 |
| 2283-T3419-ND | T3419 |
| 2283-U3631-ND | U3631 |
| 2283-D3121-ND | D3121 |
| 2283-D3631-ND | D3631 |
| 2283-C4141-ND | C4141 |
| 2283-H3020-ND | H3020 |
| 2283-H3021-ND | H3021 |
| 2283-T3110EX-ND | T3110EX |
| 2283-T3511-ND | T3511 |
| 2283-H3331-ND | H3331 |
| 2283-T3111EX-ND | T3111EX |
| 2283-D3633-ND | D3633 |
| 2283-H3060-ND | H3060 |
| 2283-D4130-ND | D4130 |
| 2283-T0211P-ND | T0211P |
| 2283-T3111P-ND | T3111P |
| 2283-H3430-ND | H3430 |
| 2283-H3061-ND | H3061 |
| 2283-D4141-ND | D4141 |
| 2283-T7411-ND | T7411 |
| 2283-H3431-ND | H3431 |
| 2283-T3419P-ND | T3419P |
| 2283-H3530-ND | H3530 |
| 2283-D3121P-ND | D3121P |
| 2283-H3531-ND | H3531 |
| 2283-H3531R-ND | H3531R |
| 2283-H3021P-ND | H3021P |
| 2283-T3511P-ND | T3511P |
| 3798-HD200-ND | HD200 |
| 3798-HR200-ND | HR200 |
| 3798-HD200-W-ND | HD200-W |
| 3798-HR200-W-ND | HR200-W |
| 2283-H3061P-ND | H3061P |
| 3798-HR200-W-M12-ND | HR200-W-M12 |
| 3798-HD200-M12-ND | HD200-M12 |
| 3798-HR200-M12-ND | HR200-M12 |
| 2283-U3631M-ND | U3631M |
| 2283-U3120M-ND | U3120M |
| 2283-H3531P-ND | H3531P |
| 4413-AM102L-ND | AM102L |
| 3798-HD200-W-M12-ND | HD200-W-M12 |
| 2726-EE354-PA2AC2-ND | EE354-PA2AC2 |
| 2726-EE310-T10PA25PC4C1-ND | EE310-T10PA25PC4C1 |
| 2726-EE310-T10K10PA25D2J3PC4C1-ND | EE310-T10K10PA25D2J3PC4C1 |
| 2726-EE33-M1T17HS3F9K5L200D2-ND | EE33-M1T17HS3F9K5L200D2 |
| 1597-101990882-ND | 101990882 |
| 4008-TM1SHC4-ND | TM1SHC4 |
| 881-RBS306-ATH-EXT-US-ND | RBS306-ATH-EXT-US |
| 2330-LDH292-ND | LDH292 |
| 2330-LDH100-ND | LDH100 |
| 149-28092-ND | 28092 |
| 45-HUMI-WB-XR-D-ND | HUMI-WB-XR-D |
| 45-EHRHT-2-I-B-1-ND | EHRHT-2-I-B-1 |
| 1597-114992648-ND | 114992648 |
| 45-EHRH-2-I-F-ND | EHRH-2-I-F |
| 1188-SNS-DH11-ND | SNS-DH11 |
| 3647-DHT11-ND | DHT11 |
| 4728-NZH-101TB-ND | NZH-101 |
| 4728-A/RH3-10K-E1-R2TB-ND | A/RH3-10K-E1-R2 |
| 2283-T3510-ND | T3510 |
| 3647-26312-ND | 26312 |
| 4728-NZH-101UTB-ND | NZH-101U |
| 4728-A/RH5-R2TB-ND | A/RH5-R2 |
| 4728-A/RH5-RTB-ND | A/RH5-R |
| 4728-A/RH5-AN-R2TB-ND | A/RH5-AN-R2 |
| 4728-A/RH5-CP-RTB-ND | A/RH5-CP-R |
| 4728-A/RH5-AN-RTB-ND | A/RH5-AN-R |
| 4728-A/RH5-CP-R2TB-ND | A/RH5-CP-R2 |
| 4728-A/RH5-DTB-ND | A/RH5-D |
| 4728-A/RH5-OTB-ND | A/RH5-O |
| 4728-A/RH5-CP-DTB-ND | A/RH5-CP-D |
| 4728-A/RH5-AN-DTB-ND | A/RH5-AN-D |
| 4728-A/RH5-CP-OTB-ND | A/RH5-CP-O |
| 4728-A/RH5-AN-OTB-ND | A/RH5-AN-O |
| 4728-A/RH3-10K-E1-RTB-ND | A/RH3-10K-E1-R |
| 4728-A/RH3-CP-R2LTB-ND | A/RH3-CP-R2L |
| 4728-A/RH3-1K-NI-R2TB-ND | A/RH3-1K-NI-R2 |
| 4728-A/RH3-1K-2W-R2TB-ND | A/RH3-1K-2W-R2 |
| 4728-A/RH3-1.8K-R2TB-ND | A/RH3-1.8K-R2 |
| 4728-A/RH3-3K-R2TB-ND | A/RH3-3K-R2 |
| 4728-A/RH3-AN-R2LTB-ND | A/RH3-AN-R2L |
| 4728-A/RH3-1K-2W-RTB-ND | A/RH3-1K-2W-R |
| 4728-A/RH3-AN-R2-05TB-ND | A/RH3-AN-R2-05 |
| 4728-A/RH3-R2OTB-ND | A/RH3-R2O |
| 4728-A/RH3-10KS-RTB-ND | A/RH3-10KS-R |
| 4728-A/RH3-3K-RTB-ND | A/RH3-3K-R |
| 4728-A/RH3-AN-BC-R2TB-ND | A/RH3-AN-BC-R2 |
| 4728-A/RH3-1K-NI-RTB-ND | A/RH3-1K-NI-R |
| 4728-A/RH3-100-2W-RTB-ND | A/RH3-100-2W-R |
| 4728-A/RH3-AN-BC-RTB-ND | A/RH3-AN-BC-R |
| 4728-A/RH3-CSI-RTB-ND | A/RH3-CSI-R |
| 4728-A/RH3-10KS-R2TB-ND | A/RH3-10KS-R2 |
| 4728-A/RH3-1K-3W-RTB-ND | A/RH3-1K-3W-R |
| 4728-A/RH3-50K-R2TB-ND | A/RH3-50K-R2 |
| 4728-A/RH3-R2S-A03-C5TB-ND | A/RH3-R2S-A03-C5 |
| 4728-A/RH3-3K-R2LTB-ND | A/RH3-3K-R2L |
| 4728-A/RH3-1.8K-RTB-ND | A/RH3-1.8K-R |
| 4728-A/RH3-CP-R-WTB-ND | A/RH3-CP-R-W |
| 4728-A/RH3-100-3W-R2TB-ND | A/RH3-100-3W-R2 |
| 4728-A/RH3-100-3W-RTB-ND | A/RH3-100-3W-R |
| 4728-A/RH3-DTB-ND | A/RH3-D |
| 4728-A/RH3-D-010TB-ND | A/RH3-D-010 |
| 4728-A/RH3-D-BBTB-ND | A/RH3-D-BB |
| 4728-A/RH3-R2TB-ND | A/RH3-R2 |
| 4728-A/RH3-RTB-ND | A/RH3-R |
| 4728-A/RH3-CP-R2SO-A11-G5TB-ND | A/RH3-CP-R2SO-A11-G5 |
| 4728-A/RH3-AN-R2OTB-ND | A/RH3-AN-R2O |
| 4728-A/RH3-SP-05TB-ND | A/RH3-SP-05 |
| 4728-A/RH3-10KS-DTB-ND | A/RH3-10KS-D |
| 4728-A/RH3-AN-BC-DTB-ND | A/RH3-AN-BC-D |
| 4728-A/RH3-CSI-DTB-ND | A/RH3-CSI-D |
| 4728-A/RH3-1K-2W-DTB-ND | A/RH3-1K-2W-D |
| 4728-A/RH3-20K-ROTB-ND | A/RH3-20K-RO |
| 4728-A/RH3-O-3.25-EHTB-ND | A/RH3-O-3.25-EH |
| 4728-A/RH3-100-2W-R2OTB-ND | A/RH3-100-2W-R2O |
| 4728-A/RH3-CP-D-BBTB-ND | A/RH3-CP-D-BB |
| 4728-A/RH3-1K-3W-DTB-ND | A/RH3-1K-3W-D |
| 4728-A/RH3-100-2W-DTB-ND | A/RH3-100-2W-D |
| 4728-A/RH3-O-BBTB-ND | A/RH3-O-BB |
| 4728-A/RH3-100KS-DTB-ND | A/RH3-100KS-D |
| 4728-A/RH3-SP-010TB-ND | A/RH3-SP-010 |
| 4728-A/RH3-3K-ROTB-ND | A/RH3-3K-RO |
| 4728-A/RH3-CP-ROTB-ND | A/RH3-CP-RO |
| 4728-A/RH3-100-3W-DTB-ND | A/RH3-100-3W-D |
| 4728-A/RH3-AN-BC-D-BBTB-ND | A/RH3-AN-BC-D-BB |
| 4728-A/RH3-AN-D-BBTB-ND | A/RH3-AN-D-BB |
| 4728-A/RH3-1K-NI-R2OTB-ND | A/RH3-1K-NI-R2O |
| 4728-A/RH3-10K-E1-DTB-ND | A/RH3-10K-E1-D |
| 4728-A/RH3-3K-DTB-ND | A/RH3-3K-D |
| 4728-A/RH3-CP-R2OTB-ND | A/RH3-CP-R2O |
| 4728-A/RH3-10K-E1-R2OTB-ND | A/RH3-10K-E1-R2O |
| 4728-A/RH3-1.8K-ROTB-ND | A/RH3-1.8K-RO |
| 4728-A/RH3-10K-E1-D-3.25-EHTB-ND | A/RH3-10K-E1-D-3.25-EH |
| 4728-A/RH3-AN-ROTB-ND | A/RH3-AN-RO |
| 4728-A/RH3-1K-2W-ROTB-ND | A/RH3-1K-2W-RO |
| 4728-A/RH3-1K-NI-DTB-ND | A/RH3-1K-NI-D |
| 4728-A/RH3-AN-RS-A16-C5TB-ND | A/RH3-AN-RS-A16-C5 |
| 4728-A/RH3-CP-R2S-A13-C5TB-ND | A/RH3-CP-R2S-A13-C5 |
| 4728-A/RH3-1.8K-DTB-ND | A/RH3-1.8K-D |
| 4728-A/RH3-1K-NI-R2S-A09-G5TB-ND | A/RH3-1K-NI-R2S-A09-G5 |
| 4728-A/RH3-CP-RS-A01-C5TB-ND | A/RH3-CP-RS-A01-C5 |
| 4728-A/RH3-AN-R2S-A03-C5TB-ND | A/RH3-AN-R2S-A03-C5 |
| 4728-A/RH3-AN-R2LOTB-ND | A/RH3-AN-R2LO |
| 4728-A/RH3-50K-DTB-ND | A/RH3-50K-D |
| 4728-A/RH3-CP-R2LOTB-ND | A/RH3-CP-R2LO |
| 4728-A/RH3-AN-RS-A02-C5TB-ND | A/RH3-AN-RS-A02-C5 |
| 4728-A/RH3-CP-R2S-A02-G5TB-ND | A/RH3-CP-R2S-A02-G5 |
| 4728-A/RH3-3K-R2OTB-ND | A/RH3-3K-R2O |
| 4728-A/RH3-100-2W-D-BBTB-ND | A/RH3-100-2W-D-BB |
| 4728-A/RH3-CP-R2S-A03-C5TB-ND | A/RH3-CP-R2S-A03-C5 |
| 4728-A/RH3-AN-R2S-A08-G5TB-ND | A/RH3-AN-R2S-A08-G5 |
| 4728-A/RH3-CP-RS-A04-C5TB-ND | A/RH3-CP-RS-A04-C5 |
| 4728-A/RH3-AN-RS-A03-C5TB-ND | A/RH3-AN-RS-A03-C5 |
| 4728-A/RH3-AN-R2S-A03-G5TB-ND | A/RH3-AN-R2S-A03-G5 |
| 4728-A/RH3-CP-RS-A03-C5TB-ND | A/RH3-CP-RS-A03-C5 |
| 4728-A/RH3-10K-E1-ROTB-ND | A/RH3-10K-E1-RO |
| 4728-A/RH3-CP-D-3.25-BBTB-ND | A/RH3-CP-D-3.25-BB |
| 4728-A/RH3-CP-R2S-A09-G5TB-ND | A/RH3-CP-R2S-A09-G5 |
| 4728-A/RH3-10K-E1-D-BBTB-ND | A/RH3-10K-E1-D-BB |
| 4728-A/RH3-BALCO-DTB-ND | A/RH3-BALCO-D |
| 4728-A/RH3-R2SO-A03-G5TB-ND | A/RH3-R2SO-A03-G5 |
| 4728-A/RH3-100-2W-ROTB-ND | A/RH3-100-2W-RO |
| 4728-A/RH3-20K-R2S-A03-C5TB-ND | A/RH3-20K-R2S-A03-C5 |
| 4728-A/RH3-10K-E1-RS-A03-A1TB-ND | A/RH3-10K-E1-RS-A03-A1 |
| 4728-A/RH5-TT100-O-4X-4TB-ND | A/RH5-TT100-O-4X-4 |
| 4728-A/RH3-20K-R2TB-ND | A/RH3-20K-R2 |
| 4728-A/RH3-AN-R2TB-ND | A/RH3-AN-R2 |
| 4728-A/RH3-CP-R2TB-ND | A/RH3-CP-R2 |
| 4728-A/RH3-AN-RTB-ND | A/RH3-AN-R |
| 4728-A/RH3-20K-RTB-ND | A/RH3-20K-R |
| 4728-A/RH3-D-4XTB-ND | A/RH3-D-4X |
| 4728-A/RH3-1K-2W-OTB-ND | A/RH3-1K-2W-O |
| 4728-A/RH3-CP-SP-05TB-ND | A/RH3-CP-SP-05 |
| 4728-A/RH3-1K-NI-O-BBTB-ND | A/RH3-1K-NI-O-BB |
| 4728-A/RH3-AN-BC-OTB-ND | A/RH3-AN-BC-O |
| 4728-A/RH3-10KS-OTB-ND | A/RH3-10KS-O |
| 4728-A/RH3-AN-SP-010TB-ND | A/RH3-AN-SP-010 |
| 4728-A/RH3-AN-R2SO-A03-D3TB-ND | A/RH3-AN-R2SO-A03-D3 |
| 4728-A/RH3-1K-NI-OTB-ND | A/RH3-1K-NI-O |
| 4728-A/RH3-1K-NI-SP-05TB-ND | A/RH3-1K-NI-SP-05 |
| 4728-A/RH3-100-2W-OTB-ND | A/RH3-100-2W-O |
| 4728-A/RH3-100KS-OTB-ND | A/RH3-100KS-O |
| 4728-A/RH3-CSI-O-BBTB-ND | A/RH3-CSI-O-BB |
| 4728-A/RH3-CSI-OTB-ND | A/RH3-CSI-O |
| 4728-A/RH3-BALCO-OTB-ND | A/RH3-BALCO-O |
| 4728-A/RH3-3K-OTB-ND | A/RH3-3K-O |
| 4728-A/RH3-CP-O-BBTB-ND | A/RH3-CP-O-BB |
| 4728-A/RH3-CP-R2SO-A04-C5TB-ND | A/RH3-CP-R2SO-A04-C5 |
| 4728-A/RH3-CP-R2SO-A01-C5TB-ND | A/RH3-CP-R2SO-A01-C5 |
| 4728-A/RH3-AN-RSO-A03-A1TB-ND | A/RH3-AN-RSO-A03-A1 |
| 4728-A/RH3-CP-SP-010TB-ND | A/RH3-CP-SP-010 |
| 4728-A/RH3-100-3W-OTB-ND | A/RH3-100-3W-O |
| 4728-A/RH3-AN-RSO-A01-C5TB-ND | A/RH3-AN-RSO-A01-C5 |
| 4728-A/RH3-AN-SP-05TB-ND | A/RH3-AN-SP-05 |
| 4728-A/RH3-3K-R2SO-A07-G5TB-ND | A/RH3-3K-R2SO-A07-G5 |
| 4728-A/RH3-AN-RSO-A03-C5TB-ND | A/RH3-AN-RSO-A03-C5 |
| 4728-A/RH3-100-3W-SP-010TB-ND | A/RH3-100-3W-SP-010 |
| 4728-A/RH3-20K-R2SO-A14-C5TB-ND | A/RH3-20K-R2SO-A14-C5 |
| 4728-A/RH3-1.8K-SP-010TB-ND | A/RH3-1.8K-SP-010 |
| 4728-A/RH3-1K-2W-SP-010TB-ND | A/RH3-1K-2W-SP-010 |
| 4728-A/RH3-CP-R2SO-A01-G5TB-ND | A/RH3-CP-R2SO-A01-G5 |
| 4728-A/RH3-CP-RSO-A01-C5TB-ND | A/RH3-CP-RSO-A01-C5 |
| 4728-A/RH3-20K-SP-010TB-ND | A/RH3-20K-SP-010 |
| 4728-A/RH3-CP-RSO-A08-C5TB-ND | A/RH3-CP-RSO-A08-C5 |
| 4728-A/RH3-AN-R2SO-A03-B4TB-ND | A/RH3-AN-R2SO-A03-B4 |
| 4728-A/RH3-AN-R2SO-A02-G5TB-ND | A/RH3-AN-R2SO-A02-G5 |
| 4728-A/RH3-50K-SP-05TB-ND | A/RH3-50K-SP-05 |
| 4728-A/RH3-1.8K-OTB-ND | A/RH3-1.8K-O |
| 4728-A/RH3-CP-RSO-A04-C5TB-ND | A/RH3-CP-RSO-A04-C5 |
| 4728-A/RH3-50K-SP-010TB-ND | A/RH3-50K-SP-010 |
| 4728-A/RH3-50K-OTB-ND | A/RH3-50K-O |
| 4728-A/RH3-CP-R2SO-A08-C5TB-ND | A/RH3-CP-R2SO-A08-C5 |
| 4728-A/RH3-CSI-RSO-A29-C5TB-ND | A/RH3-CSI-RSO-A29-C5 |
| 4728-A/RH3-AN-R2SO-A03-G5TB-ND | A/RH3-AN-R2SO-A03-G5 |
| 4728-A/RH3-CP-R2SO-A03-G5TB-ND | A/RH3-CP-R2SO-A03-G5 |
| 4728-A/RH3-3K-O-BBTB-ND | A/RH3-3K-O-BB |
| 4728-A/RH3-CP-RSO-A03-C5TB-ND | A/RH3-CP-RSO-A03-C5 |
| 4728-A/RH3-10K-E1-SP-010TB-ND | A/RH3-10K-E1-SP-010 |
| 4728-A/RH3-CP-DTB-ND | A/RH3-CP-D |
| 4728-A/RH3-20K-DTB-ND | A/RH3-20K-D |
| 4728-A/RH3-AN-DTB-ND | A/RH3-AN-D |
| 4728-A/RH3-OTB-ND | A/RH3-O |
| 4728-A/RH3-1K-2W-D-4XTB-ND | A/RH3-1K-2W-D-4X |
| 4728-A/RH3-100-2W-D-4XTB-ND | A/RH3-100-2W-D-4X |
| 4728-A/RH3-AN-D-4XTB-ND | A/RH3-AN-D-4X |
| 4728-A/RH3-O-4XTB-ND | A/RH3-O-4X |
| 4728-A/RH3-CP-D-4XTB-ND | A/RH3-CP-D-4X |
| 4728-A/RH3-AN-BC-D-4XTB-ND | A/RH3-AN-BC-D-4X |
| 4728-A/RH3-20K-D-4XTB-ND | A/RH3-20K-D-4X |
| 4728-A/RH3-1K-NI-D-4XTB-ND | A/RH3-1K-NI-D-4X |
| 4728-A/RH3-3K-D-4XTB-ND | A/RH3-3K-D-4X |
| 4728-A/RH3-CP-O-4XTB-ND | A/RH3-CP-O-4X |
| 4728-A/RH3-CP-OTB-ND | A/RH3-CP-O |
| 4728-A/RH3-20K-OTB-ND | A/RH3-20K-O |
| 4728-A/RH3-3K-O-4XTB-ND | A/RH3-3K-O-4X |
| 4728-A/RH3-1K-NI-O-4XTB-ND | A/RH3-1K-NI-O-4X |
| 4728-A/RH3-AN-OTB-ND | A/RH3-AN-O |
| 4728-A/RH3-20K-O-4XTB-ND | A/RH3-20K-O-4X |
| 4728-A/RH3-AN-O-4XTB-ND | A/RH3-AN-O-4X |
| 4728-A/RH3-10K-E1-D-4XTB-ND | A/RH3-10K-E1-D-4X |
| 4728-A/RH3-1K-2W-O-4XTB-ND | A/RH3-1K-2W-O-4X |
| 4728-A/RH3-1K-3W-O-4XTB-ND | A/RH3-1K-3W-O-4X |
| 4728-A/RH3-10K-E1-O-4XTB-ND | A/RH3-10K-E1-O-4X |
| 4728-A/RH3-BALCO-O-4XTB-ND | A/RH3-BALCO-O-4X |
| 4728-RH3-1K-NI-SP-010TB-ND | RH3-1K-NI-SP-010 |
| 4728-A/RH2-D-BBTB-ND | A/RH2-D-BB |
| 4728-A/RH2-D-3.25-BBTB-ND | A/RH2-D-3.25-BB |
| 4728-A/RH2-D-3.25-EHTB-ND | A/RH2-D-3.25-EH |
| 4728-A/RH2-AN-R2S-A03-B4TB-ND | A/RH2-AN-R2S-A03-B4 |
| 4728-A/RH2-10K-E1-R2TB-ND | A/RH2-10K-E1-R2 |
| 4728-A/RH2-1K-2W-R2TB-ND | A/RH2-1K-2W-R2 |
| 4728-A/RH2-20K-R2TB-ND | A/RH2-20K-R2 |
| 4728-A/RH2-100-2W-R2TB-ND | A/RH2-100-2W-R2 |
| 4728-A/RH2-100-3W-RTB-ND | A/RH2-100-3W-R |
| 4728-A/RH2-AN-BC-RTB-ND | A/RH2-AN-BC-R |
| 4728-A/RH2-1K-NI-RTB-ND | A/RH2-1K-NI-R |
| 4728-A/RH2-3K-R2TB-ND | A/RH2-3K-R2 |
| 4728-A/RH2-AN-R2LTB-ND | A/RH2-AN-R2L |
| 4728-A/RH2-20K-RTB-ND | A/RH2-20K-R |
| 4728-A/RH2-1K-NI-R2TB-ND | A/RH2-1K-NI-R2 |
| 4728-A/RH2-CSI-R2TB-ND | A/RH2-CSI-R2 |
| 4728-A/RH2-100-3W-R2TB-ND | A/RH2-100-3W-R2 |
| 4728-A/RH2-10K-E1-RTB-ND | A/RH2-10K-E1-R |
| 4728-A/RH2-3K-RTB-ND | A/RH2-3K-R |
| 4728-A/RH2-100KS-RTB-ND | A/RH2-100KS-R |
| 4728-A/RH2-CP-R2LTB-ND | A/RH2-CP-R2L |
| 4728-A/RH2-CSI-RTB-ND | A/RH2-CSI-R |
| 4728-A/RH2-ROTB-ND | A/RH2-RO |
| 4728-A/RH2-1K-2W-RTB-ND | A/RH2-1K-2W-R |
| 4728-A/RH2-100-2W-RTB-ND | A/RH2-100-2W-R |
| 4728-A/RH3-50K-RTB-ND | A/RH3-50K-R |
| 4728-A/RH2-1.8K-R2TB-ND | A/RH2-1.8K-R2 |
| 4728-A/RH2-10KS-R2TB-ND | A/RH2-10KS-R2 |
| 4728-A/RH2-50K-RTB-ND | A/RH2-50K-R |
| 4728-A/RH2-50K-R2TB-ND | A/RH2-50K-R2 |
| 4728-A/RH2-R2OTB-ND | A/RH2-R2O |
| 4728-A/RH2-100KS-R2TB-ND | A/RH2-100KS-R2 |
| 4728-A/RH2-10KS-RTB-ND | A/RH2-10KS-R |
| 4728-A/RH2-1K-3W-R2TB-ND | A/RH2-1K-3W-R2 |
| 4728-A/RH2-1.8K-RTB-ND | A/RH2-1.8K-R |
| 4728-A/RH2-1K-3W-RTB-ND | A/RH2-1K-3W-R |
| 4728-A/RH3-R-NISTTB-ND | A/RH3-R-NIST |
| 4728-A/RH3-R2-NISTTB-ND | A/RH3-R2-NIST |
| 4728-A/RH2-AN-BC-DTB-ND | A/RH2-AN-BC-D |
| 4728-A/RH2-CP-D-3.25-BBTB-ND | A/RH2-CP-D-3.25-BB |
| 4728-A/RH2-100-2W-DTB-ND | A/RH2-100-2W-D |
| 4728-A/RH2-AN-D-BBTB-ND | A/RH2-AN-D-BB |
| 4728-A/RH2-O-BBTB-ND | A/RH2-O-BB |
| 4728-A/RH2-10K-E1-DTB-ND | A/RH2-10K-E1-D |
| 4728-A/RH2-SP-05TB-ND | A/RH2-SP-05 |
| 4728-A/RH2-BALCO-DTB-ND | A/RH2-BALCO-D |
| 4728-A/RH2-CSI-DTB-ND | A/RH2-CSI-D |
| 4728-A/RH2-CP-D-3.25-EHTB-ND | A/RH2-CP-D-3.25-EH |
| 4728-A/RH2-10KS-DTB-ND | A/RH2-10KS-D |
| 4728-A/RH2-1K-2W-DTB-ND | A/RH2-1K-2W-D |
| 4728-A/RH2-1K-NI-DTB-ND | A/RH2-1K-NI-D |
| 4728-A/RH2-100KS-DTB-ND | A/RH2-100KS-D |
| 4728-A/RH2-CP-D-BBTB-ND | A/RH2-CP-D-BB |
| 4728-A/RH2-50K-DTB-ND | A/RH2-50K-D |
| 4728-A/RH2-1.8K-DTB-ND | A/RH2-1.8K-D |
| 4728-A/RH2-10K-E1-D-BBTB-ND | A/RH2-10K-E1-D-BB |
| 4728-A/RH2-AN-BC-D-BBTB-ND | A/RH2-AN-BC-D-BB |
| 4728-A/RH2-R2TB-ND | A/RH2-R2 |
| 4728-A/RH2-RTB-ND | A/RH2-R |
| 4728-A/RH2-CP-R2OTB-ND | A/RH2-CP-R2O |
| 4728-A/RH2-AN-R2S-A03-G5TB-ND | A/RH2-AN-R2S-A03-G5 |
| 4728-A/RH2-10K-E1-ROTB-ND | A/RH2-10K-E1-RO |
| 4728-A/RH2-3K-ROTB-ND | A/RH2-3K-RO |
| 4728-A/RH2-AN-ROTB-ND | A/RH2-AN-RO |
| 4728-A/RH2-CP-ROTB-ND | A/RH2-CP-RO |
| 4728-A/RH2-CSI-ROTB-ND | A/RH2-CSI-RO |
| 4728-A/RH2-AN-RS-A02-C5TB-ND | A/RH2-AN-RS-A02-C5 |
| 4728-A/RH2-1K-NI-R2S-A09-G5TB-ND | A/RH2-1K-NI-R2S-A09-G5 |
| 4728-A/RH2-CP-RS-A03-C5TB-ND | A/RH2-CP-RS-A03-C5 |
| 4728-A/RH2-CP-RS-A01-C5TB-ND | A/RH2-CP-RS-A01-C5 |
| 4728-A/RH2-CP-R2S-A01-G5TB-ND | A/RH2-CP-R2S-A01-G5 |
| 4728-A/RH2-AN-RS-A01-C5TB-ND | A/RH2-AN-RS-A01-C5 |
| 4728-A/RH2-AN-R2S-A01-G5TB-ND | A/RH2-AN-R2S-A01-G5 |
| 4728-A/RH2-CP-R2S-A10-B4TB-ND | A/RH2-CP-R2S-A10-B4 |
| 4728-A/RH2-CP-RS-A02-C5TB-ND | A/RH2-CP-RS-A02-C5 |
| 4728-A/RH2-AN-R2LS-A03-C5TB-ND | A/RH2-AN-R2LS-A03-C5 |
| 4728-A/RH3-D-NISTTB-ND | A/RH3-D-NIST |
| 4728-A/RH2-100KS-ROTB-ND | A/RH2-100KS-RO |
| 4728-A/RH2-AN-R2OTB-ND | A/RH2-AN-R2O |
| 4728-A/RH2-1K-2W-RS-A09-C5TB-ND | A/RH2-1K-2W-RS-A09-C5 |
| 4728-A/RH2-AN-R2LOTB-ND | A/RH2-AN-R2LO |
| 4728-A/RH2-20K-RS-A24-C5TB-ND | A/RH2-20K-RS-A24-C5 |
| 4728-A/RH2-AN-R2S-A16-B4TB-ND | A/RH2-AN-R2S-A16-B4 |
| 4728-A/RH2-1K-2W-ROTB-ND | A/RH2-1K-2W-RO |
| 4728-A/RH3-CP-R-NISTTB-ND | A/RH3-CP-R-NIST |
| 4728-A/RH2-100-2W-ROTB-ND | A/RH2-100-2W-RO |
| 4728-A/RH2-CP-R2S-A03-G5TB-ND | A/RH2-CP-R2S-A03-G5 |
| 4728-A/RH2-CP-R2S-A03-C5TB-ND | A/RH2-CP-R2S-A03-C5 |
| 4728-A/RH3-20K-R-NISTTB-ND | A/RH3-20K-R-NIST |
| 4728-A/RH2-1K-2W-R2S-A10-A1TB-ND | A/RH2-1K-2W-R2S-A10-A1 |
| 4728-A/RH2-D-4XTB-ND | A/RH2-D-4X |
| 4728-A/RH2-DTB-ND | A/RH2-D |
| 4728-A/RH2-100-3W-OTB-ND | A/RH2-100-3W-O |
| 4728-A/RH2-CP-SP-010TB-ND | A/RH2-CP-SP-010 |
| 4728-A/RH2-1K-2W-SP-010TB-ND | A/RH2-1K-2W-SP-010 |
| 4728-A/RH2-1K-2W-OTB-ND | A/RH2-1K-2W-O |
| 4728-A/RH2-1K-NI-SP-010TB-ND | A/RH2-1K-NI-SP-010 |
| 4728-A/RH2-AN-O-BBTB-ND | A/RH2-AN-O-BB |
| 4728-A/RH2-1.8K-OTB-ND | A/RH2-1.8K-O |
| 4728-A/RH2-AN-SP-05TB-ND | A/RH2-AN-SP-05 |
| 4728-A/RH2-1.8K-SP-010TB-ND | A/RH2-1.8K-SP-010 |
| 4728-A/RH2-CP-O-BBTB-ND | A/RH2-CP-O-BB |
| 4728-A/RH2-3K-OTB-ND | A/RH2-3K-O |
| 4728-A/RH2-AN-BC-OTB-ND | A/RH2-AN-BC-O |
| 4728-A/RH2-100-2W-OTB-ND | A/RH2-100-2W-O |
| 4728-A/RH2-CSI-OTB-ND | A/RH2-CSI-O |
| 4728-A/RH2-1K-NI-OTB-ND | A/RH2-1K-NI-O |
| 4728-A/RH2-20K-SP-010TB-ND | A/RH2-20K-SP-010 |
| 4728-A/RH2-10K-E1-SP-010TB-ND | A/RH2-10K-E1-SP-010 |
| 1738-1039-ND | SEN0137 |
| 1528-4885-ND | 4885 |
| 1597-101990644-ND | 101990644 |
| 1528-5665-ND | 5665 |
| 1528-2444-ND | 3660 |
| 2648-SC0329-ND | SC0329 |
| 828-EVALUATIONKITBOARDBME688-ND | EVALUATION KIT BOARD BME688 |
| 1528-5187-ND | 5187 |
| 1597-101020952-ND | 101020952 |
| 1528-4566-ND | 4566 |
| 2221-U001-C-ND | U001-C |
| 1528-1771-ND | 3251 |
| 1568-SEN-16467-ND | SEN-16467 |
| 1597-1653-ND | 101020513 |
| 1568-SEN-22395-ND | SEN-22395 |
| 1778-PIM458-ND | PIM458 |
| 1597-1737-ND | 101020634 |
| 223-1786-ND | DPP902S000 |
| 2266-2JCIE-EV01-RP1-ND,39-2JCIE-EV01-RP1-ND | 2JCIE-EV01-RP1 |
| 223-1712-ND,2266-DPP901Z000-ND | DPP901Z000 |
| 1471-MIKROE-3775-ND | MIKROE-3775 |
| 2266-2JCIE-EV01-FT1-ND,39-2JCIE-EV01-FT1-ND | 2JCIE-EV01-FT1 |
| 223-1714-ND,2266-DPP301A000-ND | DPP301A000 |
| 2266-DPP901A000-ND,223-1718-ND | DPP901A000 |
| 223-1708-ND,2266-DPP301Z000-ND | DPP301Z000 |
| 2266-DPP904R000-ND,223-1788-ND | DPP904R000 |
| 1738-SEN0528-ND | SEN0528 |
| 1568-SEN-22396-ND | SEN-22396 |
| 1528-5046-ND | 5046 |
| 1528-5190-ND | 5190 |
| 1528-5776-ND | 5776 |
| 2221-U001-D-ND | U001-D |
| 1528-4636-ND | 4636 |
| 1738-SEN0428-ND | SEN0428 |
| 1738-1089-ND | DFR0067 |
| 1597-1138-ND | 101020019 |
| 1597-1387-ND | 101020212 |
| 1471-MIKROE-5651-ND | MIKROE-5651 |
| 1528-4716-ND | 4716 |
| 1286-1153-ND | 410-347 |
| 1738-1312-ND | SEN0236 |
| 1597-1684-ND | 101020592 |
| 1568-SEN-15440-ND | SEN-15440 |
| 1738-1383-ND | SEN0248 |
| 2221-U169-ND | U169 |
| 1471-MIKROE-5301-ND | MIKROE-5301 |
| 1568-SEN-16466-ND | SEN-16466 |
| 296-50806-ND | BOOSTXL-BASSENSORS |
| 1471-1487-ND | MIKROE-1978 |
| 20-US082-HS3001EVZ-ND | US082-HS3001EVZ |
| 1568-SEN-19096-ND | SEN-19096 |
| 1471-MIKROE-4893-ND | MIKROE-4893 |
| 1738-SEN0501-ND | SEN0501 |
| 828-SHUTTLEBOARD3.0BHI360-ND | SHUTTLE BOARD 3.0 BHI360 |
| 2221-U104-ND | U104 |
| 1778-PIM635-ND | PIM635 |
| 2266-2JCIE-EV01-AR1-ND,39-2JCIE-EV01-AR1-ND | 2JCIE-EV01-AR1 |
| 2221-U053-D-ND | U053-D |
| 1832-1023-ND | ASD2511-R-T |
| 1471-2123-ND | MIKROE-3331 |
| 223-1783-ND | DPP301G000 |
| 497-14896-ND | STEVAL-MKI141V2 |
| 223-1785-ND | DPP901G000 |
| 828-SHUTTLEBOARD3.0BME280-ND | SHUTTLE BOARD 3.0 BME280 |
| 1778-PIM486-ND | PIM486 |
| 1832-1055-ND | ASD2511-R-N-T-P-L |
| 2508-SENSORSHIELDKIT-ND | SENSOR SHIELD KIT |
| 1927-5697-ND | 5697 |
| 2266-2331211-3-ND,A141304-ND | 2331211-3 |
| 2266-2331211-1-ND,A141302-ND | 2331211-1 |
| 2266-2331211-2-ND,A141303-ND | 2331211-2 |
| 1471-MIKROE-5952-ND | MIKROE-5952 |
| 1471-MIKROE-5736-ND | MIKROE-5736 |
| 1738-SEN0500-ND | SEN0500 |
| 1471-MIKROE-6241-ND | MIKROE-6241 |
| 1471-MIKROE-5761-ND | MIKROE-5761 |
| 1471-MIKROE-5546-ND | MIKROE-5546 |
| 4411-ST0248-ND | ST0248 |
| 5032-333035-ND | 333035 |
| 5016-EZO-HUM-C-ND | EZO-HUM-C |
| 2266-DPP301A00-ND | DPP301A00 |
| 5303-BE-SHEN-ND | BE-SHEN |
| 1738-SEN0414-ND | SEN0414 |
| 1597-101020932-ND | 101020932 |
| 1597-1124-ND | 101020011 |
| 1738-DFR0588-ND | DFR0588 |
| 1528-4832-ND | 4832 |
| 1471-MIKROE-4496-ND | MIKROE-4496 |
| 1738-SEN0331-ND | SEN0331 |
| 1568-1522-ND | DEV-13956 |
| 1597-101021032-ND | 101021032 |
| 1471-MIKROE-4979-ND | MIKROE-4979 |
| 1738-SEN0497-ND | SEN0497 |
| 1471-MIKROE-4316-ND | MIKROE-4316 |
| 1738-SEN0332-ND | SEN0332 |
| 1738-SEN0334-ND | SEN0334 |
| 1528-4535-ND | 4535 |
| 1832-AST1025-ND | AST1025 |
| 1471-2126-ND | MIKROE-3270 |
| 1471-MIKROE-3635-ND | MIKROE-3635 |
| 1471-1951-ND | MIKROE-2937 |
| 1471-MIKROE-4892-ND | MIKROE-4892 |
| 1471-1981-ND | MIKROE-2938 |
| 1471-2183-ND | MIKROE-3469 |
| 1568-DEV-15837-ND | DEV-15837 |
| 1471-2176-ND | MIKROE-3436 |
| 1471-MIKROE-4306-ND | MIKROE-4306 |
| 1471-MIKROE-4733-ND | MIKROE-4733 |
| 1471-MIKROE-3984-ND | MIKROE-3984 |
| 1832-AST1036-ND | AST1036 |
| 1471-MIKROE-4558-ND | MIKROE-4558 |
| 1778-1216-ND | PIM355 |
| 1471-MIKROE-4702-ND | MIKROE-4702 |
| 1471-1363-ND | MIKROE-1687 |
| 1471-MIKROE-4348-ND | MIKROE-4348 |
| 1471-1464-ND | MIKROE-1798 |
| 296-BP-BASSENSORSMKII-ND | BP-BASSENSORSMKII |
| 1471-2104-ND | MIKROE-3263 |
| 1471-MIKROE-4878-ND | MIKROE-4878 |
| 828-SHUTTLEBOARD3.0BME680-ND | SHUTTLE BOARD 3.0 BME680 |
| 1471-1616-ND | MIKROE-2101 |
| 497-18506-ND | STEVAL-MKI187V1 |
| 1471-MIKROE-4907-ND | MIKROE-4907 |
| 1471-1849-ND | MIKROE-2467 |
| 2198-104001000100-ND | 1.04001E+11 |
| 732-2501000201291-ND | 2.501E+12 |
| 1568-SEN-18632-ND | SEN-18632 |
| 1597-1002-ND | 101020074 |
| 1471-1401-ND | MIKROE-1797 |
| 1738-SEN0527-ND | SEN0527 |
| 1188-MOD-BME280-ND | MOD-BME280 |
| 1528-5989-ND | 5989 |
| 1471-MIKROE-5310-ND | MIKROE-5310 |
| 1471-MIKROE-5872-ND | MIKROE-5872 |
| 1471-MIKROE-5526-ND | MIKROE-5526 |
| 3647-26410-ND | 26410 |
| 1568-SPX-16618-ND | SPX-16618 |
| 5032-333045-ND | 333045 |
| 5032-333032-ND | 333032 |
| 1890-1024-ND | 11032 |
| SPX-15074-ND | SPX-15074 |
| 5032-333036-ND | 333036 |
| 1597-101100002-ND | 101100002 |
| 101020193-ND | 101020193 |
| 1471-1503-ND | MIKROE-1971 |
| 1471-2026-ND | MIKROE-3085 |
| 1471-2102-ND | MIKROE-3272 |
| 1471-2142-ND | MIKROE-3342 |
| 1471-MIKROE-4922-ND | MIKROE-4922 |
| 1568-SPX-14570-ND | SPX-14570 |
| 101990054-ND | 101990054 |
| 1471-1886-ND | MIKROE-2818 |
| 1471-2177-ND | MIKROE-3425 |
| 800-QCIOT-HS4001POCZ-ND | QCIOT-HS4001POCZ |
| 1471-MIKROE-5240-ND | MIKROE-5240 |
| 1927-5336-ND | 5336 |
| 1568-SPX-18976-ND | SPX-18976 |
| 1568-SPX-18365-ND | SPX-18365 |
| 1568-DEV-19630-ND | DEV-19630 |
| 1568-SPX-18366-ND | SPX-18366 |
| 2234-HUMI-01-ND | HUMI-01 |
| 1649-1114-ND | ARDUINO SHIELD SGPC3_SHTC3 |
| 1649-SEK-SHTC3-SENSORS-ND | SEK-SHTC3-SENSORS |
| 4735-RAK1901-0-SS-N-ND | RAK1901-0-SS-N |
| 1649-1097-ND | SEK-SHTXX/SGP30 |
More Posts on Humidity Sensors:
- Product Selection Guide for Humidity, Moisture Sensors - Design Tools and Resources
- Integrating Temperature and Humidity Sensing on a Chip