We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I am using Kicad 4.0.0 version. I found an issue in integrating the ICM-2948 with Package TFQFN-24 on PCB where track is not allowing to connect through IC’s Pad. Either pads are close enough to resist the track to connect or pass through.
I have not used version 4 for many years, but I doubt this is a limitation therein.
I do not believe I understand your request correctly. Are you saying that you can not connect a track/trace to a pad on the ICM-20948? Can you send a screenshot of the issue?
So here is the screenshot, I had started the Route Track option in order to connect the ICM-20948, but when I clicked the pad of IC in order to start the trace, it would start.
With Regards
Maninder
The default clearances on a new PCB project are usually set to around 8 mills (0.2 mm), which is too tight to get a trace to connect to a pad on a tight pitch QFN package. Meaning the clearance of one pad will interfere with the trace as it connects to another pad.
Depending on which board house you chose to use for fabricating your PCBs, the clearance from one signal to another can usually be tighter that the default in KiCad. (Most board houses will specify a minimum space and trace)
You can change the minimum clearances in the Design Rules dialog box. If you use net classes, the clearance will need to be changed for each class. If you use the default class for all nets, you will only need to change the one. Clearances of 6 mills (0.1524 mm) worked well for me with the 24QFN package. The width of your trace will also play an effect on being able to connect, mine was at 9.84 mills (0.25 mm) at the time I got this to work.