It’s an old Holley Projection TBI. It works OK, but I’ve got the control box out because I’m refurbing the rest of the Jeep and I’m noticing that the pots (it’s a manual adjust unit) are damaged and I’d like to replace them. There’s a manufacturer (Piher) and a number on them, but it’s not turning up anything in a search. I’ll put the numbers below and pictures if that will help.
1K641M (This one works in reverse, 0 is fully clockwise and max is CCW, but I’m not sure that matters)
100K614M
10K643M
Considering that these control an air fuel adjustment it seems to me that linear would be better than audio. Also, the legs are staggered with the two outside legs on the front and the single middle leg on the back of the unit. and I think it would be nice to have panel mounts since it would help keep them from being damaged every time they got bumped. It would also help prevent dirt and water from getting inside the control box.
Any help getting the proper replacements for these would be great.