I have a Lenovo IdeaPad 3 15itl6, employee broke screen an the connection on motherboard for the video cam was loose and seeking replacement.
There are so many different connector I am seeking assistance on identifying the actual part # on DigiKey
![20240904_231339|666x500]
(upload://5yKE1IeRJL5oZ9Z8c7PR1JXVjxm.jpeg)
Hello Cndweinland, and welcome to the DigiKey TechForum.
It appears that you would be looking for something like 455-2191-ND, if we are to assume that the distance from pin 1 to 10 is 11/32 inches this would be the closest I could find.
If we are to assume pin 1 to 3 is 1/16 inches, we do have 2057-08CH-A-10-G-IDC-ND that may work for you.
It is hard to be certain at that scale. If you are able to provide a more accurate measurements, we may be able to find something else that is closer or confirm if one of these would work for you.
Are there any other connectors that might work? I’d probably just get both to be safe. I dont have anything with 1/16
BM10B-SRSS-TB is the type of connection I am looking for. I want to get confirmation of what header I actually need in order to have it solder to the board for the connection.
Hi @cndweinland ,
It appears you have 0.8mm pitch, although we do stock BM10B-SRSS-TB which is 1.0mm pitch. You will see a few of the mating connectors for the products mentioned towards the bottom of their product page. Hopefully one of those would work for you.