Importing the Digi-Key KiCad Library into KiCad 5.0.0+

There are several different ways to manage third party libraries like this one. Using git clone is a great way to keep it up to date.

How you decide to manage the library(s) within KiCad is open to debate, but the way I prefer to use them is to pull them in to the Project Libraries, that way they are managed separately from the default libraries, this can be done as such:

  1. git clone https://github.com/Digi-Key/digikey-kicad-library.git into your preferred directory

  2. Open KiCad

  3. Import the symbols:

    A. Open Symbol Editor or Schematic editor

    image

    B. Click on Preferences then on Manage Symbol Libraries…

    image

    C. Click on the Project Specific Libraries tab:

    image

    D. Click on the Add existing library to table button:

    image

    E. Navigate to the directory where you cloned the Digi-Key KiCad Library

    F. Navigate to the digikey-symbols folder within digikey-kicad-library folder

    image

    G. At this point you can add one library at a time or all of the libraries. To add all of the libraries click on any one of the the libraries and then press Ctrl+a. This will select all of the libraries, then click the Open button.

    H. You should now see the libraries in the table:

    image

  4. Import the footprints(similar process to symbols):

    A. Open Footprint editor or PCB Layout

    image

    B. Click on Preferences then on Manage Footprint Libraries…

    image

    C. Click on the Project Specific Libraries tab:

    image

    D. Click on the Add existing library to table button:

    image

    E. Navigate to the directory where you cloned the Digi-Key KiCad Library

    F. Expand the digikey-kicad-library folder and select digikey-footprints.pretty

    image

    G. Click OK

    H. The digikey-footprints should now show in your library table

    image

Hi, migrating to KiCad and was looking for LED2472GBTR - is it missing or am I missing something? Thanks, Mike