Input Voltage of 72-WX2024N-ND

------Question for WX2024N Please Put your question below------

Hi Support team,

May I know the input voltage for this soldering station?

Thanks,
Medlyn

Hi @medlyn.manalu.mm ,

Welcome to DigiKey TechForum and thanks for your inquiry.

According to the specification:
Datasheet_WX2024N.pdf (248.1 KB)

The Weller WX2024N soldering station has an input voltage of 120 V AC (typically specified as 115–120 V, 60 Hz).

:white_check_mark: Key Electrical Specs

  • Input Voltage: 120 V AC
  • Power Consumption: 200 W (up to 255 W peak)
  • Channels: 2
  • Temperature Range: 100 °C – 550 °C (210 °F – 999 °F)
  • Fuse: T2A

Do you have the same station but with a 220 VAC input? I want to use this tool in Indonesia.

Or do you perhaps have a converter from 220 VAC to 120 VAC?

Hello,

I was able to locate some Higher voltage units that should work for your needs. Please take a look at the link below.

220-240VAC solder stations

Thank you
Ryan

1 Like

Thank you.

If I want to buy this set + knife tip

Please provide me the link. Thank you very much for your help.

Hello medlyn.manalu.mm,

The part number for this soldering station, is WX2021N-ND.

You can click on the part number, or the link is https://www.digikey.com/en/products/detail/apex-tool-group/WX2021N/2608021.

This will also be rated for 120VAC, and will have the NEMA 5-15 plug.

As I mentioned above, I need the higher voltage (220-240VAC). I found the station T0053420699, but not for the set. If you don’t mind, please provide me the link of the products related to the picture I’ve attached above.

Looking at Weller’s site, the soldering station that you are looking for is limited for sale only from European distributors.