JST SH 4-pin to JST PH 3-pin wires/adapter

I need a JST SH 4-pin to JST PH 3-pin wires adapter to connect a Adafruit QT Py to an Adafruit MOSFET Driver. The QT Py has a JST SH 4-pin and the MOSFET Driver has a JST PH 3-pin socket.

Here are the parts I’m using.:
MOSFET DriverAdafruit QT Py ESP32-S3 WiFi Dev Board with STEMMA QT [8 MB Flash / No PSRAM] : ID 5426 : Adafruit Industries, Unique & fun DIY electronics and kits

Hello,

The only JST part I found was on the JST web site. STEMMA QT / Qwiic JST SH 4-pin to Premium Male Headers Cable - 150mm Long. Is what they show.

The Adafruit part number is 4209, DigiKey part number 1528-4209-ND

I do not see any type of 3 to 4 pin adapter from JST.

The connector on the Adafruit MOSFET Driver 5648 is meant only for V+, signal, and ground. The Adafruit board 5426 has a connector that is meant to be used with I2C. To send signal to the driver board you are going to need to use a different pin that is not SDA or SCL.

If you use an adapter cable, you would also be limited 3.3V and 600mA.

1 Like

What solution do you recommend?

The connectors between the boards are not compatible. You will need to connect the MOSFET driver board to the pins on the ESP32-S3 board instead.