Introduction
In our previous article, “Power Supply Design Guide: How to Build Efficient and Reliable Power Circuits”, we explored the complete design flow of power circuits—from requirements analysis to layout and testing. Building on that foundation, this article focuses on practical techniques and key design considerations that play a critical role in enhancing power circuit performance, reducing EMI, and improving thermal management.
Key Considerations in Power Circuit Design
1. Use Simulation Tools
- When designing power circuits, simulation tools such as LTspice and PSIM can be used to simulate circuit behavior and stability.
- Design and testing should be done step-by-step, begin with simple models and gradually increase complexity.
2. PCB Layout Best Practices
- The switching loop of the switching power supply should be minimized in PCB layout to reduce EMI.
- Place input and output capacitors close to the switching devices to minimize parasitic inductance.
- Use multi-layer PCBs with dedicated ground layers to reduce electrical noise.
3. Choose the Right Power Control Mode
- Current Mode Control offers faster dynamic response, suitable for dynamic loads.
- Voltage Mode Control is simpler, suited for stable loads.
- Multi-Mode Control, such as PFM (Pulse Frequency Modulation) and PWM (Pulse Width Modulation) switching, can enhance efficiency during light loads.
4. Inductor and Capacitor Selection
- Choose inductors with saturation current ratings higher than maximum current to prevent magnetic saturation.
- Use low ESR capacitors on the output side to improve voltage regulation.
5. Switching Noise Management
- Add RC snubber circuits in parallel with switching devices to suppress voltage spikes and lower EMI.
6. Efficiency Improvement Techniques
- Use synchronous rectification instead of traditional diodes to reduce power losses and boost efficiency.
- Integrate soft-start circuits to limit inrush current and protect components during power-up.
7. Thermal Management
- Heat dissipation components and techniques should also be added to the circuit, as MOSFETs and rectifier diodes are often major heat sources.
- Use heat sinks, thermal paste, multilayer PCB and copper pours to improve heat dissipation.
- Reinforce key current paths with copper areas to lower impedance and assist thermal management.
8. Balancing Design Trade-Offs
- A good design requires the right balance between performance, efficiency, and reliability.
- Make application-specific adjustments based on operational conditions and priorities.
Related Article
Power Supply Design Guide: How to Build Efficient and Reliable Power Circuits